Build System Based on CMake
Build Process Flow
Broadly speaking, the build process flow can be divided into Kconfig process and CMake process.
When you run a build, build system starts from the example CMakelists.txt to work:
cmake_minimum_required(VERSION 3.30.0)
include(${SdkRootDirPath}/cmake/extension/mcux.cmake)
## In mcux.cmake, build system does the following work
# 1. Load used extension modules like python.cmake, ruby.cmake, sysbuild.cmake, etc
# 2. Clean cached cmake compiler flags variable
# 3. Load toolchain.cmake
# 4. Load board variable
# 5. Load device variable
# Kconfig needs board and device variables to work. With board and device variable, cmake has the environment to start Kconfig. This execution will be done in the following "project"
project(hello_world LANGUAGES C CXX ASM PROJECT_BOARD_PORT_PATH ${board_root}/${board}/demo_apps/hello_world)
## In this "project" macro, build system does the following work
# 6. Add execution cmake target
# 7. Add pristine cmake target
# 8. Execute Kconfig process to get .config and config headers
# 9. Process .config to get
# a. All used variables in cmake files so that all cmake files can be included
# b. component and project segment if-endif guard condition value so that CMake knows whether include or skip the component or project segment
# config headers with compiler macros inside which are in the build tree
# 10. Add run cmake target
# 11. Add GUI generation cmake target
include(${SdkRootDirPath}/CMakeLists.txt)
# ${SdkRootDirPath}/CMakeLists.txt is the assembly point for all device/board, drivers, components, middlewares cmake data.
# After the include(${SdkRootDirPath}/CMakeLists.txt), the project has got the environment setup and all depended data included
# If needed, load other customized cmake
include(${SdkRootDirPath}/examples/demo_apps/reconfig.cmake OPTIONAL)
include(${SdkRootDirPath}/${project_board_port_path}/reconfig.cmake OPTIONAL)
# Add the project self source and include
mcux_add_source(
SOURCES hello_world.c
)
mcux_add_include(
INCLUDES .
)
# get board porting sources and configuration data
include(${SdkRootDirPath}/${board_root}/${board}/demo_apps/hello_world/reconfig.cmake OPTIONAL)
# Convert binary to bin format
mcux_convert_binary(BINARY ${APPLICATION_BINARY_DIR}/${MCUX_SDK_PROJECT_NAME}.bin)
Toolchains Support
MCUXpresso SDK supports all mainstream toolchains in the embedded world beyond traditional armgcc.
The toolchain list supported by our build system is armgcc, iar, mdk, xtensa, codewarrior, riscvllvm and zephyr. The CMake toolchain setting files are placed in mcuxsdk/cmake/toolchain folder.
cmake
├── toolchain
├── armgcc.cmake # zephyr shares the same armgcc.cmake
├── codewarrior.cmake
├── iar.cmake
├── mdk.cmake
├── riscvllvm.cmake
├── xtensa.cmake
All toolchain files generally follow the same pattern, here is the iar.cmake:
set(CMAKE_EXECUTABLE_SUFFIX ".elf")
set(TOOLCHAIN_ROOT $ENV{IAR_DIR})
string(REGEX REPLACE "\\\\" "/" TOOLCHAIN_ROOT "${TOOLCHAIN_ROOT}")
if(NOT TOOLCHAIN_ROOT)
message(FATAL_ERROR "***Please set IAR_DIR in environment variables***")
endif()
SET(TARGET_TRIPLET "arm/bin")
set(AS "iasmarm")
set(CC "iccarm")
set(CXX "iccarm")
set(LD "ilinkarm")
set(AR "iarchive")
set(CPP "iccarm")
set(OC "ielftool")
set(OD "objdump")
set(AS ${TOOLCHAIN_ROOT}/${TARGET_TRIPLET}/${AS}${TOOLCHAIN_EXT})
set(CC ${TOOLCHAIN_ROOT}/${TARGET_TRIPLET}/${CC}${TOOLCHAIN_EXT})
set(CXX ${TOOLCHAIN_ROOT}/${TARGET_TRIPLET}/${CXX}${TOOLCHAIN_EXT})
set(LD ${TOOLCHAIN_ROOT}/${TARGET_TRIPLET}/${LD}${TOOLCHAIN_EXT})
set(AR ${TOOLCHAIN_ROOT}/${TARGET_TRIPLET}/${AR}${TOOLCHAIN_EXT})
set(CPP ${TOOLCHAIN_ROOT}/${TARGET_TRIPLET}/${CPP}${TOOLCHAIN_EXT})
set(OC ${TOOLCHAIN_ROOT}/${TARGET_TRIPLET}/${OC}${TOOLCHAIN_EXT})
set(OD ${TOOLCHAIN_ROOT}/${TARGET_TRIPLET}/${OD}${TOOLCHAIN_EXT})
set(CMAKE_ASM_COMPILER "${AS}")
set(CMAKE_C_COMPILER "${CC}")
set(CMAKE_CXX_COMPILER "${CXX}")
set(CMAKE_OBJCOPY "${OC}")
set(CMAKE_OBJDUMP "${OD}")
set(OBJDUMP_OUT_CMD "")
set(OBJDUMP_BIN_CMD "--bin")
The CMake variable for toolchain is CONFIG_TOOLCHAIN.
If you need to enable new toolchain, please follow the existing toolchain file to prepare the new one and place it in mcuxsdk/cmake/toolchain.
CMake Extension
MCUXpresso SDK is a comprehensive product including hundred of boards and devices, thousands of components and ten thousands of examples, all mainstream toolchains. The MCUXpresso CMake extensions aims to greatly reduce SDK data development and maintenance efforts.
Following extensions are provided for you to facilitate component, example and misc data record for all toolchains. All extension functions start with prefix mcux_
Source and Include
mcux_add_source/mcux_add_include
Adding source can be done with mcux_add_source.
For include path, the following functions are provided:
mcux_add_includeSet include path for all source code
mcux_add_asm_includeSet include path for assembly code
mcux_add_c_includeSet include path for C code
mcux_add_cpp_includeSet include path for CPP code
Here is the argument table:
Argument Name |
Argument Type |
Explanation |
|---|---|---|
BASE_PATH |
Single |
If provided, the final source path equals |
CONFIG |
Single |
|
PREINCLUDE |
Single |
|
PREINCLUDE_TYPE |
Multiple |
Can be any one or a combination of |
EXCLUDE |
Single |
|
SOURCES |
Multiple |
The sources. This is only for |
SCOPE |
Single |
Specify the source scope, can be INTERFACE/PUBLIC/PRIVATE. This is only for |
INCLUDES |
Multiple |
The includes. This is only for |
TARGET_FILES |
Multiple |
This is only for |
COMPILERS |
Multiple |
The compilers. It means the source or include only supports the listed compilers. |
TOOLCHAINS |
Multiple |
The toolchains. It means the source or include only supports the listed toolchains. |
CORES |
Multiple |
The cores. It means the source or include only supports the listed cores. |
CORE_IDS |
Multiple |
The core_ids. It means the source or include only supports the listed core_ids. This is usually to distinguish the support for core in multicore device. |
DEVICES |
Multiple |
The devices. It means the source or include only supports the listed device, like MIMXRT1176. |
DEVICE_IDS |
Multiple |
The device ids. It means the source or include only supports the listed device id, like MIMXRT1176xxxxx. |
FPU |
Multiple |
The fpu. It means the source or include only supports the listed fpu. fpu enum values are NO_FPU, SP_FPU and DP_FPU. |
DSP |
Multiple |
The dsp. It means the source or include only supports the listed dsp. dsp enum values are NO_DSP and HAS_DSP. |
TRUSTZONE |
Multiple |
The trustzone, enum values are TZ and NO_TZ. TZ means the source or include are only enabled on device with SAU, NO_TZ means they are only enabled on device without SAU. |
COMPONENTS |
Multiple |
The components. It means the source or include only supports the listed components. |
Wildcard *.<extension> and ** is supported in mcux_add_source, frequently used ones are *.*, *.c and *.h.
** will add alll kinds of files in all sub folders recursively into build.
If the number of files is relatively small, it is not recommended to use wildcards because it is implicit and time-consumed in build.
Here is one example:
# In drivers/uart/CMakelists.txt
if(CONFIG_MCUX_COMPONENT_driver.uart)
# with wildcard, it can be this way
mcux_add_source(
SOURCES *.*
)
mcux_add_include(
INCLUDES .
)
endif()
mcux_add_codewarrior_sys_include
Add header files search path for codewarrior system libraries.
Argument Name |
Argument Type |
Explanation |
|---|---|---|
TARGETS |
Multiple |
The build targets, like debug release |
SYS_SEARCH_PATH |
Multiple |
The path to be searched for header files |
SYS_PATH_RECURSIVELY |
Multiple |
The path and all the subdirectories to be searched recursively for header files |
Here is one example
mcux_add_codewarrior_sys_include(
SYS_SEARCH_PATH
"\"${MCUToolsBaseDir}/DSP56800x_EABI_Tools/M56800E Support/runtime_56800E/include\""
"\"${MCUToolsBaseDir}/DSP56800x_EABI_Tools/M56800E Support/msl/MSL_C/MSL_Common/Include\""
"\"${MCUToolsBaseDir}/DSP56800x_EABI_Tools/M56800E Support/msl/MSL_C/DSP_56800E/prefix\""
SYS_PATH_RECURSIVELY
"\"${MCUToolsBaseDir}/DSP56800x_EABI_Tools/M56800E Support\""
)
mcux_add_library
Specify the library to be linked.
Argument Name |
Argument Type |
Explanation |
|---|---|---|
BASE_PATH |
Single |
If provided, the final library path equals |
LIBS |
Multiple |
The libraries to be added |
SCOPE |
Single |
Specify the library scope, can be INTERFACE/PUBLIC/PRIVATE. This is only for |
TOOLCHAINS |
Multiple |
The toolchains. It means the library only supports the listed toolchains. |
CORES |
Multiple |
The cores. It means the library only supports the listed cores. |
CORE_IDS |
Multiple |
The core_ids. It means the library only supports the listed core_ids. This is usually to distinguish the support for core in multicore device. |
DEVICES |
Multiple |
The devices. It means the library only supports the listed device, like MIMXRT1176. |
DEVICE_IDS |
Multiple |
The device ids. It means the library only supports the listed device id, like MIMXRT1176xxxxx. |
FPU |
Multiple |
The fpu. It means the library only supports the listed fpu. fpu enum values are NO_FPU, SP_FPU and DP_FPU. |
DSP |
Multiple |
The dsp. It means the library only supports the listed dsp. dsp enum values are NO_DSP and HAS_DSP |
TRUSTZONE |
Multiple |
The trustzone, enum values are TZ and NO_TZ. TZ means the libraries are only enabled on device with SAU, NO_TZ means they are only enabled on device without SAU. |
COMPONENTS |
Multiple |
The components. It means the library only supports the listed components. |
GENERATED |
Single |
|
EXCLUDE |
Single |
|
HIDDEN |
Single |
|
TARGETS |
Multiple |
Specify the library is for designated build configuration targets. |
Here is one example:
mcux_add_library(
LIBS lib/kw45b41/kw45b41_nbu_libthreadx.a
TOOLCHAINS iar
)
The library can also be added by mcux_add_configuration. However it requires the absolute path and does not support source level dependency condition. Therefore, mcux_add_library is preferred for library adding.
mcux_convert_binary
Specify the output binary format
Argument Name |
Argument Type |
Explanation |
|---|---|---|
TOOLCHAINS |
Multiple |
Supported toolchains |
BINARY |
Single |
The target output binary name |
TARGET |
Single |
The target to be converted, the default is ${MCUX_SDK_PROJECT_NAME} if not set |
EXTRA_ARGS |
Multiple |
Extra arguments for binary conversion |
Here is one example:
mcux_convert_binary(
TOOLCHAINS armgcc mdk iar
BINARY ${APPLICATION_BINARY_DIR}/${MCUX_SDK_PROJECT_NAME}.bin
)
mcux_convert_binary(
TOOLCHAINS armgcc
BINARY ${APPLICATION_BINARY_DIR}/mybuild_slim.bin
EXTRA_ARGS --remove-section .fEraseNVM --remove-section .sEraseNVM
)
mcux_convert_binary(TARGET app BINARY ${APPLICATION_BINARY_DIR}/app.bin)
Note: Please make sure the target is executable type, otherwise the conversion will be skipped and you will get warning message like:
CMake Warning at mcuxsdk/cmake/extension/logging.cmake:46 (message):
WARNING: mcux_platformlib is library type, can't be converted to binary file by mcux_convert_binary
mcux_add_iar_linker_script/mcux_add_mdk_linker_script/mcux_add_armgcc_linker_script/mcux_add_codewarrior_linker_script/mcux_add_riscvllvm_linker_script
Add linker for toolchain.
Argument Name |
Argument Type |
Explanation |
|---|---|---|
TARGETS |
Multiple |
The build targets, like debug release. |
BASE_PATH |
Single |
If provided, the final linker path equals |
LINKER |
Single |
The linker path |
Here is one example
mcux_add_iar_linker_script(
TARGETS debug release
BASE_PATH ${SdkRootDirPath}
LINKER devices/${soc_portfolio}/${soc_series}/${device}/iar/${CONFIG_MCUX_TOOLCHAIN_LINKER_DEVICE_PREFIX}_flash.icf
)
mcux_add_armgcc_linker_script(
TARGETS debug release
BASE_PATH ${SdkRootDirPath}
LINKER devices/${soc_portfolio}/${soc_series}/${device}/gcc/${CONFIG_MCUX_TOOLCHAIN_LINKER_DEVICE_PREFIX}_flash.ld
)
mcux_add_mdk_linker_script(
TARGETS debug release
BASE_PATH ${SdkRootDirPath}
LINKER devices/${soc_portfolio}/${soc_series}/${device}/arm/${CONFIG_MCUX_TOOLCHAIN_LINKER_DEVICE_PREFIX}_flash.scf
)
Please remember to set TARGETS for the linker, otherwise the linker will be enabled for all targets.
MACRO
mcux_add_macro
Argument Name |
Argument Type |
Explanation |
|---|---|---|
TARGETS |
Multiple |
Supported build targets. If not provided, then supporting all targets. |
TOOLCHAINS |
Multiple |
Supported toolchains. If not provided, then supporting all toolchains. |
AS |
Single |
The assemble compiler macros. |
CC |
Single |
The c compiler macros. |
CX |
Single |
The cxx compiler macros. |
Note:
mcux_add_macroautomatically prefixes the macros that do not have the-Dprefix and duplicated macros will be removedHere is one example
mcux_add_macro( CC "FOO -DFOO -DBAR=1" # Equals -DFOO -DBAR=1 )
For all macros added by
mcux_add_configurationormcux_add_macro, if there are the duplicated macro names without value, like-DA -DA, or with the same value, like-DC=3 -DC=3, only one macro will be kept. If there are duplicated macro name with different values, build system will use the last one.If you want to set macro for assembler, c compiler and cpp compiler at the same time, there is an easy way to omit AS/CC/CX parameters:
mcux_add_macro( "-DFOO -DBAR=1" )
If the vaule of macro contains quotation marks, please use the escape symbol for them, for example:
mcux_add_macro( CC "-DMBEDTLS_CONFIG_FILE=\\\"ksdk_mbedtls_config.h\\\"" )
mcux_add_linker_symbol
The CMake function mcux_add_configuration requires the complete toolchain setting. For linker macro setting, you have to add prefix for linker symbol. The prefix may be different for each linker. For example, --config_def= for iar, --predefine= for mdk. To be convenient to set linker symbol for all toolchains, mcux_add_linker_symbol is provided.
Argument Name |
Argument Type |
Explanation |
|---|---|---|
TARGETS |
Multiple |
Supported build targets. If not provided, then supporting all targets. |
SYMBOLS |
Multiple |
The linker symbols. |
For example:
mcux_add_linker_symbol(
SYMBOLS gUseNVMLink_d=1
gEraseNVMLink_d=1
_ram_vector_table_=1
gFlashNbuImage_d=1
gUseProdInfoLegacyMode_d=1
)
For compatibility, it’s also supported to wrap all symbols in double quotes.
Configuration
mcux_add_configuration
Add configuration for all toolchains with specified build targets.
Argument Name |
Argument Type |
Explanation |
|---|---|---|
TARGETS |
Multiple |
Supported build targets. If not provided, then supporting all targets |
TOOLCHAINS |
Multiple |
Supported toolchains. If not provided, then supporting all toolchains |
LIB |
Multiple |
The library, the full path |
AS |
Single |
The assemble compiler flag |
CC |
Single |
The c compiler flags |
CX |
Single |
The cxx compiler flags |
LD |
Single |
The linker flags |
Please use native compiler flags of the compilers.
Here is one example
mcux_add_configuration(
TARGETS release
TOOLCHAINS IAR
AS "-M\"<>\" -w+ -s -j"
CC "--diag_suppress=Pa082,Pa050 --endian=little -e --use_c++_inline --silent"
CX "--diag_suppress=Pa082,Pa050 --endian=little -e --c++ --silent"
)
mcux_add_iar_configuration\mcux_add_mdk_configuration\mcux_add_armgcc_configuration\mcux_add_xcc_configuration\mcux_add_codewarrior_configuration
Very similar with mcux_add_configuration, just for specified toolchain.
EXTRA_FLAGS
Besides these mcux_add_ extension functions, you can directly pass compiler and linker flags with the following EXTRA flags directly from the command line:
Argument Name |
Explanation |
|---|---|
EXTRA_CPPFLAGS |
c and cpp preprocessor flags |
EXTRA_AFLAGS |
assembly compiler flags |
EXTRA_CFLAGS |
c compiler flags |
EXTRA_CXXFLAGS |
cpp compiler flags |
EXTRA_LDFLAGS |
linker flags |
Here is one example:
west build -b evkbmimxrt1170 examples/demo_apps/hello_world -Dcore_id=cm7 -DEXTRA_CPPFLAGS=-save-temps=obj
You can pass multiple flags once with double quotation marks like:
west build -b evkbmimxrt1170 examples/demo_apps/hello_world -Dcore_id=cm7 -DEXTRA_CPPFLAGS="-save-temps=obj -fno-inline"
Pre/Post Build Command
mcux_add_custom_command
CMake provides built-in function add_custom_command which is useful for performing an operation before or after building the target by setting PRE_BUILD | PRE_LINK | POST_BUILD parameters. For more details, please refer to add_custom_command. Based on this function, build system provides customized CMake function mcux_add_custom_command to set pre/post build command for specific targets and toolchains.
It shall only be used in the project CMakelists.txt, not the component one.
Argument Name |
Argument Type |
Explanation |
|---|---|---|
TARGETS |
Multiple |
Supported build targets. If not provided, then supporting all targets |
TOOLCHAINS |
Multiple |
Supported toolchains. If not provided, then supporting all toolchains |
BUILD_EVENT |
Single |
Specify the time when the command is executed, can be |
BUILD_COMMAND |
Multiple |
Specify the command-line(s) to execute. The format is same as CMake built-in function |
BYPRODUCTS |
Multiple |
Specify the files to be generated by command. It can be omitted if the directory of the generated files exist. |
WORKING_DIRECTORY |
Single |
Specify the working directory to execute the command. The default directory is |
Here is one example:
mcux_add_custom_command(
TARGETS debug release
TOOLCHAINS armgcc
BUILD_EVENT PRE_BUILD
BUILD_COMMAND ${TOOLCHAIN_DIR}/bin/arm-none-eabi-gcc -E -P -xc -I${SdkRootDirPath}/middleware/tfm/tf-m/platform/ext/target/nxp/evkmimxrt685/partition -I${SdkRootDirPath}/middleware/tfm/tf-m/platform/ext/common ${SdkRootDirPath}/middleware/tfm/tf-m/platform/ext/common/gcc/tfm_common_ns.ld -o ${SdkRootDirPath}/middleware/tfm/tf-m/platform/ext/common/gcc/tfm_common_ns_pre.ld
)
According to add_custom_command, for Ninja and Make generator, the PRE_BUILD behaves the same as PRE_LINK. Therefore, If you want to create files which is used for compilation, build system has provided a specific build event parameter PRE_COMPILE to simplify and unify custom command setting, for example:
mcux_add_custom_command(
BUILD_EVENT PRE_COMPILE
BUILD_COMMAND
sh ../middleware/wireless/zigbee/tools/ZPSConfig/Source/ZPSConfig
-n coordinator
-e LITTLE_ENDIAN
-t JN518x
-l ../middleware/wireless/zigbee/platform/K32W1/libs/libZPSNWK.a
-a ../middleware/wireless/zigbee/platform/K32W1/libs/libZPSAPL.a
-f ../middleware/wireless/zigbee/examples/zigbee_coordinator/src/coordinator.zpscfg
-o ../middleware/wireless/zigbee/examples/zigbee_coordinator/src/
BYPRODUCTS
../middleware/wireless/zigbee/examples/zigbee_coordinator/src/zps_gen.c
../middleware/wireless/zigbee/examples/zigbee_coordinator/src/zps_gen.h
)
Remove
Besides adding data, the build system also supports removing defined data. For example, if in a common definition, a macro is defined for examples in the board, but your example shall not use it, then you can use following remove function to remove it.
mcux_remove_configuration
Remove configuration for all toolchains with specified build targets.
Argument Name |
Argument Type |
Explanation |
|---|---|---|
TARGETS |
Multiple |
Supported build targets. If not provided, then supporting all targets |
TOOLCHAINS |
Multiple |
Supported toolchains. If not provided, then supporting all toolchains |
LIB |
Multiple |
The full path of the library |
AS |
Single |
The assemble compiler flags |
CC |
Single |
The c compiler flags |
CX |
Single |
The cxx compiler flags |
LD |
Single |
The linker flags |
Please use native compiler flags of the compilers.
Here is one example:
mcux_remove_configuration(
TARGETS release
AS "-DMCUXPRESSO_SDK -DNDEBUG"
CC "-DMCUXPRESSO_SDK -DNDEBUG"
CX "-DMCUXPRESSO_SDK -DNDEBUG"
)
mcux_remove_iar_configuration/mcux_remove_mdk_configuration/mcux_remove_armgcc_configuration
Very similar with mcux_remove_configuration, just for specified toolchain.
mcux_remove_macro
Remove macros for all toolchains with specified build targets.
Argument Name |
Argument Type |
Explanation |
|---|---|---|
TARGETS |
Multiple |
Supported build targets. If not provided, then supporting all targets |
TOOLCHAINS |
Multiple |
Supported toolchains. If not provided, then supporting all toolchains |
AS |
Single |
The assemble compiler macros |
CC |
Single |
The c compiler macros |
CX |
Single |
The cxx compiler macros |
mcux_remove_macro automatically prefixes macros that do not have the -D prefix
Here is one example:
mcux_remove_macro(CC "TESTMACRO")
mcux_remove_linker_symbol
Remove linker symbol for all toolchains with specified build targets.
Argument Name |
Argument Type |
Explanation |
|---|---|---|
TARGETS |
Multiple |
Supported build targets. If not provided, then supporting all targets |
SYMBOLS |
Single |
The linker symbols to be removed |
Here is one example:
mcux_remove_linker_symbol(
SYMBOLS "gFlashNbuImage_d=1"
)
mcux_remove_iar_linker_script/mcux_remove_mdk_linker_script/mcux_remove_armgcc_linker_script/mcux_remove_codewarrior_linker_script
Argument Name |
Argument Type |
Explanation |
|---|---|---|
TARGETS |
Multiple |
The build targets, like debug release |
BASE_PATH |
Single |
If provided, the final linker path equals |
LINKER |
Single |
The linker path |
Here is one example:
mcux_remove_iar_linker_script(
TARGETS debug release
BASE_PATH ${SdkRootDirPath}
LINKER devices/${soc_portfolio}/${soc_series}/${device}/iar/${CONFIG_MCUX_TOOLCHAIN_LINKER_DEVICE_PREFIX}_flash.icf
)
mcux_remove_armgcc_linker_script(
TARGETS debug release
BASE_PATH ${SdkRootDirPath}
LINKER devices/${soc_portfolio}/${soc_series}/${device}/gcc/${CONFIG_MCUX_TOOLCHAIN_LINKER_DEVICE_PREFIX}_flash.ld
)
mcux_remove_mdk_linker_script(
TARGETS debug release
BASE_PATH ${SdkRootDirPath}
LINKER devices/${soc_portfolio}/${soc_series}/${device}/arm/${CONFIG_MCUX_TOOLCHAIN_LINKER_DEVICE_PREFIX}_flash.scf
)
mcux_project_remove_include\mcux_project_remove_source
Remove project source or include.
Argument Name |
Argument Type |
Explanation |
|---|---|---|
BASE_PATH |
Single |
If provided, the final source path equals |
INCLUDES |
Multiple |
The include path. |
SOURCES |
Multiple |
The source path. |
Here is one example:
mcux_project_remove_source(
SOURCES hello_world.c
)
mcux_project_remove_include(
INCLUDES .
)
mcux_remove_library
Remove libraries. It will take effect no matter the library was added before or after this statement.
Argument Name |
Argument Type |
Explanation |
|---|---|---|
BASE_PATH |
Single |
If provided, the final source path equals |
LIBS |
Multiple |
The library files to be removed |
Here is one example:
mcux_remove_library(
BASE_PATH ${SdkRootDirPath}
SOURCES devices/${soc_portfolio}/${soc_series}/${device}/iar/iar_lib_power.a
)
Misc
mcux_set_variable
Set variable with global scope. It requests that variable defined by mcux_set_variable must be unique. Build system will report error if there are duplicated variables defined with mcux_set_variable.
Here is one example:
mcux_set_variable(soc_series Kinetis)
mcux_set_list
Set a cmake list.
Here is one example
mcux_set_list(KW47_FAMILY "KW47B42Z83xxxA KW47B42Z96xxxA KW47B42Z97xxxA KW47B42ZB2xxxA KW47B42ZB3xxxA KW47B42ZB6xxxA KW47B42ZB7xxxA KW47Z42082xxxA KW47Z42092xxxA KW47Z420B2xxxA KW47Z420B3xxxA")
mcux_add_cmakelists
Add CMakelists.txt
Here is one example:
mcux_add_cmakelists(${CMAKE_CURRENT_LIST_DIR}/drivers)
mcux_load_all_cmakelists_in_directory
Load all cmakelists under one directory
mcux_load_all_cmakelists_in_directory(${SdkRootDirPath}/drivers)