Hardware requirements

  • Micro USB cable

  • FRDM-RW612 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo

  1. Connect a micro USB cable between the PC host and the MCU-Link USB port (J10) on the board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the example.

Running the demo

When the demo runs successfully, the terminal will display similar information like the following:

ELS PKC common example

============================ ELS get info:pass RNG PRNG random:pass Flow protection:pass Memory data invariant compare:pass Memory data invariant copy:pass Key component operations:pass PKC power down wake-up init:pass

============================ RESULT: All 7 test PASS!! ELS example END