Hardware requirements
Mini/micro USB cable
MCXW23-EVK Board
Personal Computer
Board settings
USART hardware flow control on one board. The USART sends data to itself(loopback), and hardware flow control function is enabled on this example. So please make sure the correct connection for example.
Pin Name Board Location connect to Pin Name Board Location
USART_TX J17-4 ---------- USART_RX J17-3
USART_CTS J24-3 ---------- USART_RTS J18-3
Prepare the Demo
Connect a USB cable between the host PC and the EVK board J33.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the terminal like:
This is USART hardware flow control example on one board.
This example will send data to itself and will use hardware flow control to avoid the overflow.
Please make sure you make the correct line connection. Basically, the connection is:
USART_TX -- USART_RX
USART_RTS -- USART_CTS
Data matched! Transfer successfully.