Hardware requirements
Mini/micro USB cable
MCXW23-EVK Board
Personal Computer
Board settings
No special is needed.
Prepare the Demo
Connect a USB cable between the host PC and the EVK board J33.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the terminal like:
Usart functional API interrupt example
Board receives characters then sends them out
Now please input: