Hybrid (Dual-mode) Bluetooth Low Energy and Generic FSK

The Hybrid (Dual-mode) Bluetooth Low Energy and Generic FSK application demonstrates Generic FSK transmission/reception and Bluetooth advertising/scanning/multiple connections coexistence.

The Bluetooth LE part of this demo implements a modified version of the Wireless UART demo application, capable of multiple Bluetooth LE connections.

Based on the Hardware link-layer implementation, the Bluetooth Low Energy has a higher priority than the Generic FSK protocol and as the effect, the Generic FSK communication is executed during the Idle states (inactive periods) of the Bluetooth LE. The coexistence of the two protocols is handled internally at the Controller level.

The Bluetooth LE part of the application behaves at first as a GAP central node. It enters GAP Limited Discovery Procedure and searches for other Wireless UART devices to connect. To change the device role to GAP peripheral, use the ROLESW button. The device enters GAP General Discoverable Mode and waits for a GAP central node to connect.

The Generic FSK part of the application can either enter in the receive state by double clicking the SCANSW button or it can start the periodic transmit by long pressing the ROLESW button. It cannot enter in both states at the same time.

The Generic FSK has lower priority than the Bluetooth LE. Therefore, any ongoing Generic FSK receive is paused by the Controller when Bluetooth LE activity is ongoing. The reception is automatically resumed by the Controller when there is no Bluetooth LE activity.

The first Generic FSK transmit command is buffered if there is continuous Bluetooth LE activity (for example, for continuous Bluetooth LE scanning). Any succeeding Generic FSK transmit command indicates failure in the command line interface, if the initial buffered transmit command was not sent yet.

This section describes the implemented profiles and services, user interactions, and testing methods for the Hybrid (Dual-Mode) Bluetooth Low Energy and Generic FSK application.

Implemented profile and services

The Hybrid (Dual-Mode) Bluetooth Low Energy and Generic FSK application implements the GATT client and server for the custom Wireless UART profile and services. It also acts as a Generic FSK transmitter/receiver, repeating a custom packet, at a fixed periodic interval. It uses a predefined identifier, isolated to the address used in the Bluetooth LE protocol of the demo.

  • Wireless UART Service (UUID: 01ff0100-ba5e-f4ee-5ca1-eb1e5e4b1ce0)

  • Battery Service v1.0

  • Device Information Service v1.1

The Wireless UART service is a custom service that implements a custom writable ASCII Char characteristic (UUID: 01ff0101-ba5e-f4ee-5ca1-eb1e5e4b1ce0) that holds the character written by the peer device.

The application is ready to start either Bluetooth LE scanning for Wireless UART Service, Bluetooth LE advertising Wireless UART Service, Generic FSK periodic transmit of a custom packet or Generic FSK receive, in the available slots not used by the Bluetooth LE protocol.

Parent topic:Hybrid (Dual-mode) Bluetooth Low Energy and Generic FSK

Supported platforms

The following platforms support the Hybrid (dual-mode) Bluetooth Low Energy and Generic FSK application:

  • KW45B41Z-EVK

  • KW45B41Z-LOC

  • KW47-EVK

  • KW47-LOC

Parent topic:Hybrid (Dual-mode) Bluetooth Low Energy and Generic FSK

User interface

After flashing the board, the device is in idle mode (all LEDs flashing). To start Bluetooth LE scanning, press the SCANSW button. When in GAP Limited Discovery Procedure of GAP General Discoverable Mode, CONNLED is flashing. When the node connects to a peer device, CONNLED turns solid. To disconnect the node, hold the SCANSW button pressed for 2-3 seconds. The node then re-enters GAP Limited Discovery Procedure.

To start Generic FSK receiving, double click the SCANSW button and the device starts receiving packets on the same channel as the Bluetooth LE channel 37, with the network address defined in gGenFSK_NetworkAddress_c. The receiver only prints the packets that have the predefined identifier at gGenFSK_Identifier_c. To stop Generic FSK reception, double click the ROLESW button.

On a different device, start Generic FSK transmit by long pressing the ROLESW button. To stop the periodic Generic FSK transmit, long press again the ROLESW button, if the transmit procedure is ongoing. The long press ROLESW acts as a toggle for the transmit.

Parent topic:Hybrid (Dual-mode) Bluetooth Low Energy and Generic FSK

Usage

The application is built to work with another supported platform running the same example. When testing with two boards, perform the following steps:

Case 1 (Bluetooth LE)

  1. Open a serial port terminal and connect to the two boards, in the same manner described in Testing devices. The figure below displays the start screen after the board is reset.

    Tera Term – Hybrid Wireless UART (Bluetooth LE) - Generic FSK start screen Tera Term – Hybrid Wireless UART (Bluetooth LE) - Generic FSK start screen

  2. The application starts as a GAP central. To switch the role to a GAP peripheral, press the ROLESW button. Depending on the role, when pressing the SCANSW button, the application starts either scanning or advertising.

  3. As soon as the CONNLED turns solid on both devices, the user can start writing in one of the consoles. The text appears on the other terminal.

  4. After creating a connection, the role (central or peripheral) is displayed on the console. The role switch can be pressed again before creating a new connection. An output example can be observed in the figure below.

    Tera Term – received text on Wireless UART (Bluetooth LE) Tera Term – received text on Wireless UART (Bluetooth LE)

Parent topic:Usage

Case 2 (Generic FSK)

When operating the Generic FSK mode, the following steps should be followed.

  1. Open a serial port terminal and connect to the two boards, in the same manner described in Testing devices. The start screen after the board is reset is the same as in Figure.

  2. The Generic FSK communication direction is not preset. To start receiving, double click the SCANSW button on one board. Then, the device starts receiving packets on the same channel as the Bluetooth LE channel 37.

  3. To start transmitting, long press the ROLESW button on the other board. The transmitting device uses an identifier known by the receiver and its packets are displayed in the CLI as shown in Figure:

    Teraterm – packet transmit/receive on Generic FSK

  4. To stop Generic FSK reception, double click the ROLESW button.

  5. To stop the periodic Generic FSK transmit operation, long press the ROLESW button again, if the transmit procedure is ongoing. The long press of the ROLESW button acts as a toggle for the transmit. At this point, both devices can reverse the direction of communication by following the exact same steps.

    See Figure.

    Tera Term – stop Generic FSK activity

Parent topic:Usage

Case 3 (Dual-mode)

The application is ready to combine both scenarios. It can either:

  • Establish a Bluetooth LE connection and perform Generic FSK activity.

  • During Generic FSK activity, the Bluetooth LE connection can be established and the Controller pauses receiving or announcing the discarded Generic FSK transmissions. This activity is resumed after the Bluetooth LE activity is finished.

To run the Dual-mode scenario, follow the steps below:

  1. Establish a Bluetooth LE connection as described in Case 1 (Bluetooth LE).

  2. Start Generic FSK activity as described in Case 2 (Generic FSK), independent of the Bluetooth LE roles chosen in Case 1.

  3. Start typing in either of the terminals. As seen in Figure, the Bluetooth LE activity is prioritized. In this step, characters are printed in the peer’s terminal and Generic FSK continues in the available slots, not used by the Bluetooth LE link.

    Teraterm – Mixed Wireless UART (Bluetooth LE) and Generic FSK activity

Parent topic:Usage

Parent topic:Hybrid (Dual-mode) Bluetooth Low Energy and Generic FSK

Customization

Use the steps below to change the default settings of this demo.

For Bluetooth LE, the default advertising config (gAdvParams) parameter is found in the app_config.c file. Also, the scanning parameters (gScanParams) can be found in this file.

Note: The Generic FSK protocol is active during the inactive periods of the Bluetooth LE protocol. The demo is currently configured to have the scan window equal to the scan interval to make the user aware of this, but this can be changed.

For Generic FSK, the following defines of interest can be found in genfsk_app.h, described below:

Name

Description

gGenFSK_NetworkAddress_c

This is the network address used for the Generic FSK, in the transmitter payload. It is implicitly set to the 0x8E89BED6, but this can be reconfigured. Ensure that it is also changed on the receiver in the hybrid_gfsk.c controller file.

gGenFSK_H0Value_c

H0 value is used in the header.

gGenFSK_Identifier_c

This is the identifier used by the transmitter to be filtered at the receiver. The current implementation filters the Generic FSK packets received, based on this define.

gGenFskApp_TxInterval_c

This is the interval the transmitter will repeat the transmission of a packet. It is set in milliseconds.

Files of interest

The demo can be found in the w_uart_genfsk from the available examples.

The demo is based on the basic Wireless UART with the addition of some Generic FSK files required for working in dual-mode, described below.

File name

Description

genfsk_app.c

Application common module. Handles the HCI commands and events for the Generic FSK. Sends the events to the application.

genfsk_app.h

Application common module. Exposes public functions.

hybrid_gfsk.c

Controller common module. Handles initialization of Generic FSK.

hybrid_gfsk.h

Controller common module. Exposes public functions.

Parent topic:Hybrid (Dual-mode) Bluetooth Low Energy and Generic FSK

Parent topic:Bluetooth LE stack and demo applications