Logo
25.06.00-pvw1
MCUXpresso SDK Project v: latest
Document Release Versions
24.12.00-pvw2
24.12.00
25.03.00-pvw2
25.03.00
latest

Introduction

  • MCUXpresso SDK
  • Setup

Getting Started

  • Github Repository
  • Zip Package

User Guide

  • Drivers
  • Examples
  • Middlewares
  • RTOS
  • Boards

Development

  • Architecture
  • Build And Configuration System
  • Developing with MCUXpresso SDK

Releases

  • Release Notes
mcuxsdk
  • Docs / 25.06.00-pvw1 »
  • Touchlink
  • Open on Repo Report an issue with this page

Touchlink

Touchlink commissioning is used to form a new network and/or join a node to an existing network. Touchlink is initiated on a node called the ‘initiator’ which either is a member of an existing network or (if not) creates a new network. In both cases, the initiator joins a second node to the network, called the ‘target’ node.

Touchlink is provided as a cluster in the ZigBee Cluster Library (ZCL). The initiator must support the Touchlink cluster as a client and the target node must support the cluster as a server. If it is required on a node, Touchlink commissioning must be enabled via the ZigBee Base Device attribute u8bdbCommissioningMode. For detailed information on the Touchlink Commissioning cluster and how to implement Touchlink, refer to the (ZigBee Cluster Library User Guide (JNUG3132)[https://kex-daily.nxp.com/mcuxsdk-internal/latest/html/_static/wireless/Zigbee/JN-UG-3132-ZigBee3-Cluster-Library.pdf].

A ‘Touchlink Pre-configured Link Key’ is provided, which is used during the commissioning of a node into a secured network (see Network security).

If Touchlink commissioning is not successful, this is indicated by a status of NO_SCAN_RESPONSE through the attribute ebdbCommissioningStatus (all other states indicate success).

Parent topic:Network commissioning


Copyright 2025, NXP. Last generated on Apr 23, 2025 13:43+0200; branch release/25.06.00-pvw1, revision 37f4823f37be0be386f37b97e43a105ab02ecab1.