MCUXpresso SDK Changelog
ADC16
[2.3.0]
Improvements
Added new API ADC16_EnableAsynchronousClockOutput() to enable/disable ADACK output.
In ADC16_GetDefaultConfig(), set enableAsynchronousClock to false.
[2.2.0]
Improvements
Added hardware average mode in adc_config_t structure, then the hardware average mode can be set by invoking ADC16_Init() function.
[2.1.0]
New Features:
Supported KM series’ new ADC reference voltage source, bandgap from PMC.
[2.0.3]
Bug Fixes
Fixed IAR warning Pa082: the order of volatile access should be defined.
[2.0.2]
Improvements
Used conversion control feature macro instead of that in IO map.
[2.0.1]
Bug Fixes
Fixed MISRA-2012 rules.
Rule 16.4, 10.1, 13.2, 14.4 and 17.7.
[2.0.0]
Initial version
CLOCK
[2.5.3]
Bug Fixes
Fixed an issue that in CLOCK_SetFbeMode() C4 register not updated.
[2.5.2]
Bug Fixes
Fixed violations of MISRA C-2012 rule 18.1.
[2.5.1]
Bug Fixes
Fixed violations of MISRA C-2012 rule 10.1, rule 10.8, rule 12.2 and so on.
[2.5.0]
New Features
Moved SDK_DelayAtLeastUs function from clock driver to common driver.
Fixed IAR warning Pa082 for the clock driver.
[2.4.0]
New Features
Added two APIs to set slow and fast internal reference clock variable.
[2.3.0]
Bug Fixes
Fixed the issue for MISRA-2012 check.
Fixed rule 10.4, rule 10.1, rule 10.6, rule 13.5, rule 10.8.
Fixed incorrect External Oscillator Configuration sequence and ensure oscillator configuration be executed before it be enabled.
New Features
Added new API CLOCK_DelayAtLeastUs() implemented by DWT to allow users set delay in unit of microsecond.
[2.2.1]
Bug Fixes
Fixed the issue that MCG could not switch to FEE/FBE/PBE modes when OSCERCLK clock not enabled.
[2.2.0]
New Features
Updated CLOCK_SetFeiMode/CLOCK_SetFbiMode/CLOCK_BootToFeiMode() to support set MCG_C4[DMX32]=1 in FEI/FBI modes.
Bug Fixes
Updated IP_CLOCKS array, remove unused gates and add missing gates.
[2.1.0]
Other Changes
Merged fsl_mcg and fsl_osc into fsl_clock.
[2.0.0]
Initial version.
CMP
[2.0.3]
Improvements
Updated to clear CMP settings in DeInit function.
[2.0.2]
Bug Fixes
Fixed the violations of MISRA 2012 rules:
Rule 10.3
[2.0.1]
Bug Fixes
Fixed MISRA-2012 rules.
Rule 14.4, rule 10.3, rule 10.1, rule 10.4 and rule 17.7.
[2.0.0]
Initial version.
COMMON
[2.6.0]
Bug Fixes
Fix CERT-C violations.
[2.5.0]
New Features
Added new APIs InitCriticalSectionMeasurementContext, DisableGlobalIRQEx and EnableGlobalIRQEx so that user can measure the execution time of the protected sections.
[2.4.3]
Improvements
Enable irqs that mount under irqsteer interrupt extender.
[2.4.2]
Improvements
Add the macros to convert peripheral address to secure address or non-secure address.
[2.4.1]
Improvements
Improve for the macro redefinition error when integrated with zephyr.
[2.4.0]
New Features
Added EnableIRQWithPriority, IRQ_SetPriority, and IRQ_ClearPendingIRQ for ARM.
Added MSDK_EnableCpuCycleCounter, MSDK_GetCpuCycleCount for ARM.
[2.3.3]
New Features
Added NETC into status group.
[2.3.2]
Improvements
Make driver aarch64 compatible
[2.3.1]
Bug Fixes
Fixed MAKE_VERSION overflow on 16-bit platforms.
[2.3.0]
Improvements
Split the driver to common part and CPU architecture related part.
[2.2.10]
Bug Fixes
Fixed the ATOMIC macros build error in cpp files.
[2.2.9]
Bug Fixes
Fixed MISRA C-2012 issue, 5.6, 5.8, 8.4, 8.5, 8.6, 10.1, 10.4, 17.7, 21.3.
Fixed SDK_Malloc issue that not allocate memory with required size.
[2.2.8]
Improvements
Included stddef.h header file for MDK tool chain.
New Features:
Added atomic modification macros.
[2.2.7]
Other Change
Added MECC status group definition.
[2.2.6]
Other Change
Added more status group definition.
Bug Fixes
Undef __VECTOR_TABLE to avoid duplicate definition in cmsis_clang.h
[2.2.5]
Bug Fixes
Fixed MISRA C-2012 rule-15.5.
[2.2.4]
Bug Fixes
Fixed MISRA C-2012 rule-10.4.
[2.2.3]
New Features
Provided better accuracy of SDK_DelayAtLeastUs with DWT, use macro SDK_DELAY_USE_DWT to enable this feature.
Modified the Cortex-M7 delay count divisor based on latest tests on RT series boards, this setting lets result be closer to actual delay time.
[2.2.2]
New Features
Added include RTE_Components.h for CMSIS pack RTE.
[2.2.1]
Bug Fixes
Fixed violation of MISRA C-2012 Rule 3.1, 10.1, 10.3, 10.4, 11.6, 11.9.
[2.2.0]
New Features
Moved SDK_DelayAtLeastUs function from clock driver to common driver.
[2.1.4]
New Features
Added OTFAD into status group.
[2.1.3]
Bug Fixes
MISRA C-2012 issue fixed.
Fixed the rule: rule-10.3.
[2.1.2]
Improvements
Add SUPPRESS_FALL_THROUGH_WARNING() macro for the usage of suppressing fallthrough warning.
[2.1.1]
Bug Fixes
Deleted and optimized repeated macro.
[2.1.0]
New Features
Added IRQ operation for XCC toolchain.
Added group IDs for newly supported drivers.
[2.0.2]
Bug Fixes
MISRA C-2012 issue fixed.
Fixed the rule: rule-10.4.
[2.0.1]
Improvements
Removed the implementation of LPC8XX Enable/DisableDeepSleepIRQ() function.
Added new feature macro switch “FSL_FEATURE_HAS_NO_NONCACHEABLE_SECTION” for specific SoCs which have no noncacheable sections, that helps avoid an unnecessary complex in link file and the startup file.
Updated the align(x) to attribute(aligned(x)) to support MDK v6 armclang compiler.
[2.0.0]
Initial version.
CRC
[2.0.4]
Improvements
Release peripheral from reset if necessary in init function.
[2.0.3]
Bug fix:
Fix MISRA issues.
[2.0.2]
Bug fix:
Fix MISRA issues.
[2.0.1]
Bug fix:
DATA and DATALL macro definition moved from header file to source file.
[2.0.0]
Initial version.
DAC
[2.0.2]
Bug Fixes
Fixed MISRA-2012 issues:
Rule 10.3, 10.8 and 17.7.
[2.0.1]
Bug Fixes
Moved the default DAC_Enable(…, true) from DAC_Init() to the application code so that users can enable the DAC’s output.
[2.0.0]
Initial version.
DMAMUX
[2.1.1]
Improvements
Add macro FSL_FEATURE_DMAMUX_CHANNEL_NEEDS_ENDIAN_CONVERT and DMAMUX_CHANNEL_ENDIAN_CONVERTn do channel endian convert.
[2.1.0]
Improvements
Modify the type of parameter source from uint32_t to int32_t in the DMAMUX_SetSource.
[2.0.5]
Improvements
Added feature FSL_FEATURE_DMAMUX_CHCFG_REGISTER_WIDTH for the difference of CHCFG register width.
[2.0.4]
Bug Fixes
Fixed violations of MISRA C-2012 rule 10.4.
[2.0.3]
Bug Fixes
Fixed the issue for MISRA-2012 check.
Fixed rule 10.4 and rule 10.3.
[2.0.2]
New Features
Added an always-on enable feature to a DMA channel for ULP1 DMAMUX support.
[2.0.1]
Bug Fixes
Fixed the build warning issue by changing the type of parameter source from uint8_t to uint32_t when setting DMA request source in DMAMUX_SetSourceChange.
[2.0.0]
Initial version.
DSPI
[2.2.7]
Improvements
Added macros to disable some features.
[2.2.6]
Bug Fixes
Fixed the txData from void * to const void * in transmit API.
[2.2.5]
Improvements
Initialized the EDMA configuration structure in the DSPI EDMA driver.
[2.2.4]
Bug Fixes
Fixed bug that instance with shared TR/RX EDMA request cannot transfer 1 datawidth of data as master in single transfer.
[2.2.3]
Improvements
Added macro of getting maximum transfer size using EDMA way.
[2.2.2]
Bug Fixes
MISRA C-2012 issue fixed:
Fixed rules, containing: 10.8, 10.3.
Fixed the build warning issue.
Fixed the bug that PCS would temporarily pull down for a while during master initialization.
Fixed compiling error of undefined identifier g_dspiDummyData.
Changed the type of kDSPI_AllStatusFlag and kDSPI_AllInterruptEnable from int to uint32_t to fix Pe068 warning of integer conversion.
Eliminated IAR Pa082 warning in DSPI_MasterTransferDMA.
[2.2.1]
Bug Fixes
Fixed the bug for double execution of transfer complete callback in master interrupt transfer mode. In the interrupt routine, the DSPI interrupt may drop in the situation of the interrupt pending by itself while receiving the last frame, adding check to the transfer state to execute the callback function.
Fixed wrong logic in DSPI_SetFifoEnable().
MISRA C-2012 issue fixed.
Fixed rules, containing: rule-12.1, rule-17.7, rule-16.4, rule-14.4, rule-10.4, rule-10.8, rule-10.3, rule-10.1, rule-10.6, rule-13.5, rule-11.3, rule-13.2, rule-8.3, and rule-8.5.
[2.2.0]
New Features
Added gasket feature for SPI EDMA driver, which reduces one channel used in the EDMA master transfer. With this feature support, only two channels are needed. For example, if the gasket feature is supported, we could use the DSPI_MasterTransferCreateHandleEDMA function like below: DSPI_MasterTransferCreateHandleEDMA(EXAMPLE_DSPI_MASTER_BASEADDR, &g_dspi_edma_m_handle, DSPI_MasterUserCallback, &userData, &dspiEdmaMasterRxRegToRxDataHandle, NULL, &dspiEdmaMasterIntermediaryToTxRegHandle);
Added dummy data setup API to allow users to configure the dummy data to be transferred.
Added new APIs for half-duplex transfer function. Users can send and receive data by one API in the polling/interrupt/EDMA way, and they can choose either to transmit first or to receive first. Additionally, the PCS pin can be configured as assert status in transmission (between transmit and receive) by setting the isPcsAssertInTransfer to true.
[2.1.4]
Bug Fixes
DSPI EDMA driver: the DSPI instance has been separated, so the DMA request source can now transfer up to 32767 Bytes data in one DSPI_MasterTransferEDMA() transfer.
[2.1.3]
Bug Fixes
DSPI EDMA driver can no longer support the case that the transfer data size is odd, but the bitsPerFrame is greater than 8.
Improvements
Added #ifndef/#endif to allow users to change the default TX value at compile time.
[2.1.2]
Bug Fixes
DSPI_MasterTransferBlocking function would hang in some corner cases (for example, some cases with bitsPerFrame is 4,6 and kDSPI_MasterPcsContinuous transfer mode).
[2.1.1]
Bug Fixes
Set the EOQ (End Of Queue) bit to TRUE for the last transfer in transactional APIs.
[2.1.0]
New Features
Added Transfer prefix in transactional APIs.
[2.0.0]
Initial version.
DSPI_EDMA
[2.2.7]
Improvements
Added macro to disable slave functionality.
[2.2.6]
Improvements
Add EDMA ext API to accommodate more types of EDMA.
[2.2.5]
Refer DSPI driver change log 2.0.0 to 2.4.1
EDMA
[2.4.5]
Bug Fixes
Fixed memory convert would convert NULL as zero address issue.
[2.4.4]
Bug Fixes
Fixed comments by replacing STCD with TCD
Fixed the TCD overwrite issue when submit transfer request in the callback if there is a active TCD in hardware.
Fixed violations of MISRA C-2012 rule 10.8,5.6.
[2.4.3]
Improvements
Added FSL_FEATURE_MEMORY_HAS_ADDRESS_OFFSET to convert the address between system mapped address and dma quick access address.
Bug Fixes
Fixed the wrong tcd done count calculated in first TCD interrupt for the non scatter gather case.
[2.4.2]
Bug Fixes
Fixed the wrong tcd done count calculated in first TCD interrupt by correct the initial value of the header.
Fixed violations of MISRA C-2012 rule 10.3, 10.4.
[2.4.1]
Bug Fixes
Added clear CITER and BITER registers in EDMA_AbortTransfer to make sure the TCD registers in a correct state for next calling of EDMA_SubmitTransfer.
Removed the clear DONE status for ESG not enabled case to aovid DONE bit cleared unexpectedly.
[2.4.0]
Improvements
Added api EDMA_EnableContinuousChannelLinkMode to support continuous link mode.
Added apis EDMA_SetMajorOffsetConfig/EDMA_TcdSetMajorOffsetConfig to support major loop address offset feature.
Added api EDMA_EnableChannelMinorLoopMapping for minor loop offset feature.
Removed the reduntant IRQ Handler in edma driver.
[2.3.2]
Improvements
Fixed HIS ccm issue in function EDMA_PrepareTransferConfig.
Fixed violations of MISRA C-2012 rule 11.6, 10.7, 10.3, 18.1.
Bug Fixes
Added ACTIVE & BITER & CITER bitfields to determine the channel status to fixed the issue of the transfer request cannot submit by function EDMA_SubmitTransfer when channel is idle.
[2.3.1]
Improvements
Added source/destination address alignment check.
Added driver IRQ handler support for multi DMA instance in one SOC.
[2.3.0]
Improvements
Added new api EDMA_PrepareTransferConfig to allow different configurations of width and offset.
Bug Fixes
Fixed violations of MISRA C-2012 rule 10.4, 10.1.
Fixed the Coverity issue regarding out-of-bounds write.
[2.2.0]
Improvements
Added peripheral-to-peripheral support in EDMA driver.
[2.1.9]
Bug Fixes
Fixed MISRA issue: Rule 10.7 and 10.8 in function EDMA_DisableChannelInterrupts and EDMA_SubmitTransfer.
Fixed MISRA issue: Rule 10.7 in function EDMA_EnableAsyncRequest.
[2.1.8]
Bug Fixes
Fixed incorrect channel preemption base address used in EDMA_SetChannelPreemptionConfig API which causes incorrect configuration of the channel preemption register.
[2.1.7]
Bug Fixes
Fixed incorrect transfer size setting.
Added 8 bytes transfer configuration and feature for RT series;
Added feature to support 16 bytes transfer for Kinetis.
Fixed the issue that EDMA_HandleIRQ would go to incorrect branch when TCD was not used and callback function not registered.
[2.1.6]
Bug Fixes
Fixed KW3X MISRA Issue.
Rule 14.4, 10.8, 10.4, 10.7, 10.1, 10.3, 13.5, and 13.2.
Improvements
Cleared the IRQ handler unavailable for specific platform with macro FSL_FEATURE_EDMA_MODULE_CHANNEL_IRQ_ENTRY_SHARED_OFFSET.
[2.1.5]
Improvements
Improved EDMA IRQ handler to support half interrupt feature.
[2.1.4]
Bug Fixes
Cleared enabled request, status during EDMA_Init for the case that EDMA is halted before reinitialization.
[2.1.3]
Bug Fixes
Added clear DONE bit in IRQ handler to avoid overwrite TCD issue.
Optimized above solution for the case that transfer request occurs in callback.
[2.1.2]
Improvements
Added interface to get next TCD address.
Added interface to get the unused TCD number.
[2.1.1]
Improvements
Added documentation for eDMA data flow when scatter/gather is implemented for the EDMA_HandleIRQ API.
Updated and corrected some related comments in the EDMA_HandleIRQ API and edma_handle_t struct.
[2.1.0]
Improvements
Changed the EDMA_GetRemainingBytes API into EDMA_GetRemainingMajorLoopCount due to eDMA IP limitation (see API comments/note for further details).
[2.0.5]
Improvements
Added pubweak DriverIRQHandler for K32H844P (16 channels shared).
[2.0.4]
Improvements
Added support for SoCs with multiple eDMA instances.
Added pubweak DriverIRQHandler for KL28T DMA1 and MCIMX7U5_M4.
[2.0.3]
Bug Fixes
Fixed the incorrect pubweak IRQHandler name issue, which caused re-definition build errors when client set his/her own IRQHandler, by changing the 32-channel IRQHandler name to DriverIRQHandler.
[2.0.2]
Bug Fixes
Fixed incorrect minorLoopBytes type definition in _edma_transfer_config struct, and defined minorLoopBytes as uint32_t instead of uint16_t.
[2.0.1]
Bug Fixes
Fixed the eDMA callback issue (which did not check valid status) in EDMA_HandleIRQ API.
[2.0.0]
Initial version.
EWM
[2.0.3]
Bug Fixes
Fixed violation of MISRA C-2012 rules: 10.1, 10.3.
[2.0.2]
Bug Fixes
Fixed violation of MISRA C-2012 rules: 10.3, 10.4.
[2.0.1]
Bug Fixes
Fixed the hard fault in EWM_Deinit.
[2.0.0]
Initial version.
FLASH
[3.2.0]
New Feature
Basic support for FTFC
[3.1.3]
New Feature
Support 512KB flash for Kinetis E serials.
[3.1.2]
Bug Fixes — Remove redundant comments.
[3.1.1]
Bug Fixes — MISRA C-2012 issue fixed: rule 10.3
[3.1.0]
New Feature
Support erase flash asynchronously.
[3.0.2]
Bug Fixes — MISRA C-2012 issue fixed: rule 8.4, 17.7, 10.4, 16.1, 21.15, 11.3, 10.7 — building warning -Wnull-dereference on arm compiler v6
[3.0.1]
New Features
Added support FlexNVM alias for (kw37/38/39).
[3.0.0]
Improvements
Reorganized FTFx flash driver source file.
Extracted flash cache driver from FTFx driver.
Extracted flexnvm flash driver from FTFx driver.
[2.3.1]
Bug Fixes
Unified Flash IFR design from K3.
New encoding rule for K3 flash size.
[2.3.0]
New Features
Added support for device with LP flash (K3S/G).
Added flash prefetch speculation APIs.
Improvements
Refined flash_cache_clear function.
Reorganized the member of flash_config_t struct.
[2.2.0]
New Features
Supported FTFL device in FLASH_Swap API.
Supported various pflash start addresses.
Added support for KV58 in cache clear function.
Added support for device with secondary flash (KW40).
Bug Fixes
Compiled execute-in-ram functions as PIC binary code for driver use.
Added missed flexram properties.
Fixed unaligned variable issue for execute-in-ram function code array.
[2.1.0]
Improvements
Updated coding style to align with KSDK 2.0.
Different-alignment-size support for pflash and flexnvm.
Improved the implementation of execute-in-ram functions.
[2.0.0]
Initial version
FLEXBUS
[2.1.1]
Bug Fixes
MISRA C-2012 issue fixed: rule 10.3, 10.4, and 14.4.
[2.1.0]
Bug Fixes
Added secondary wait states (SWS), which enabled flag into configuration structure, and updated FLEXBUS_Init() function according to SWS.
Fixed MISRA issues regarding rule 10.1/10.4.
[2.0.2]
Bug Fixes
Removed dissociated chip clearing operation while initializing the FLEXBUS module. Only the associated chip’s register will be cleared.
[2.0.1]
Bug Fixes
Corrected FLEXBUS_Deinit() function to disable clock.
[2.0.0]
Initial version.
FTM
[2.7.1]
Bug Fixes
Added function macro when accsee FLTCTRL register FSTATE bit to prevent access nonexistent register.
Added function macro to prevent access nonexistent FTM channel for API FTM_ConfigSinglePWM() and FTM_ConfigCombinePWM().
[2.7.0]
Improvements
Support period dithering and edge dithering feature with new APIs:
FTM_SetPeriodDithering()
FTM_SetEdgeDithering()
Support get channel n output and input state feature with new APIs:
FTM_GetChannelOutputState()
FTM_GetChannelInputState()
Support configure deadtime for specific combined channel pair with new API:
FTM_SetPairDeadTime()
Support filter clock prescale, fault output state.
Support new APIs to configure PWM and Modified Combine PWM:
FTM_ConfigSinglePWM()
FTM_ConfigCombinePWM()
Support new API to configure channel software output control:
FTM_SetSoftwareOutputCtrl()
FTM_GetSoftwareOutputValue()
FTM_GetSoftwareOutputEnable()
Support new API to update FTM counter initial value, modulo value and chanle value:
FTM_SetInitialModuloValue()
FTM_SetChannelValue()
[2.6.1]
Improvements
Release peripheral from reset if necessary in init function.
[2.6.0]
Improvements
Added support to half and full cycle reload feature with new APIs:
FTM_SetLdok()
FTM_SetHalfCycPeriod()
FTM_LoadFreq()
Bug Fixes
Set the HWRSTCNT and SWRSTCNT bits to optional at initialization.
[2.5.0]
Improvements
Added FTM_CalculateCounterClkDiv to help calculates the counter clock prescaler.
Modify FTM_UpdatePwmDutycycle API to make it return pwm duty cycles status.
Bug Fixes
Fixed TPM_SetupPwm can’t configure 100% center align combined PWM issues.
[2.4.1]
Bug Fixes
Added function macro to determine if FTM instance has only basic features, to prevent access to protected register bits.
[2.4.0]
Improvements
Added CNTIN register initialization in FTM_SetTimerPeriod API.
Added a new API to read the captured value of a FTM channel configured in capture mode:
FTM_GetInputCaptureValue()
[2.3.0]
Improvements
Added support of EdgeAligned/CenterAligned/Asymmetrical combine PWM mode in FTM_SetupPWM() and FTM_SetupPwmMode() APIs.
Remove kFTM_ComplementaryPwm from support PWM mode, and add new parameter “enableComplementary” in structure ftm_chnl_pwm_signal_param_t.
Rename FTM_SetupFault() API to FTM_SetupFaultInput() to avoid ambiguity.
[2.2.3]
Bug Fixes
MISRA C-2012 issue fixed: rule 14.4 and 17.7.
[2.2.2]
Bug Fixes
Fixed the issue that when FTM instance has only TPM features cannot be initialized by FTM_Init() function. By added function macro to assert FTM is TPM only instance.
[2.2.1]
Bug Fixes
MISRA C-2012 issue fixed: rule 10.1, 10.3, 10.4, 10.6, 10.7 and 11.9.
[2.2.0]
Bug Fixes
Fixed the issue of comparison between signed and unsigned integer expressions.
Improvements
Added support of complementary mode in FTM_SetupPWM() and FTM_SetupPwmMode() APIs.
Added new parameter “enableDeadtime” in structure ftm_chnl_pwm_signal_param_t.
[2.1.1]
Bug Fixes
Fixed COVERITY integer handing issue where the right operand of a left bit shift statement should not be a negative value. This appears in FTM_SetReloadPoints().
[2.1.0]
Improvements
Added a new API FTM_SetupPwmMode() to allow the user to set the channel match value in units of timer ticks. New configure structure called ftm_chnl_pwm_config_param_t was added to configure the channel’s PWM parameters. This API is similar with FTM_SetupPwm() API, but the new API will not set the timer period(MOD value), it will be useful for users to set the PWM parameters without changing the timer period.
Bug Fixes
Added feature macro to enable/disable the external trigger source configuration.
[2.0.4]
Improvements
Added a new API to enable DMA transfer:
FTM_EnableDmaTransfer()
[2.0.3]
Bug Fixes
Updated the FTM driver to enable fault input after configuring polarity.
[2.0.2]
Improvements
Added support to Quad Decoder feature with new APIs:
FTM_GetQuadDecoderFlags()
FTM_SetQuadDecoderModuloValue()
FTM_GetQuadDecoderCounterValue()
FTM_ClearQuadDecoderCounterValue()
[2.0.1]
Bug Fixes
Updated the FTM driver to fix write to ELSA and ELSB bits.
FTM combine mode: set the COMBINE bit before writing to CnV register.
[2.0.0]
Initial version.
GPIO
[2.8.2]
Bug Fixes
Fixed COVERITY issue that GPIO_GetInstance could return clock array overflow values due to GPIO base and clock being out of sync.
[2.8.1]
Bug Fixes
Fixed CERT INT31-C issues.
[2.8.0]
Improvements
Add API GPIO_PortInit/GPIO_PortDeinit to set GPIO clock enable and releasing GPIO reset.
[2.8.0]
Improvements
Add API GPIO_PortInit/GPIO_PortDeinit to set GPIO clock enable and releasing GPIO reset.
Remove support for API GPIO_GetPinsDMARequestFlags with GPIO_ISFR_COUNT <= 1.
[2.7.3]
Improvements
Release peripheral from reset if necessary in init function.
[2.7.2]
New Features
Support devices without PORT module.
[2.7.1]
Bug Fixes
Fixed MISRA C-2012 rule 10.4 issues in GPIO_GpioGetInterruptChannelFlags() function and GPIO_GpioClearInterruptChannelFlags() function.
[2.7.0]
New Features
Added API to support Interrupt select (IRQS) bitfield.
[2.6.0]
New Features
Added API to get GPIO version information.
Added API to control a pin for general purpose input.
Added some APIs to control pin in secure and previliege status.
[2.5.3]
Bug Fixes
Correct the feature macro typo: FSL_FEATURE_GPIO_HAS_NO_INDEP_OUTPUT_CONTORL.
[2.5.2]
Improvements
Improved GPIO_PortSet/GPIO_PortClear/GPIO_PortToggle functions to support devices without Set/Clear/Toggle registers.
[2.5.1]
Bug Fixes
Fixed wrong macro definition.
Fixed MISRA C-2012 rule issues in the FGPIO_CheckAttributeBytes() function.
Defined the new macro to separate the scene when the width of registers is different.
Removed some redundant macros.
New Features
Added some APIs to get/clear the interrupt status flag when the port doesn’t control pins’ interrupt.
[2.4.1]
Improvements
Improved GPIO_CheckAttributeBytes() function to support 8 bits width GACR register.
[2.4.0]
Improvements
API interface added:
New APIs were added to configure the GPIO interrupt clear settings.
[2.3.2]
Bug Fixes
Fixed the issue for MISRA-2012 check.
Fixed rule 3.1, 10.1, 8.6, 10.6, and 10.3.
[2.3.1]
Improvements
Removed deprecated APIs.
[2.3.0]
New Features
Updated the driver code to adapt the case of interrupt configurations in GPIO module. New APIs were added to configure the GPIO interrupt settings if the module has this feature on it.
[2.2.1]
Improvements
API interface changes:
Refined naming of APIs while keeping all original APIs by marking them as deprecated. The original APIs will be removed in next release. The main change is updating APIs with prefix of _PinXXX() and _PortXXX.
[2.1.1]
Improvements
API interface changes:
Added an API for the check attribute bytes.
[2.1.0]
Improvements
API interface changes:
Added “pins” or “pin” to some APIs’ names.
Renamed “_PinConfigure” to “GPIO_PinInit”.
I2C
[2.0.10]
Bug Fixes
Fixed coverity issues.
[2.0.9]
Bug Fixes
Fixed the MISRA-2012 violations.
Fixed rule 8.4, 10.1, 10.4, 13.5, 20.8.
[2.0.8]
Bug Fixes
Fixed the bug that DFEN bit of I2C Status register 2 could not be set in I2C_MasterInit.
MISRA C-2012 issue fixed: rule 14.2, 15.7, and 16.4.
Eliminated IAR Pa082 warnings from I2C_MasterTransferDMA and I2C_MasterTransferCallbackDMA by assigning volatile variables to local variables and using local variables instead.
Fixed MISRA issues.
Fixed rules 10.1, 10.3, 10.4, 11.9, 14.4, 15.7, 17.7.
Improvements
Improved timeout mechanism when waiting certain state in transfer API.
Updated the I2C_WAIT_TIMEOUT macro to unified name I2C_RETRY_TIMES.
Moved the master manually acknowledge byte operation into static function I2C_MasterAckByte.
Fixed control/status clean flow issue inside I2C_MasterReadBlocking to avoid potential issue that pending status is cleaned before it’s proceeded.
[2.0.7]
Bug Fixes
Fixed the issue for MISRA-2012 check.
Fixed rule 11.9 ,15.7 ,14.4 ,10.4 ,10.8 ,10.3, 10.1, 10.6, 13.5, 11.3, 13.2, 17.7, 5.7, 8.3, 8.5, 11.1, 16.1.
Fixed Coverity issue of unchecked return value in I2C_RTOS_Transfer.
Fixed variable redefine issue by moving i2cBases from fsl_i2c.h to fsl_i2c.c.
Improvements
Added I2C_MASTER_FACK_CONTROL macro to enable FACK control for master transfer receive flow with IP supporting double buffer, then master could hold the SCL by manually setting TX AK/NAK during data transfer.
[2.0.6]
Bug Fixes
Fixed the issue that I2C Master transfer APIs(blocking/non-blocking) did not support the situation of master transfer with subaddress and transfer data size being zero, which means no data followed by the subaddress.
[2.0.5]
Improvements
Added I2C_WATI_TIMEOUT macro to allow the user to specify the timeout times for waiting flags in functional API and blocking transfer API.
[2.0.4]
Bug Fixes
Added a proper handle for transfer config flag kI2C_TransferNoStartFlag to support transmit with kI2C_TransferNoStartFlag flag. Support write only or write+read with no start flag; does not support read only with no start flag.
[2.0.3]
Bug Fixes
Removed enableHighDrive member in the master/slave configuration structure because the operation to HDRS bit is useless, the user need to use DSE bit in port register to configure the high drive capability.
Added register reset operation in I2C_MasterInit and I2C_SlaveInit APIs. Fixed issue where I2C could not switch between master and slave mode.
Improved slave IRQ handler to handle the corner case that stop flag and address match flag come synchronously.
[2.0.2]
Bug Fixes
Fixed issue in master receive and slave transmit mode with no stop flag. The master could not succeed to start next transfer because the master could not send out re-start signal.
Fixed the out-of-order issue of data transfer due to memory barrier.
Added hold time configuration for slave. By leaving the SCL divider and MULT reset values when configured to slave mode, the setup and hold time of the slave is then reduced outside of spec for lower baudrates. This can cause intermittent arbitration loss on the master side.
New Features
Added address nak event for master.
Added general call event for slave.
[2.0.1]
New Features
Added double buffer enable configuration for SoCs which have the DFEN bit in S2 register.
Added flexible transmit/receive buffer size support in I2C_SlaveHandleIRQ.
Added start flag clear, address match, and release bus operation in I2C_SlaveWrite/ReadBlocking API.
Bug Fixes
Changed the kI2C_SlaveRepeatedStartEvent to kI2C_SlaveStartEvent.
[2.0.0]
Initial version.
LLWU
[2.0.5]
Bug Fixes
Fixed violations of the MISRA C-2012 rules 10.3.
Fixed the issue that function LLWU_SetExternalWakeupPinMode() does not work on 32-bit width platforms.
[2.0.4]
Bug Fixes
Fixed violations of the MISRA C-2012 rules 10.3, 10.4, 10.6, 10.7, 11.3.
Fixed issue that LLWU_ClearExternalWakeupPinFlag may clear other filter flags by mistake on platforms with 32-bit LLWU registers.
[2.0.3]
Bug Fixes
Fixed MISRA-2012 rules.
Rule 16.4.
[2.0.2]
Improvements
Corrected driver function LLWU_SetResetPinMode parameter name.
Bug Fixes
Fixed MISRA-2012 rules.
Rule 14.4, 10.8, 10.4, 10.3.
[2.0.1]
Other Changes
Updates for KL8x.
[2.0.0]
Initial version.
LPTMR
[2.2.0]
Improvements
Updated lptmr_prescaler_clock_select_t, only define the valid options.
[2.1.1]
Improvements
Updated the characters from “PTMR” to “LPTMR” in “FSL_FEATURE_PTMR_HAS_NO_PRESCALER_CLOCK_SOURCE_1_SUPPORT” feature definition.
[2.1.0]
Improvements
Implement for some special devices’ not supporting for all clock sources.
Bug Fixes
Fixed issue when accessing CMR register.
[2.0.2]
Bug Fixes
Fixed MISRA-2012 issues.
Rule 10.1.
[2.0.1]
Improvements
Updated the LPTMR driver to support 32-bit CNR and CMR registers in some devices.
[2.0.0]
Initial version.
LPUART
[2.9.1]
Bug Fixes
Fixed coverity issues.
[2.9.0]
New Feature
Added support for swap TXD and RXD pins.
Added common IRQ handler entry LPUART_DriverIRQHandler.
[2.8.3]
Improvements
Conditionally compile interrupt handling code to solve the problem of using this driver on CPU cores that do not support interrupts.
[2.8.2]
Bug Fix
Fixed the bug that LPUART_TransferEnable16Bit controled by wrong feature macro.
[2.8.1]
Bug Fixes
Fixed issue for MISRA-2012 check.
Fixed rule-5.3, rule-5.8, rule-10.4, rule-11.3, rule-11.8.
[2.8.0]
Improvements
Added support of DATA register for 9bit or 10bit data transmit in write and read API. Such as: LPUART_WriteBlocking16bit, LPUART_ReadBlocking16bit, LPUART_TransferEnable16Bit LPUART_WriteNonBlocking16bit, LPUART_ReadNonBlocking16bit.
[2.7.7]
Bug Fixes
Fixed the bug that baud rate calculation overflow when srcClock_Hz is 528MHz.
[2.7.6]
Bug Fixes
Fixed LPUART_EnableInterrupts and LPUART_DisableInterrupts bug that blocks if the LPUART address doesn’t support exclusive access.
[2.7.5]
Improvements
Release peripheral from reset if necessary in init function.
[2.7.4]
Improvements
Added support for atomic register accessing in LPUART_EnableInterrupts and LPUART_DisableInterrupts.
[2.7.3]
Bug Fixes
Fixed violations of the MISRA C-2012 rules 15.7.
[2.7.2]
Bug Fix
Fixed the bug that the OSR calculation error when lupart init and lpuart set baud rate.
[2.7.1]
Improvements
Added support for LPUART_BASE_PTRS_NS in security mode in file fsl_lpuart.c.
[2.7.0]
Improvements
Split some functions, fixed CCM problem in file fsl_lpuart.c.
[2.6.0]
Bug Fixes
Fixed bug that when there are multiple lpuart instance, unable to support different ISR.
[2.5.3]
Bug Fixes
Fixed comments by replacing unused status flags kLPUART_NoiseErrorInRxDataRegFlag and kLPUART_ParityErrorInRxDataRegFlag with kLPUART_NoiseErrorFlag and kLPUART_ParityErrorFlag.
[2.5.2]
Bug Fixes
Fixed bug that when setting watermark for TX or RX FIFO, the value may exceed the maximum limit.
Improvements
Added check in LPUART_TransferDMAHandleIRQ and LPUART_TransferEdmaHandleIRQ to ensure if user enables any interrupts other than transfer complete interrupt, the dma transfer is not terminated by mistake.
[2.5.1]
Improvements
Use separate data for TX and RX in lpuart_transfer_t.
Bug Fixes
Fixed bug that when ring buffer is used, if some data is received in ring buffer first before calling LPUART_TransferReceiveNonBlocking, the received data count returned by LPUART_TransferGetReceiveCount is wrong.
[2.5.0]
Bug Fixes
Added missing interrupt enable masks kLPUART_Match1InterruptEnable and kLPUART_Match2InterruptEnable.
Fixed bug in LPUART_EnableInterrupts, LPUART_DisableInterrupts and LPUART_GetEnabledInterrupts that the BAUD[LBKDIE] bit field should be soc specific.
Fixed bug in LPUART_TransferHandleIRQ that idle line interrupt should be disabled when rx data size is zero.
Deleted unused status flags kLPUART_NoiseErrorInRxDataRegFlag and kLPUART_ParityErrorInRxDataRegFlag, since firstly their function are the same as kLPUART_NoiseErrorFlag and kLPUART_ParityErrorFlag, secondly to obtain them one data word must be read out thus interfering with the receiving process.
Fixed bug in LPUART_GetStatusFlags that the STAT[LBKDIF], STAT[MA1F] and STAT[MA2F] should be soc specific.
Fixed bug in LPUART_ClearStatusFlags that tx/rx FIFO is reset by mistake when clearing flags.
Fixed bug in LPUART_TransferHandleIRQ that while clearing idle line flag the other bits should be masked in case other status bits be cleared by accident.
Fixed bug of race condition during LPUART transfer using transactional APIs, by disabling and re-enabling the global interrupt before and after critical operations on interrupt enable register.
Fixed DMA/eDMA transfer blocking issue by enabling tx idle interrupt after DMA/eDMA transmission finishes.
New Features
Added APIs LPUART_GetRxFifoCount/LPUART_GetTxFifoCount to get rx/tx FIFO data count.
Added APIs LPUART_SetRxFifoWatermark/LPUART_SetTxFifoWatermark to set rx/tx FIFO water mark.
[2.4.1]
Bug Fixes
Fixed MISRA advisory 17.7 issues.
[2.4.0]
New Features
Added APIs to configure 9-bit data mode, set slave address and send address.
[2.3.1]
Bug Fixes
Fixed MISRA advisory 15.5 issues.
[2.3.0]
Improvements
Modified LPUART_TransferHandleIRQ so that txState will be set to idle only when all data has been sent out to bus.
Modified LPUART_TransferGetSendCount so that this API returns the real byte count that LPUART has sent out rather than the software buffer status.
Added timeout mechanism when waiting for certain states in transfer driver.
[2.2.8]
Bug Fixes
Fixed issue for MISRA-2012 check.
Fixed rule-10.3, rule-14.4, rule-15.5.
Eliminated Pa082 warnings by assigning volatile variables to local variables and using local variables instead.
Fixed MISRA issues.
Fixed rules 10.1, 10.3, 10.4, 10.8, 14.4, 11.6, 17.7.
Improvements
Added check for kLPUART_TransmissionCompleteFlag in LPUART_WriteBlocking, LPUART_TransferHandleIRQ, LPUART_TransferSendDMACallback and LPUART_SendEDMACallback to ensure all the data would be sent out to bus.
Rounded up the calculated sbr value in LPUART_SetBaudRate and LPUART_Init to achieve more acurate baudrate setting. Changed osr from uint32_t to uint8_t since osr’s bigest value is 31.
Modified LPUART_ReadBlocking so that if more than one receiver errors occur, all status flags will be cleared and the most severe error status will be returned.
[2.2.7]
Bug Fixes
Fixed issue for MISRA-2012 check.
Fixed rule-12.1, rule-17.7, rule-14.4, rule-13.3, rule-14.4, rule-10.4, rule-10.8, rule-10.3, rule-10.7, rule-10.1, rule-11.6, rule-13.5, rule-11.3, rule-13.2, rule-8.3.
[2.2.6]
Bug Fixes
Fixed the issue of register’s being in repeated reading status while dealing with the IRQ routine.
[2.2.5]
Bug Fixes
Do not set or clear the TIE/RIE bits when using LPUART_EnableTxDMA and LPUART_EnableRxDMA.
[2.2.4]
Improvements
Added hardware flow control function support.
Added idle-line-detecting feature in LPUART_TransferNonBlocking function. If an idle line is detected, a callback is triggered with status kStatus_LPUART_IdleLineDetected returned. This feature may be useful when the received Bytes is less than the expected received data size. Before triggering the callback, data in the FIFO (if has FIFO) is read out, and no interrupt will be disabled, except for that the receive data size reaches 0.
Enabled the RX FIFO watermark function. With the idle-line-detecting feature enabled, users can set the watermark value to whatever you want (should be less than the RX FIFO size). Data is received and a callback will be triggered when data receive ends.
[2.2.3]
Improvements
Changed parameter type in LPUART_RTOS_Init struct from rtos_lpuart_config to lpuart_rtos_config_t.
Bug Fixes
Disabled LPUART receive interrupt instead of all NVICs when reading data from ring buffer. Otherwise when the ring buffer is used, receive nonblocking method will disable all NVICs to protect the ring buffer. This may has a negative effect on other IPs that are using the interrupt.
[2.2.2]
Improvements
Added software reset feature support.
Added software reset API in LPUART_Init.
[2.2.1]
Improvements
Added separate RX/TX IRQ number support.
[2.2.0]
Improvements
Added support of 7 data bits and MSB.
[2.1.1]
Improvements
Removed unnecessary check of event flags and assert in LPUART_RTOS_Receive.
Added code to always wait for RX event flag in LPUART_RTOS_Receive.
[2.1.0]
Improvements
Update transactional APIs.
LPUART_EDMA
[2.4.0]
Refer LPUART driver change log 2.1.0 to 2.4.0
MCM
[2.2.0]
Improvements
Support platforms with less features.
[2.1.0]
Others
Remove byteID from mcm_lmem_fault_attribute_t for document update.
[2.0.0]
Initial version.
PDB
[2.0.4]
Bug Fixes
Fixed violations of MISRA C-2012 rule 10.1 and 10.4.
[2.0.3]
Bug Fixes
Fixed violations of MISRA C-2012 rule 17.7.
[2.0.2]
Improvement:
Used macros in feature file instead of that in IO map.
[2.0.1]
Changed PDB register base array to const.
[2.0.0]
Initial version.
PIT
[2.1.1]
Bug Fixes
Enable PIT when using RTI to ensure RTI can work properly in debug mode.
Improvements
Added status check in PIT_SetRtiTimerPeriod to ensure the load value is synchronized into the RTI clock domain.
Added note for PIT_RTI_Init to remind users wait RTI sync.
[2.1.0]
New Features
Support RTI (Real Time Interrupt) timer.
[2.0.5]
Improvements
Support workaround for ERR007914. This workaround guarantee the write to MCR register is not ignored.
[2.0.4]
Bug Fixes
Fixed PIT_SetTimerPeriod implementation, the load value trigger should be PIT clock cycles minus 1.
[2.0.3]
Bug Fixes
Clear all status bits for all channels to make sure the status of all TCTRL registers is clean.
[2.0.2]
Bug Fixes
Fixed MISRA-2012 issues.
Rule 10.1.
[2.0.1]
Bug Fixes
Cleared timer enable bit for all channels in function PIT_Init() to make sure all channels stay in disable status before setting other configurations.
Fixed MISRA-2012 rules.
Rule 14.4, rule 10.4.
[2.0.0]
Initial version.
PMC
[2.0.3]
Bug Fixes
Fixed the violation of MISRA C-2012 rule 11.3.
[2.0.2]
Bug Fixes
Fixed the violations of MISRA 2012 rules:
Rule 10.3.
[2.0.1]
Bug Fixes
Fixed MISRA issues.
Rule 10.8, Rule 10.3.
[2.0.0]
Initial version.
PORT
[2.5.1]
Bug Fixes
Fix CERT INT31-C issues.
[2.5.0]
Bug Fixes
Correct the kPORT_MuxAsGpio for some platforms.
[2.4.1]
Bug Fixes
Fixed the violations of MISRA C-2012 rules: 10.1, 10.8 and 14.4.
[2.4.0]
New Features
Updated port_pin_config_t to support input buffer and input invert.
[2.3.0]
New Features
Added new APIs for Electrical Fast Transient(EFT) detect.
Added new API to configure port voltage range.
[2.2.0]
New Features
Added new api PORT_EnablePinDoubleDriveStrength.
[2.1.1]
Bug Fixes
Fixed the violations of MISRA C-2012 rules: 10.1, 10.4,11.3,11.8, 14.4.
[2.1.0]
New Features
Updated the driver code to adapt the case of the interrupt configurations in GPIO module. Will move the pin configuration APIs to GPIO module.
[2.0.2]
Other Changes
Added feature guard macros in the driver.
[2.0.1]
Other Changes
Added “const” in function parameter.
Updated some enumeration variables’ names.
RCM
[2.0.4]
Bug Fixes
Fixed violation of MISRA C-2012 rule 10.3
[2.0.3]
Bug Fixes
Fixed violation of MISRA C-2012 rules.
[2.0.2]
Bug Fixes
Fixed MISRA issue.
Rule 10.8, rule 10.1, rule 13.2, rule 3.1.
[2.0.1]
Bug Fixes
Fixed kRCM_SourceSw bit shift issue.
[2.0.0]
Initial version.
RNGA
[2.0.2]
Bug fix:
Fix MISRA issue.
[2.0.1]
Bug fix:
Fixed C++ build warning in RNGA driver.
[2.0.0]
Initial version.
RTC
[2.3.0]
Improvements
Added API RTC_EnableLPOClock to set 1kHz LPO clock.
Added API RTC_EnableCrystalClock to replace API RTC_SetClockSource.
[2.2.2]
Improvements
Refine _rtc_interrupt_enable order.
[2.2.1]
Bug Fixes
Fixed the issue of Pa082 warning.
Fixed the issue of bit field mask checking.
Fixed the issue of hard code in RTC_Init.
[2.2.0]
Bug Fixes
Fixed MISRA C-2012 issue.
Fixed rule contain: rule-17.7, rule-14.4, rule-10.4, rule-10.7, rule-10.1, rule-10.3.
Fixed central repository code formatting issue.
Improvements
Added an API for enabling wakeup pin.
[2.1.0]
Improvements
Added feature macro check for many features.
[2.0.0]
Initial version.
SAI
[2.4.5]
Bug Fixes
Fixed violations of MISRA C-2012 rule 10.1, 10.3, 10.4, 10.5, 10.6, 10.7, 10.8, 12.4.
[2.4.4]
Bug Fixes
Fixed enumeration sai_fifo_combine_t - add RX configuration.
[2.4.3]
Bug Fixes
Fixed enumeration sai_fifo_combine_t value configuration issue.
[2.4.2]
Improvements
Release peripheral from reset if necessary in init function.
[2.4.1]
Bug Fixes
Fixed bitWidth incorrectly assigned issue.
[2.4.0]
Improvements
Removed deprecated APIs.
[2.3.8]
Bug Fixes
Fixed violations of MISRA C-2012 rule 10.4.
[2.3.7]
Improvements
Change feature “FSL_FEATURE_SAI_FIFO_COUNT” to “FSL_FEATURE_SAI_HAS_FIFO”.
Added feature “FSL_FEATURE_SAI_FIFO_COUNTn(x)” to align SAI fifo count function with IP in function
[2.3.6]
Bug Fixes
Fixed violations of MISRA C-2012 rule 5.6.
[2.3.5]
Improvements
Make driver to be aarch64 compatible.
[2.3.4]
Bug Fixes
Corrected the fifo combine feature macro used in driver.
[2.3.3]
Bug Fixes
Added bit clock polarity configuration when sai act as slave.
Fixed out of bound access coverity issue.
Fixed violations of MISRA C-2012 rule 10.3, 10.4.
[2.3.2]
Bug Fixes
Corrected the frame sync configuration when sai act as slave.
[2.3.1]
Bug Fixes
Corrected the peripheral name in function SAI0_DriverIRQHandler.
Fixed violations of MISRA C-2012 rule 17.7.
[2.3.0]
Bug Fixes
Fixed the build error caused by the SOC has no fifo feature.
[2.2.3]
Bug Fixes
Corrected the peripheral name in function SAI0_DriverIRQHandler.
[2.2.2]
Bug Fixes
Fixed the issue of MISRA 2004 rule 9.3.
Fixed sign-compare warning.
Fixed the PA082 build warning.
Fixed sign-compare warning.
Fixed violations of MISRA C-2012 rule 10.3,17.7,10.4,8.4,10.7,10.8,14.4,17.7,11.6,10.1,10.6,8.4,14.3,16.4,18.4.
Allow to reset Rx or Tx FIFO pointers only when Rx or Tx is disabled.
Improvements
Added 24bit raw audio data width support in sai sdma driver.
Disabled the interrupt/DMA request in the SAI_Init to avoid generates unexpected sai FIFO requests.
[2.2.1]
Improvements
Added mclk post divider support in function SAI_SetMasterClockDivider.
Removed useless configuration code in SAI_RxSetSerialDataConfig.
Bug Fixes
Fixed the SAI SDMA driver build issue caused by the wrong structure member name used in the function SAI_TransferRxSetConfigSDMA/SAI_TransferTxSetConfigSDMA.
Fixed BAD BIT SHIFT OPERATION issue caused by the FSL_FEATURE_SAI_CHANNEL_COUNTn.
Applied ERR05144: not set FCONT = 1 when TMR > 0, otherwise the TX may not work.
[2.2.0]
Improvements
Added new APIs for parameters collection and simplified user interfaces:
SAI_Init
SAI_SetMasterClockConfig
SAI_TxSetBitClockRate
SAI_TxSetSerialDataConfig
SAI_TxSetFrameSyncConfig
SAI_TxSetFifoConfig
SAI_TxSetBitclockConfig
SAI_TxSetConfig
SAI_TxSetTransferConfig
SAI_RxSetBitClockRate
SAI_RxSetSerialDataConfig
SAI_RxSetFrameSyncConfig
SAI_RxSetFifoConfig
SAI_RxSetBitclockConfig
SAI_RXSetConfig
SAI_RxSetTransferConfig
SAI_GetClassicI2SConfig
SAI_GetLeftJustifiedConfig
SAI_GetRightJustifiedConfig
SAI_GetTDMConfig
[2.1.9]
Improvements
Improved SAI driver comment for clock polarity.
Added enumeration for SAI for sample inputs on different edges.
Changed FSL_FEATURE_SAI_CHANNEL_COUNT to FSL_FEATURE_SAI_CHANNEL_COUNTn(base) for the difference between the different SAI instances.
Added new APIs:
SAI_TxSetBitClockDirection
SAI_RxSetBitClockDirection
SAI_RxSetFrameSyncDirection
SAI_TxSetFrameSyncDirection
[2.1.8]
Improvements
Added feature macro test for the sync mode2 and mode 3.
Added feature macro test for masterClockHz in sai_transfer_format_t.
[2.1.7]
Improvements
Added feature macro test for the mclkSource member in sai_config_t.
Changed “FSL_FEATURE_SAI5_SAI6_SHARE_IRQ” to “FSL_FEATURE_SAI_SAI5_SAI6_SHARE_IRQ”.
Added #ifndef #endif check for SAI_XFER_QUEUE_SIZE to allow redefinition.
Bug Fixes
Fixed build error caused by feature macro test for mclkSource.
[2.1.6]
Improvements
Added feature macro test for mclkSourceClockHz check.
Added bit clock source name for general devices.
Bug Fixes
Fixed incorrect channel numbers setting while calling RX/TX set format together.
[2.1.5]
Bug Fixes
Corrected SAI3 driver IRQ handler name.
Added I2S4/5/6 IRQ handler.
Added base in handler structure to support different instances sharing one IRQ number.
New Features
Updated SAI driver for MCR bit MICS.
Added 192 KHZ/384 KHZ in the sample rate enumeration.
Added multi FIFO interrupt/SDMA transfer support for TX/RX.
Added an API to read/write multi FIFO data in a blocking method.
Added bclk bypass support when bclk is same with mclk.
[2.1.4]
New Features
Added an API to enable/disable auto FIFO error recovery in platforms that support this feature.
Added an API to set data packing feature in platforms which support this feature.
[2.1.3]
New Features
Added feature to make I2S frame sync length configurable according to bitWidth.
[2.1.2]
Bug Fixes
Added 24-bit support for SAI eDMA transfer. All data shall be 32 bits for send/receive, as eDMA cannot directly handle 3-Byte transfer.
[2.1.1]
Improvements
Reduced code size while not using transactional API.
[2.1.0]
Improvements
API name changes:
SAI_GetSendRemainingBytes -> SAI_GetSentCount.
SAI_GetReceiveRemainingBytes -> SAI_GetReceivedCount.
All names of transactional APIs were added with “Transfer” prefix.
All transactional APIs use base and handle as input parameter.
Unified the parameter names.
Bug Fixes
Fixed WLC bug while reading TCSR/RCSR registers.
Fixed MOE enable flow issue. Moved MOE enable after MICS settings in SAI_TxInit/SAI_RxInit.
[2.0.0]
Initial version.
SAI_EDMA
[2.7.3]
Bug Fixes
Fixed violations of MISRA C-2012 rule 10.1, 10.3, 10.4, 10.5, 10.6, 10.7, 10.8, 12.4.
[2.7.2]
Improvements
Add macros MCUX_SDK_SAI_EDMA_TX_ENABLE_INTERNAL and MCUX_SDK_SAI_EDMA_RX_ENABLE_INTERNAL to let the user decide whether to enable SAI when calling SAI_TransferSendEDMA/SAI_TransferReceiveEDMA.
[2.7.1]
Improvements
Add EDMA ext API to accommodate more types of EDMA.
[2.7.0]
Improvements
Updated api SAI_TransferReceiveEDMA to support voice channel block interleave transfer.
Updated api SAI_TransferSendEDMA to support voice channel block interleave transfer.
Added new api SAI_TransferSetInterleaveType to support channel interleave type configurations.
[2.6.0]
Improvements
Removed deprecated APIs.
[2.5.1]
Bug Fixes
Fixed violations of MISRA C-2012 rule 20.7.
[2.5.0]
Improvements
Added new api SAI_TransferSendLoopEDMA/SAI_TransferReceiveLoopEDMA to support loop transfer.
Added multi sai channel transfer support.
[2.4.0]
Improvements
Added new api SAI_TransferGetValidTransferSlotsEDMA which can be used to get valid transfer slot count in the sai edma transfer queue.
Deprecated the api SAI_TransferRxSetFormatEDMA and SAI_TransferTxSetFormatEDMA.
Bug Fixes
Fixed violations of MISRA C-2012 rule 10.3,10.4.
[2.3.2]
Refer SAI driver change log 2.1.0 to 2.3.2
SIM
[2.2.0]
Improvements
Added API to trigger TRGMUX.
[2.1.3]
Improvements
Updated function SIM_GetUniqueId to support different register names.
[2.1.2]
Bug Fixes
Fixed SIM_GetUniqueId bug that could not get UIDH.
[2.1.1]
Bug Fixes
Fixed violations of the MISRA C-2012 rules 10.1, 10.4
[2.1.0]
Improvements
Added new APIs: SIM_GetRfAddr() and SIM_EnableSystickClock().
[2.0.0]
Initial version.
SMC
[2.0.7]
Bug Fixes
Fixed MISRA-2012 issue 10.3.
[2.0.6]
Bug Fixes
Fixed issue for MISRA-2012 check.
Fixed rule 10.3, rule 11.3.
[2.0.5]
Bug Fixes
Fixed issue for MISRA-2012 check.
Fixed rule 15.7, rule 14.4, rule 10.3, rule 10.1, rule 10.4.
[2.0.4]
Bug Fixes
When entering stop modes, used RAM function for the flash synchronization issue. Application should make sure that, the RW data of fsl_smc.c is located in memory region which is not powered off in stop modes.
[2.0.3]
Improvements
Added APIs SMC_PreEnterStopModes, SMC_PreEnterWaitModes, SMC_PostExitWaitModes, and SMC_PostExitStopModes.
[2.0.2]
Bug Fixes
Added DSB before WFI while ISB after WFI.
Other Changes
Updated SMC_SetPowerModeVlpw implementation.
[2.0.1]
Other Changes
Updated for KL8x.
[2.0.0]
Initial version.
UART
[2.5.1]
Improvements
Use separate data for TX and RX in uart_transfer_t.
Bug Fixes
Fixed bug that when ring buffer is used, if some data is received in ring buffer first before calling UART_TransferReceiveNonBlocking, the received data count returned by UART_TransferGetReceiveCount is wrong.
[2.5.0]
New Features
Added APIs UART_GetRxFifoCount/UART_GetTxFifoCount to get rx/tx FIFO data count.
Added APIs UART_SetRxFifoWatermark/UART_SetTxFifoWatermark to set rx/tx FIFO water mark.
Bug Fixes
Fixed bug of race condition during UART transfer using transactional APIs, by disabling and re-enabling the global interrupt before and after critical operations on interrupt enable registers.
Fixed DMA/eDMA transfer blocking issue by enabling tx idle interrupt after DMA/eDMA transmission finishes.
[2.4.0]
New Features
Added APIs to configure 9-bit data mode, set slave address and send address.
[2.3.0]
Bug Fixes
Fixed the bug that, when framing/parity/noise/overflow flag or idle line detect flag is set, receive FIFO should be flushed to avoid FIFO pointer being in unknown state, since FIFO has no valid data.
Improvements
Modified UART_TransferHandleIRQ so that txState will be set to idle only when all data has been sent out to bus.
Modified UART_TransferGetSendCount so that this API returns the real byte count that UART has sent out rather than the software buffer status.
Added timeout mechanism when waiting for certain states in transfer driver.
[2.2.0]
New Features
Added UART hardware FIFO enable/disable API.
Improvements
Added check for kUART_TransmissionCompleteFlag in UART_TransferHandleIRQ, UART_SendEDMACallback and UART_TransferSendDMACallback to ensure all the data would be sent out to bus.
Bug Fixes
Eliminated IAR Pa082 warnings from UART_TransferGetRxRingBufferLength, UART_GetEnabledInterrupts, UART_GetStatusFlags and UART_TransferHandleIRQ.
Added code in UART_ReadBlocking so that if more than one receiver errors occur, all status flags will be cleared and the most severe error status will be returned.
Fixed MISRA issues.
Fixed rules 10.1, 10.3, 10.4, 14.4, 11.6, 17.7.
[2.1.6]
Bug Fixes
Fixed the issue of register’s being in repeatedly reading status while performing the IRQ routine.
[2.1.5]
Improvements
Added hardware flow control function support.
Added idle-line-detecting feature in UART_TransferNonBlocking function. If an idle line is detected, a callback will be triggered with status kStatus_UART_IdleLineDetected returned. This feature may be useful when the number of received bytes is less than the expected receive data size. Before triggering the callback, data in the FIFO is read out (if it has FIFO), and no interrupt will be disabled except for the case that the receive data size reaches 0.
Enabled the RX FIFO watermark function. With the idle-line-detecting feature enabled, you can set the watermark value to whatever you want (should not be bigger than the RX FIFO size). Data is then received and a callback will be triggered when data receive ends.
[2.1.4]
Improvements
Changed parameter type in UART_RTOS_Init() struct rtos_uart_config –> uart_rtos_config_t.
Bug Fixes
Disabled UART receive interrupt instead of global interrupt when reading data from ring buffer. With ring buffer used, receive nonblocking will disable global interrupt to protect the ring buffer. This has a negative effect on other IPs using interrupt.
[2.1.3]
New Features
Added RX framing error and parity error status check when using interrupt transfer.
[2.1.2]
Bug Fixes
Fixed baud rate fine adjust bug to make the computed baud rate more accurate.
[2.1.1]
Bug Fixes
Removed needless check of event flags and assert in UART_RTOS_Receive.
Always waited for RX event flag in UART_RTOS_Receive.
[2.1.0]
Improvements
Added transactional API.
[2.0.0]
Initial version.
UART_EDMA
[2.5.2]
Bug Fixes
Fixed violations of the MISRA C-2012 rules.
[2.5.1]
Bug Fixes
Fixed violations of the MISRA C-2012 rules.
[2.5.0]
Refer UART driver change log 2.1.0 to 2.5.0
VREF
[2.1.2]
Bug Fixes
Fixed the violation of MISRA-2012 rule 10.3.
Fixed MISRA C-2012 rule 10.3, rule 10.4 violation.
[2.1.1]
Bug Fixes
MISRA-2012 issue fixed.
Fixed rules containing: rule-10.4, rule-10.3, rule-10.1.
[2.1.0]
Improvements
Added new functions to support L5K board: added VREF_SetTrim2V1Val() and VREF_GetTrim2V1Val() functions to supply 2V1 output mode.
[2.0.0]
Initial version.
WDOG
[2.0.2]
Improvements
WDG_Init() adds a 256 bus clock delay for WCT window finish.
[2.0.1]
Bug Fixes
MISRA C-2012 issue fixed: rule 10.3, 10.4, 10.6, 10.7 11.9 and 17.7.
[2.0.0]
Initial version.