MCUXpresso SDK Changelog


ACMP

[2.3.0]

  • Improvements

    • Expose C0 register FILTER_CNT bitfield and FPR bitfield to the user.

[2.2.0]

  • Improvements

    • Updated feature macros for roundrobin mode, window mode, filter mode, and 3V domain removes.

[2.1.0]

  • New Feature

    • Supported the plateforms which don’t have hysteresis mode.

[2.0.6]

  • Bug Fixes

    • Fixed the wrong comments, the DAC value should range from 0 to 255.

[2.0.5]

  • Bug Fixes

    • Fixed the out-of-bounds error of Coverity caused by missing an assert sentence to avoid the return value of ACMP_GetInstance() exceeding the array bounds.

    • Fixed the violations of MISRA C-2012 rules:

      • Rule 10.1, 14.4, 16.4, 17.7.

[2.0.4]

  • Bug Fixes

    • Avoided changing w1c bit in ACMP_SetRoundRobinPreState().

[2.0.3]

  • New Features

    • Added feature functions for usage of different power domains(1.8 V and 3 V). These functions are first enabled in ULP1. They are about:

      • ACMP_EnableLinkToDAC()

      • ACMP_SetDiscreteModeConfig()

      • ACMP_GetDefaultDiscreteModeConfig()

[2.0.2]

  • Other Changes

    • Changed coding style of peripheral base address from “s_acmpBases” to “s_acmpBase”.

[2.0.1]

  • Bug Fixes

    • Fixed bug regarding the function “ACMP_SetRoundRobinConfig”. It will not continue execution but returns directly after disabling round robin mode.


ADC12

[2.0.7]

  • Improvements

    • Change the method for judging the end of calibration. Previously, it was judged based on the COCO bit of the SC1 register. After the update, it is judged based on the CAL bit of the SC3 register. In some cases, SC1[COCO] was already set to 1 before calibration was performed, which caused calibration to fail.

[2.0.6]

  • Improvements

    • Removed useless comments of ADC12_DoAutoCalibration() function.

[2.0.5]

  • Bug Fixes

    • Fixed the violations of MISRA C-2012 rule 10.4.

[2.0.4]

  • Bug Fixes

    • Fixed the violations of MISRA C-2012 rules:

      • Rule 4.7 10.1 10.3 10.4 10.8 12.2 16.4 17.7

[2.0.3]

  • Improvements

    • Used conversion control feature macro instead of that in IO map.

[2.0.2]

  • Bug Fixes

    • Set ADC clock frequency as half of the maximum value for calibration.

[2.0.1]

  • New Features

    • Added a feature to control enablement of DMA.

[2.0.0]

  • Initial version.


CLOCK

[2.3.0]

  • Bug Fixes

    • Removed unimplemented kSCG_AsyncDiv1Clk.

[2.2.1]

  • Bug Fixes

    • Fixed MISRA C-2012 rule 10.1, rule 10.4, rule 10.8 and so on.

[2.2.0]

  • New Features

    • Moved SDK_DelayAtLeastUs function from clock driver to common driver.

[2.1.0]

  • New Features

    • Added new API CLOCK_DelayAtLeastUs() implemented by DWT to allow users set delay in unit of microsecond.

[2.0.0]

  • Initial version.


COMMON

[2.6.0]

  • Bug Fixes

    • Fix CERT-C violations.

[2.5.0]

  • New Features

    • Added new APIs InitCriticalSectionMeasurementContext, DisableGlobalIRQEx and EnableGlobalIRQEx so that user can measure the execution time of the protected sections.

[2.4.3]

  • Improvements

    • Enable irqs that mount under irqsteer interrupt extender.

[2.4.2]

  • Improvements

    • Add the macros to convert peripheral address to secure address or non-secure address.

[2.4.1]

  • Improvements

    • Improve for the macro redefinition error when integrated with zephyr.

[2.4.0]

  • New Features

    • Added EnableIRQWithPriority, IRQ_SetPriority, and IRQ_ClearPendingIRQ for ARM.

    • Added MSDK_EnableCpuCycleCounter, MSDK_GetCpuCycleCount for ARM.

[2.3.3]

  • New Features

    • Added NETC into status group.

[2.3.2]

  • Improvements

    • Make driver aarch64 compatible

[2.3.1]

  • Bug Fixes

    • Fixed MAKE_VERSION overflow on 16-bit platforms.

[2.3.0]

  • Improvements

    • Split the driver to common part and CPU architecture related part.

[2.2.10]

  • Bug Fixes

    • Fixed the ATOMIC macros build error in cpp files.

[2.2.9]

  • Bug Fixes

    • Fixed MISRA C-2012 issue, 5.6, 5.8, 8.4, 8.5, 8.6, 10.1, 10.4, 17.7, 21.3.

    • Fixed SDK_Malloc issue that not allocate memory with required size.

[2.2.8]

  • Improvements

    • Included stddef.h header file for MDK tool chain.

  • New Features:

    • Added atomic modification macros.

[2.2.7]

  • Other Change

    • Added MECC status group definition.

[2.2.6]

  • Other Change

    • Added more status group definition.

  • Bug Fixes

    • Undef __VECTOR_TABLE to avoid duplicate definition in cmsis_clang.h

[2.2.5]

  • Bug Fixes

    • Fixed MISRA C-2012 rule-15.5.

[2.2.4]

  • Bug Fixes

    • Fixed MISRA C-2012 rule-10.4.

[2.2.3]

  • New Features

    • Provided better accuracy of SDK_DelayAtLeastUs with DWT, use macro SDK_DELAY_USE_DWT to enable this feature.

    • Modified the Cortex-M7 delay count divisor based on latest tests on RT series boards, this setting lets result be closer to actual delay time.

[2.2.2]

  • New Features

    • Added include RTE_Components.h for CMSIS pack RTE.

[2.2.1]

  • Bug Fixes

    • Fixed violation of MISRA C-2012 Rule 3.1, 10.1, 10.3, 10.4, 11.6, 11.9.

[2.2.0]

  • New Features

    • Moved SDK_DelayAtLeastUs function from clock driver to common driver.

[2.1.4]

  • New Features

    • Added OTFAD into status group.

[2.1.3]

  • Bug Fixes

    • MISRA C-2012 issue fixed.

      • Fixed the rule: rule-10.3.

[2.1.2]

  • Improvements

    • Add SUPPRESS_FALL_THROUGH_WARNING() macro for the usage of suppressing fallthrough warning.

[2.1.1]

  • Bug Fixes

    • Deleted and optimized repeated macro.

[2.1.0]

  • New Features

    • Added IRQ operation for XCC toolchain.

    • Added group IDs for newly supported drivers.

[2.0.2]

  • Bug Fixes

    • MISRA C-2012 issue fixed.

      • Fixed the rule: rule-10.4.

[2.0.1]

  • Improvements

    • Removed the implementation of LPC8XX Enable/DisableDeepSleepIRQ() function.

    • Added new feature macro switch “FSL_FEATURE_HAS_NO_NONCACHEABLE_SECTION” for specific SoCs which have no noncacheable sections, that helps avoid an unnecessary complex in link file and the startup file.

    • Updated the align(x) to attribute(aligned(x)) to support MDK v6 armclang compiler.

[2.0.0]

  • Initial version.


CRC

[2.0.4]

  • Improvements

    • Release peripheral from reset if necessary in init function.

[2.0.3]

  • Bug fix:

    • Fix MISRA issues.

[2.0.2]

  • Bug fix:

    • Fix MISRA issues.

[2.0.1]

  • Bug fix:

    • DATA and DATALL macro definition moved from header file to source file.

[2.0.0]

  • Initial version.


EWM

[2.0.3]

  • Bug Fixes

    • Fixed violation of MISRA C-2012 rules: 10.1, 10.3.

[2.0.2]

  • Bug Fixes

    • Fixed violation of MISRA C-2012 rules: 10.3, 10.4.

[2.0.1]

  • Bug Fixes

    • Fixed the hard fault in EWM_Deinit.

[2.0.0]

  • Initial version.


FLASH

[3.2.0]

  • New Feature

    • Basic support for FTFC

[3.1.3]

  • New Feature

    • Support 512KB flash for Kinetis E serials.

[3.1.2]

  • Bug Fixes — Remove redundant comments.

[3.1.1]

  • Bug Fixes — MISRA C-2012 issue fixed: rule 10.3

[3.1.0]

  • New Feature

    • Support erase flash asynchronously.

[3.0.2]

  • Bug Fixes — MISRA C-2012 issue fixed: rule 8.4, 17.7, 10.4, 16.1, 21.15, 11.3, 10.7 — building warning -Wnull-dereference on arm compiler v6

[3.0.1]

  • New Features

    • Added support FlexNVM alias for (kw37/38/39).

[3.0.0]

  • Improvements

    • Reorganized FTFx flash driver source file.

    • Extracted flash cache driver from FTFx driver.

    • Extracted flexnvm flash driver from FTFx driver.

[2.3.1]

  • Bug Fixes

    • Unified Flash IFR design from K3.

    • New encoding rule for K3 flash size.

[2.3.0]

  • New Features

    • Added support for device with LP flash (K3S/G).

    • Added flash prefetch speculation APIs.

  • Improvements

    • Refined flash_cache_clear function.

    • Reorganized the member of flash_config_t struct.

[2.2.0]

  • New Features

    • Supported FTFL device in FLASH_Swap API.

    • Supported various pflash start addresses.

    • Added support for KV58 in cache clear function.

    • Added support for device with secondary flash (KW40).

  • Bug Fixes

    • Compiled execute-in-ram functions as PIC binary code for driver use.

    • Added missed flexram properties.

    • Fixed unaligned variable issue for execute-in-ram function code array.

[2.1.0]

  • Improvements

    • Updated coding style to align with KSDK 2.0.

    • Different-alignment-size support for pflash and flexnvm.

    • Improved the implementation of execute-in-ram functions.

[2.0.0]

  • Initial version


FTM

[2.7.1]

  • Bug Fixes

    • Added function macro when accsee FLTCTRL register FSTATE bit to prevent access nonexistent register.

    • Added function macro to prevent access nonexistent FTM channel for API FTM_ConfigSinglePWM() and FTM_ConfigCombinePWM().

[2.7.0]

  • Improvements

    • Support period dithering and edge dithering feature with new APIs:

      • FTM_SetPeriodDithering()

      • FTM_SetEdgeDithering()

    • Support get channel n output and input state feature with new APIs:

      • FTM_GetChannelOutputState()

      • FTM_GetChannelInputState()

    • Support configure deadtime for specific combined channel pair with new API:

      • FTM_SetPairDeadTime()

    • Support filter clock prescale, fault output state.

    • Support new APIs to configure PWM and Modified Combine PWM:

      • FTM_ConfigSinglePWM()

      • FTM_ConfigCombinePWM()

    • Support new API to configure channel software output control:

      • FTM_SetSoftwareOutputCtrl()

      • FTM_GetSoftwareOutputValue()

      • FTM_GetSoftwareOutputEnable()

    • Support new API to update FTM counter initial value, modulo value and chanle value:

      • FTM_SetInitialModuloValue()

      • FTM_SetChannelValue()

[2.6.1]

  • Improvements

    • Release peripheral from reset if necessary in init function.

[2.6.0]

  • Improvements

    • Added support to half and full cycle reload feature with new APIs:

      • FTM_SetLdok()

      • FTM_SetHalfCycPeriod()

      • FTM_LoadFreq()

  • Bug Fixes

    • Set the HWRSTCNT and SWRSTCNT bits to optional at initialization.

[2.5.0]

  • Improvements

    • Added FTM_CalculateCounterClkDiv to help calculates the counter clock prescaler.

    • Modify FTM_UpdatePwmDutycycle API to make it return pwm duty cycles status.

  • Bug Fixes

    • Fixed TPM_SetupPwm can’t configure 100% center align combined PWM issues.

[2.4.1]

  • Bug Fixes

    • Added function macro to determine if FTM instance has only basic features, to prevent access to protected register bits.

[2.4.0]

  • Improvements

    • Added CNTIN register initialization in FTM_SetTimerPeriod API.

    • Added a new API to read the captured value of a FTM channel configured in capture mode:

      • FTM_GetInputCaptureValue()

[2.3.0]

  • Improvements

    • Added support of EdgeAligned/CenterAligned/Asymmetrical combine PWM mode in FTM_SetupPWM() and FTM_SetupPwmMode() APIs.

    • Remove kFTM_ComplementaryPwm from support PWM mode, and add new parameter “enableComplementary” in structure ftm_chnl_pwm_signal_param_t.

    • Rename FTM_SetupFault() API to FTM_SetupFaultInput() to avoid ambiguity.

[2.2.3]

  • Bug Fixes

    • MISRA C-2012 issue fixed: rule 14.4 and 17.7.

[2.2.2]

  • Bug Fixes

    • Fixed the issue that when FTM instance has only TPM features cannot be initialized by FTM_Init() function. By added function macro to assert FTM is TPM only instance.

[2.2.1]

  • Bug Fixes

    • MISRA C-2012 issue fixed: rule 10.1, 10.3, 10.4, 10.6, 10.7 and 11.9.

[2.2.0]

  • Bug Fixes

    • Fixed the issue of comparison between signed and unsigned integer expressions.

  • Improvements

    • Added support of complementary mode in FTM_SetupPWM() and FTM_SetupPwmMode() APIs.

    • Added new parameter “enableDeadtime” in structure ftm_chnl_pwm_signal_param_t.

[2.1.1]

  • Bug Fixes

    • Fixed COVERITY integer handing issue where the right operand of a left bit shift statement should not be a negative value. This appears in FTM_SetReloadPoints().

[2.1.0]

  • Improvements

    • Added a new API FTM_SetupPwmMode() to allow the user to set the channel match value in units of timer ticks. New configure structure called ftm_chnl_pwm_config_param_t was added to configure the channel’s PWM parameters. This API is similar with FTM_SetupPwm() API, but the new API will not set the timer period(MOD value), it will be useful for users to set the PWM parameters without changing the timer period.

  • Bug Fixes

    • Added feature macro to enable/disable the external trigger source configuration.

[2.0.4]

  • Improvements

    • Added a new API to enable DMA transfer:

      • FTM_EnableDmaTransfer()

[2.0.3]

  • Bug Fixes

    • Updated the FTM driver to enable fault input after configuring polarity.

[2.0.2]

  • Improvements

    • Added support to Quad Decoder feature with new APIs:

      • FTM_GetQuadDecoderFlags()

      • FTM_SetQuadDecoderModuloValue()

      • FTM_GetQuadDecoderCounterValue()

      • FTM_ClearQuadDecoderCounterValue()

[2.0.1]

  • Bug Fixes

    • Updated the FTM driver to fix write to ELSA and ELSB bits.

    • FTM combine mode: set the COMBINE bit before writing to CnV register.

[2.0.0]

  • Initial version.


GPIO

[2.8.2]

  • Bug Fixes

    • Fixed COVERITY issue that GPIO_GetInstance could return clock array overflow values ​​due to GPIO base and clock being out of sync.

[2.8.1]

  • Bug Fixes

    • Fixed CERT INT31-C issues.

[2.8.0]

  • Improvements

    • Add API GPIO_PortInit/GPIO_PortDeinit to set GPIO clock enable and releasing GPIO reset.

[2.8.0]

  • Improvements

    • Add API GPIO_PortInit/GPIO_PortDeinit to set GPIO clock enable and releasing GPIO reset.

    • Remove support for API GPIO_GetPinsDMARequestFlags with GPIO_ISFR_COUNT <= 1.

[2.7.3]

  • Improvements

    • Release peripheral from reset if necessary in init function.

[2.7.2]

  • New Features

    • Support devices without PORT module.

[2.7.1]

  • Bug Fixes

    • Fixed MISRA C-2012 rule 10.4 issues in GPIO_GpioGetInterruptChannelFlags() function and GPIO_GpioClearInterruptChannelFlags() function.

[2.7.0]

  • New Features

    • Added API to support Interrupt select (IRQS) bitfield.

[2.6.0]

  • New Features

    • Added API to get GPIO version information.

    • Added API to control a pin for general purpose input.

    • Added some APIs to control pin in secure and previliege status.

[2.5.3]

  • Bug Fixes

    • Correct the feature macro typo: FSL_FEATURE_GPIO_HAS_NO_INDEP_OUTPUT_CONTORL.

[2.5.2]

  • Improvements

    • Improved GPIO_PortSet/GPIO_PortClear/GPIO_PortToggle functions to support devices without Set/Clear/Toggle registers.

[2.5.1]

  • Bug Fixes

    • Fixed wrong macro definition.

    • Fixed MISRA C-2012 rule issues in the FGPIO_CheckAttributeBytes() function.

    • Defined the new macro to separate the scene when the width of registers is different.

    • Removed some redundant macros.

  • New Features

    • Added some APIs to get/clear the interrupt status flag when the port doesn’t control pins’ interrupt.

[2.4.1]

  • Improvements

    • Improved GPIO_CheckAttributeBytes() function to support 8 bits width GACR register.

[2.4.0]

  • Improvements

    • API interface added:

      • New APIs were added to configure the GPIO interrupt clear settings.

[2.3.2]

  • Bug Fixes

    • Fixed the issue for MISRA-2012 check.

      • Fixed rule 3.1, 10.1, 8.6, 10.6, and 10.3.

[2.3.1]

  • Improvements

    • Removed deprecated APIs.

[2.3.0]

  • New Features

    • Updated the driver code to adapt the case of interrupt configurations in GPIO module. New APIs were added to configure the GPIO interrupt settings if the module has this feature on it.

[2.2.1]

  • Improvements

    • API interface changes:

      • Refined naming of APIs while keeping all original APIs by marking them as deprecated. The original APIs will be removed in next release. The main change is updating APIs with prefix of _PinXXX() and _PortXXX.

[2.1.1]

  • Improvements

    • API interface changes:

      • Added an API for the check attribute bytes.

[2.1.0]

  • Improvements

    • API interface changes:

      • Added “pins” or “pin” to some APIs’ names.

      • Renamed “_PinConfigure” to “GPIO_PinInit”.


LPI2C

[2.6.1]

  • Bug Fixes

    • Fixed coverity issues.

[2.6.0]

  • New Feature

    • Added common IRQ handler entry LPI2C_DriverIRQHandler.

[2.5.7]

  • Improvements

    • Added support for separated IRQ handlers.

[2.5.6]

  • Improvements

    • Conditionally compile interrupt handling code to solve the problem of using this driver on CPU cores that do not support interrupts.

[2.5.5]

  • Bug Fixes

    • Fixed LPI2C_SlaveInit() - allow to disable SDA/SCL glitch filter.

[2.5.4]

  • Bug Fixes

    • Fixed LPI2C_MasterTransferBlocking() - the return value was sometime affected by call of LPI2C_MasterStop().

[2.5.3]

  • Improvements

    • Added handler for LPI2C7 and LPI2C8.

[2.5.2]

  • Bug Fixes

    • Fixed ERR051119 to ignore the nak flag when IGNACK=1 in LPI2C_MasterCheckAndClearError.

[2.5.1]

  • Bug Fixes

    • Added bus stop incase of bus stall in LPI2C_MasterTransferBlocking.

  • Improvements

    • Release peripheral from reset if necessary in init function.

[2.5.0]

  • New Features

    • Added new function LPI2C_SlaveEnableAckStall to enable or disable ACKSTALL.

[2.4.1]

  • Improvements

    • Before master transfer with transactional APIs, enable master function while disable slave function and vise versa for slave transfer to avoid the one affecting the other.

[2.4.0]

  • Improvements

    • Split some functions, fixed CCM problem in file fsl_lpi2c.c.

  • Bug Fixes

    • Fixed bug in LPI2C_MasterInit that the MCFGR2’s value set in LPI2C_MasterSetBaudRate may be overwritten by mistake.

[2.3.2]

  • Improvements

    • Initialized the EDMA configuration structure in the LPI2C EDMA driver.

[2.3.1]

  • Improvements

    • Updated LPI2C_GetCyclesForWidth to add the parameter of minimum cycle, because for master SDA/SCL filter, master bus idle/pin low timeout and slave SDA/SCL filter configuration, 0 means disabling the feature and cannot be used.

  • Bug Fixes

    • Fixed bug in LPI2C_SlaveTransferHandleIRQ that when restart detect event happens the transfer structure should not be cleared.

    • Fixed bug in LPI2C_RunTransferStateMachine, that when only slave address is transferred or there is still data remaining in tx FIFO the last byte’s nack cannot be ignored.

    • Fixed bug in slave filter doze enable, that when FILTDZ is set it means disable rather than enable.

    • Fixed bug in the usage of LPI2C_GetCyclesForWidth. First its return value cannot be used directly to configure the slave FILTSDA, FILTSCL, DATAVD or CLKHOLD, because the real cycle width for them should be FILTSDA+3, FILTSCL+3, FILTSCL+DATAVD+3 and CLKHOLD+3. Second when cycle period is not affected by the prescaler value, prescaler value should be passed as 0 rather than 1.

    • Fixed wrong default setting for LPI2C slave. If enabling the slave tx SCL stall, then the default clock hold time should be set to 250ns according to I2C spec for 100kHz standard mode baudrate.

    • Fixed bug that before pushing command to the tx FIFO the FIFO occupation should be checked first in case FIFO overflow.

[2.3.0]

  • New Features

    • Supported reading more than 256 bytes of data in one transfer as master.

    • Added API LPI2C_GetInstance.

  • Bug Fixes

    • Fixed bug in LPI2C_MasterTransferAbortEDMA, LPI2C_MasterTransferAbort and LPI2C_MasterTransferHandleIRQ that before sending stop signal whether master is active and whether stop signal has been sent should be checked, to make sure no FIFO error or bus error will be caused.

    • Fixed bug in LPI2C master EDMA transactional layer that the bus error cannot be caught and returned by user callback, by monitoring bus error events in interrupt handler.

    • Fixed bug in LPI2C_GetCyclesForWidth that the parameter used to calculate clock cycle should be 2^prescaler rather than prescaler.

    • Fixed bug in LPI2C_MasterInit that timeout value should be configured after baudrate, since the timeout calculation needs prescaler as parameter which is changed during baudrate configuration.

    • Fixed bug in LPI2C_MasterTransferHandleIRQ and LPI2C_RunTransferStateMachine that when master writes with no stop signal, need to first make sure no data remains in the tx FIFO before finishes the transfer.

[2.2.0]

  • Bug Fixes

    • Fixed issue that the SCL high time, start hold time and stop setup time do not meet I2C specification, by changing the configuration of data valid delay, setup hold delay, clock high and low parameters.

    • MISRA C-2012 issue fixed.

      • Fixed rule 8.4, 13.5, 17.7, 20.8.

[2.1.12]

  • Bug Fixes

    • Fixed MISRA advisory 15.5 issues.

[2.1.11]

  • Bug Fixes

    • Fixed the bug that, during master non-blocking transfer, after the last byte is sent/received, the kLPI2C_MasterNackDetectFlag is expected, so master should not check and clear kLPI2C_MasterNackDetectFlag when remainingBytes is zero, in case FIFO is emptied when stop command has not been sent yet.

    • Fixed the bug that, during non-blocking transfer slave may nack master while master is busy filling tx FIFO, and NDF may not be handled properly.

[2.1.10]

  • Bug Fixes

    • MISRA C-2012 issue fixed.

      • Fixed rule 10.3, 14.4, 15.5.

    • Fixed unaligned access issue in LPI2C_RunTransferStateMachine.

    • Fixed uninitialized variable issue in LPI2C_MasterTransferHandleIRQ.

    • Used linked TCD to disable tx and enable rx in read operation to fix the issue that for platform sharing the same DMA request with tx and rx, during LPI2C read operation if interrupt with higher priority happened exactly after command was sent and before tx disabled, potentially both tx and rx could trigger dma and cause trouble.

    • Fixed MISRA issues.

      • Fixed rules 10.1, 10.3, 10.4, 11.6, 11.9, 14.4, 17.7.

    • Fixed the waitTimes variable not re-assignment issue for each byte read.

  • New Features

    • Added the IRQHandler for LPI2C5 and LPI2C6 instances.

  • Improvements

    • Updated the LPI2C_WAIT_TIMEOUT macro to unified name I2C_RETRY_TIMES.

[2.1.9]

  • Bug Fixes

    • Fixed Coverity issue of unchecked return value in I2C_RTOS_Transfer.

    • Fixed Coverity issue of operands did not affect the result in LPI2C_SlaveReceive and LPI2C_SlaveSend.

    • Removed STOP signal wait when NAK detected.

    • Cleared slave repeat start flag before transmission started in LPI2C_SlaveSend/LPI2C_SlaveReceive. The issue was that LPI2C_SlaveSend/LPI2C_SlaveReceive did not handle with the reserved repeat start flag. This caused the next slave to send a break, and the master was always in the receive data status, but could not receive data.

[2.1.8]

  • Bug Fixes

    • Fixed the transfer issue with LPI2C_MasterTransferNonBlocking, kLPI2C_TransferNoStopFlag, with the wait transfer done through callback in a way of not doing a blocking transfer.

    • Fixed the issue that STOP signal did not appear in the bus when NAK event occurred.

[2.1.7]

  • Bug Fixes

    • Cleared the stopflag before transmission started in LPI2C_SlaveSend/LPI2C_SlaveReceive. The issue was that LPI2C_SlaveSend/LPI2C_SlaveReceive did not handle with the reserved stop flag and caused the next slave to send a break, and the master always stayed in the receive data status but could not receive data.

[2.1.6]

  • Bug Fixes

    • Fixed driver MISRA build error and C++ build error in LPI2C_MasterSend and LPI2C_SlaveSend.

    • Reset FIFO in LPI2C Master Transfer functions to avoid any byte still remaining in FIFO during last transfer.

    • Fixed the issue that LPI2C_MasterStop did not return the correct NAK status in the bus for second transfer to the non-existing slave address.

[2.1.5]

  • Bug Fixes

    • Extended the Driver IRQ handler to support LPI2C4.

    • Changed to use ARRAY_SIZE(kLpi2cBases) instead of FEATURE COUNT to decide the array size for handle pointer array.

[2.1.4]

  • Bug Fixes

    • Fixed the LPI2C_MasterTransferEDMA receive issue when LPI2C shared same request source with TX/RX DMA request. Previously, the API used scatter-gather method, which handled the command transfer first, then the linked TCD which was pre-set with the receive data transfer. The issue was that the TX DMA request and the RX DMA request were both enabled, so when the DMA finished the first command TCD transfer and handled the receive data TCD, the TX DMA request still happened due to empty TX FIFO. The result was that the RX DMA transfer would start without waiting on the expected RX DMA request.

    • Fixed the issue by enabling IntMajor interrupt for the command TCD and checking if there was a linked TCD to disable the TX DMA request in LPI2C_MasterEDMACallback API.

[2.1.3]

  • Improvements

    • Added LPI2C_WATI_TIMEOUT macro to allow the user to specify the timeout times for waiting flags in functional API and blocking transfer API.

    • Added LPI2C_MasterTransferBlocking API.

[2.1.2]

  • Bug Fixes

    • In LPI2C_SlaveTransferHandleIRQ, reset the slave status to idle when stop flag was detected.

[2.1.1]

  • Bug Fixes

    • Disabled the auto-stop feature in eDMA driver. Previously, the auto-stop feature was enabled at transfer when transferring with stop flag. Since transfer was without stop flag and the auto-stop feature was enabled, when starting a new transfer with stop flag, the stop flag would be sent before the new transfer started, causing unsuccesful sending of the start flag, so the transfer could not start.

    • Changed default slave configuration with address stall false.

[2.1.0]

  • Improvements

    • API name changed:

      • LPI2C_MasterTransferCreateHandle -> LPI2C_MasterCreateHandle.

      • LPI2C_MasterTransferGetCount -> LPI2C_MasterGetTransferCount.

      • LPI2C_MasterTransferAbort -> LPI2C_MasterAbortTransfer.

      • LPI2C_MasterTransferHandleIRQ -> LPI2C_MasterHandleInterrupt.

      • LPI2C_SlaveTransferCreateHandle -> LPI2C_SlaveCreateHandle.

      • LPI2C_SlaveTransferGetCount -> LPI2C_SlaveGetTransferCount.

      • LPI2C_SlaveTransferAbort -> LPI2C_SlaveAbortTransfer.

      • LPI2C_SlaveTransferHandleIRQ -> LPI2C_SlaveHandleInterrupt.

[2.0.0]

  • Initial version.


LPIT

[2.1.1]

  • Improvements

    • Release peripheral from reset if necessary in init function.

[2.1.0]

  • Improvements

    • Add new function LPIT_SetTimerValue to set timeout period.

[2.0.2]

  • Improvements

    • Improved LPIT_SetTimerPeriod implementation, configure timeout value with LPIT ticks minus 1 generate more correct interval.

    • Added timeout value configuration check for LPIT_SetTimerPeriod, at least input 3 ticks for calling LPIT_SetTimerPeriod.

  • Bug Fixes

    • Fixed MISRA C-2012 rule 17.7 violations.

[2.0.1]

  • Bug Fixes

    • MISRA C-2012 issue fixed.

      • Fixed rules, containing: rule-10.3, rule-14.4, rule-15.5.

[2.0.0]

  • Initial version.


LPSPI

[2.7.0]

  • New Feature

    • Added common IRQ handler entry LPSPI_DriverIRQHandler.

[2.6.10]

  • Improvements

    • Conditionally compile interrupt handling code to solve the problem of using this driver on CPU cores that do not support interrupts.

[2.6.9]

  • Bug Fixes

    • Fixed reading of TCR register

    • Workaround for errata ERR050606

[2.6.8]

  • Bug Fixes

    • Fixed build error when SPI_RETRY_TIMES is defined to non-zero value.

[2.6.7]

  • Bug Fixes

    • Fixed the txData from void * to const void * in transmit API _lpspi_master_handle and _lpspi_slave_handle.

[2.6.6]

  • Bug Fixes

    • Added LPSPI register init in LPSPI_MasterInit incase of LPSPI register exist.

[2.6.5]

  • Improvements

    • Introduced FSL_FEATURE_LPSPI_HAS_NO_PCSCFG and FSL_FEATURE_LPSPI_HAS_NO_MULTI_WIDTH for conditional compile.

    • Release peripheral from reset if necessary in init function.

[2.6.4]

  • Bug Fixes

    • Added LPSPI6_DriverIRQHandler for LPSPI6 instance.

[2.6.3]

  • Hot Fixes

    • Added macro switch in function LPSPI_Enable about ERRATA051472.

[2.6.2]

  • Bug Fixes

    • Disabled lpspi before LPSPI_MasterSetBaudRate incase of LPSPI opened.

[2.6.1]

  • Bug Fixes

    • Fixed return value while calling LPSPI_WaitTxFifoEmpty in function LPSPI_MasterTransferNonBlocking.

[2.6.0]

  • Feature

    • Added the new feature of multi-IO SPI .

[2.5.3]

  • Bug Fixes

    • Fixed 3-wire txmask of handle vaule reentrant issue.

[2.5.2]

  • Bug Fixes

    • Workaround for errata ERR051588 by clearing FIFO after transmit underrun occurs.

[2.5.1]

  • Bug Fixes

    • Workaround for errata ERR050456 by resetting the entire module using LPSPIn_CR[RST] bit.

[2.5.0]

  • Bug Fixes

    • Workaround for errata ERR011097 to wait the TX FIFO to go empty when writing TCR register and TCR[TXMSK] value is 1.

    • Added API LPSPI_WaitTxFifoEmpty for wait the txfifo to go empty.

[2.4.7]

  • Bug Fixes

    • Fixed bug that the SR[REF] would assert if software disabled or enabled the LPSPI module in LPSPI_Enable.

[2.4.6]

  • Improvements

    • Moved the configuration of registers for the 3-wire lpspi mode to the LPSPI_MasterInit and LPSPI_SlaveInit function.

[2.4.5]

  • Improvements

    • Improved LPSPI_MasterTransferBlocking send performance when frame size is 1-byte.

[2.4.4]

  • Bug Fixes

    • Fixed LPSPI_MasterGetDefaultConfig incorrect default inter-transfer delay calculation.

[2.4.3]

  • Bug Fixes

    • Fixed bug that the ISR response speed is too slow on some platforms, resulting in the first transmission of overflow, Set proper RX watermarks to reduce the ISR response times.

[2.4.2]

  • Bug Fixes

    • Fixed bug that LPSPI_MasterTransferBlocking will modify the parameter txbuff and rxbuff pointer.

[2.4.1]

  • Bug Fixes

    • Fixed bug that LPSPI_SlaveTransferNonBlocking can’t detect RX error.

[2.4.0]

  • Improvements

    • Split some functions, fixed CCM problem in file fsl_lpspi.c.

[2.3.1]

  • Improvements

    • Initialized the EDMA configuration structure in the LPSPI EDMA driver.

  • Bug Fixes

    • Fixed bug that function LPSPI_MasterTransferBlocking should return after the transfer complete flag is set to make sure the PCS is re-asserted.

[2.3.0]

  • New Features

    • Supported the master configuration of sampling the input data using a delayed clock to improve slave setup time.

[2.2.1]

  • Bug Fixes

    • Fixed bug in LPSPI_SetPCSContinous when disabling PCS continous mode.

[2.2.0]

  • Bug Fixes

    • Fixed bug in 3-wire polling and interrupt transfer that the received data is not correct and the PCS continous mode is not working.

[2.1.0]

  • Improvements

    • Improved LPSPI_SlaveTransferHandleIRQ to fill up TX FIFO instead of write one data to TX register which improves the slave transmit performance.

    • Added new functional APIs LPSPI_SelectTransferPCS and LPSPI_SetPCSContinous to support changing PCS selection and PCS continous mode.

  • Bug Fixes

    • Fixed bug in non-blocking and EDMA transfer APIs that kStatus_InvalidArgument is returned if user configures 3-wire mode and full-duplex transfer at the same time, but transfer state is already set to kLPSPI_Busy by mistake causing following transfer can not start.

    • Fixed bug when LPSPI slave using EDMA way to transfer, tx should be masked when tx data is null, otherwise in 3-wire mode which tx/rx use the same pin, the received data will be interfered.

[2.0.5]

  • Improvements

    • Added timeout mechanism when waiting certain states in transfer driver.

  • Bug Fixes

    • Fixed the bug that LPSPI can not transfer large data using EDMA.

    • Fixed MISRA 17.7 issues.

    • Fixed variable overflow issue introduced by MISRA fix.

    • Fixed issue that rxFifoMaxBytes should be calculated according to transfer width rather than FIFO width.

    • Fixed issue that completion flag was not cleared after transfer completed.

[2.0.4]

  • Bug Fixes

    • Fixed in LPSPI_MasterTransferBlocking that master rxfifo may overflow in stall condition.

    • Eliminated IAR Pa082 warnings.

    • Fixed MISRA issues.

      • Fixed rules 10.1, 10.3, 10.4, 10.6, 11.9, 14.2, 14.4, 15.7, 17.7.

[2.0.3]

  • Bug Fixes

    • Removed LPSPI_Reset from LPSPI_MasterInit and LPSPI_SlaveInit, because this API may glitch the slave select line. If needed, call this function manually.

[2.0.2]

  • New Features

    • Added dummy data set up API to allow users to configure the dummy data to be transferred.

    • Enabled the 3-wire mode, SIN and SOUT pins can be configured as input/output pin.

[2.0.1]

  • Bug Fixes

    • Fixed the bug that the clock source should be divided by the PRESCALE setting in LPSPI_MasterSetDelayTimes function.

    • Fixed the bug that LPSPI_MasterTransferBlocking function would hang in some corner cases.

  • Optimization

    • Added #ifndef/#endif to allow user to change the default TX value at compile time.

[2.0.0]

  • Initial version.


LPTMR

[2.2.0]

  • Improvements

    • Updated lptmr_prescaler_clock_select_t, only define the valid options.

[2.1.1]

  • Improvements

    • Updated the characters from “PTMR” to “LPTMR” in “FSL_FEATURE_PTMR_HAS_NO_PRESCALER_CLOCK_SOURCE_1_SUPPORT” feature definition.

[2.1.0]

  • Improvements

    • Implement for some special devices’ not supporting for all clock sources.

  • Bug Fixes

    • Fixed issue when accessing CMR register.

[2.0.2]

  • Bug Fixes

    • Fixed MISRA-2012 issues.

      • Rule 10.1.

[2.0.1]

  • Improvements

    • Updated the LPTMR driver to support 32-bit CNR and CMR registers in some devices.

[2.0.0]

  • Initial version.


LPUART

[2.9.1]

  • Bug Fixes

    • Fixed coverity issues.

[2.9.0]

  • New Feature

    • Added support for swap TXD and RXD pins.

    • Added common IRQ handler entry LPUART_DriverIRQHandler.

[2.8.3]

  • Improvements

    • Conditionally compile interrupt handling code to solve the problem of using this driver on CPU cores that do not support interrupts.

[2.8.2]

  • Bug Fix

    • Fixed the bug that LPUART_TransferEnable16Bit controled by wrong feature macro.

[2.8.1]

  • Bug Fixes

    • Fixed issue for MISRA-2012 check.

      • Fixed rule-5.3, rule-5.8, rule-10.4, rule-11.3, rule-11.8.

[2.8.0]

  • Improvements

    • Added support of DATA register for 9bit or 10bit data transmit in write and read API. Such as: LPUART_WriteBlocking16bit, LPUART_ReadBlocking16bit, LPUART_TransferEnable16Bit LPUART_WriteNonBlocking16bit, LPUART_ReadNonBlocking16bit.

[2.7.7]

  • Bug Fixes

    • Fixed the bug that baud rate calculation overflow when srcClock_Hz is 528MHz.

[2.7.6]

  • Bug Fixes

    • Fixed LPUART_EnableInterrupts and LPUART_DisableInterrupts bug that blocks if the LPUART address doesn’t support exclusive access.

[2.7.5]

  • Improvements

    • Release peripheral from reset if necessary in init function.

[2.7.4]

  • Improvements

    • Added support for atomic register accessing in LPUART_EnableInterrupts and LPUART_DisableInterrupts.

[2.7.3]

  • Bug Fixes

    • Fixed violations of the MISRA C-2012 rules 15.7.

[2.7.2]

  • Bug Fix

    • Fixed the bug that the OSR calculation error when lupart init and lpuart set baud rate.

[2.7.1]

  • Improvements

    • Added support for LPUART_BASE_PTRS_NS in security mode in file fsl_lpuart.c.

[2.7.0]

  • Improvements

    • Split some functions, fixed CCM problem in file fsl_lpuart.c.

[2.6.0]

  • Bug Fixes

    • Fixed bug that when there are multiple lpuart instance, unable to support different ISR.

[2.5.3]

  • Bug Fixes

    • Fixed comments by replacing unused status flags kLPUART_NoiseErrorInRxDataRegFlag and kLPUART_ParityErrorInRxDataRegFlag with kLPUART_NoiseErrorFlag and kLPUART_ParityErrorFlag.

[2.5.2]

  • Bug Fixes

    • Fixed bug that when setting watermark for TX or RX FIFO, the value may exceed the maximum limit.

  • Improvements

    • Added check in LPUART_TransferDMAHandleIRQ and LPUART_TransferEdmaHandleIRQ to ensure if user enables any interrupts other than transfer complete interrupt, the dma transfer is not terminated by mistake.

[2.5.1]

  • Improvements

    • Use separate data for TX and RX in lpuart_transfer_t.

  • Bug Fixes

    • Fixed bug that when ring buffer is used, if some data is received in ring buffer first before calling LPUART_TransferReceiveNonBlocking, the received data count returned by LPUART_TransferGetReceiveCount is wrong.

[2.5.0]

  • Bug Fixes

    • Added missing interrupt enable masks kLPUART_Match1InterruptEnable and kLPUART_Match2InterruptEnable.

    • Fixed bug in LPUART_EnableInterrupts, LPUART_DisableInterrupts and LPUART_GetEnabledInterrupts that the BAUD[LBKDIE] bit field should be soc specific.

    • Fixed bug in LPUART_TransferHandleIRQ that idle line interrupt should be disabled when rx data size is zero.

    • Deleted unused status flags kLPUART_NoiseErrorInRxDataRegFlag and kLPUART_ParityErrorInRxDataRegFlag, since firstly their function are the same as kLPUART_NoiseErrorFlag and kLPUART_ParityErrorFlag, secondly to obtain them one data word must be read out thus interfering with the receiving process.

    • Fixed bug in LPUART_GetStatusFlags that the STAT[LBKDIF], STAT[MA1F] and STAT[MA2F] should be soc specific.

    • Fixed bug in LPUART_ClearStatusFlags that tx/rx FIFO is reset by mistake when clearing flags.

    • Fixed bug in LPUART_TransferHandleIRQ that while clearing idle line flag the other bits should be masked in case other status bits be cleared by accident.

    • Fixed bug of race condition during LPUART transfer using transactional APIs, by disabling and re-enabling the global interrupt before and after critical operations on interrupt enable register.

    • Fixed DMA/eDMA transfer blocking issue by enabling tx idle interrupt after DMA/eDMA transmission finishes.

  • New Features

    • Added APIs LPUART_GetRxFifoCount/LPUART_GetTxFifoCount to get rx/tx FIFO data count.

    • Added APIs LPUART_SetRxFifoWatermark/LPUART_SetTxFifoWatermark to set rx/tx FIFO water mark.

[2.4.1]

  • Bug Fixes

    • Fixed MISRA advisory 17.7 issues.

[2.4.0]

  • New Features

    • Added APIs to configure 9-bit data mode, set slave address and send address.

[2.3.1]

  • Bug Fixes

    • Fixed MISRA advisory 15.5 issues.

[2.3.0]

  • Improvements

    • Modified LPUART_TransferHandleIRQ so that txState will be set to idle only when all data has been sent out to bus.

    • Modified LPUART_TransferGetSendCount so that this API returns the real byte count that LPUART has sent out rather than the software buffer status.

    • Added timeout mechanism when waiting for certain states in transfer driver.

[2.2.8]

  • Bug Fixes

    • Fixed issue for MISRA-2012 check.

      • Fixed rule-10.3, rule-14.4, rule-15.5.

    • Eliminated Pa082 warnings by assigning volatile variables to local variables and using local variables instead.

    • Fixed MISRA issues.

      • Fixed rules 10.1, 10.3, 10.4, 10.8, 14.4, 11.6, 17.7.

  • Improvements

    • Added check for kLPUART_TransmissionCompleteFlag in LPUART_WriteBlocking, LPUART_TransferHandleIRQ, LPUART_TransferSendDMACallback and LPUART_SendEDMACallback to ensure all the data would be sent out to bus.

    • Rounded up the calculated sbr value in LPUART_SetBaudRate and LPUART_Init to achieve more acurate baudrate setting. Changed osr from uint32_t to uint8_t since osr’s bigest value is 31.

    • Modified LPUART_ReadBlocking so that if more than one receiver errors occur, all status flags will be cleared and the most severe error status will be returned.

[2.2.7]

  • Bug Fixes

    • Fixed issue for MISRA-2012 check.

      • Fixed rule-12.1, rule-17.7, rule-14.4, rule-13.3, rule-14.4, rule-10.4, rule-10.8, rule-10.3, rule-10.7, rule-10.1, rule-11.6, rule-13.5, rule-11.3, rule-13.2, rule-8.3.

[2.2.6]

  • Bug Fixes

    • Fixed the issue of register’s being in repeated reading status while dealing with the IRQ routine.

[2.2.5]

  • Bug Fixes

    • Do not set or clear the TIE/RIE bits when using LPUART_EnableTxDMA and LPUART_EnableRxDMA.

[2.2.4]

  • Improvements

    • Added hardware flow control function support.

    • Added idle-line-detecting feature in LPUART_TransferNonBlocking function. If an idle line is detected, a callback is triggered with status kStatus_LPUART_IdleLineDetected returned. This feature may be useful when the received Bytes is less than the expected received data size. Before triggering the callback, data in the FIFO (if has FIFO) is read out, and no interrupt will be disabled, except for that the receive data size reaches 0.

    • Enabled the RX FIFO watermark function. With the idle-line-detecting feature enabled, users can set the watermark value to whatever you want (should be less than the RX FIFO size). Data is received and a callback will be triggered when data receive ends.

[2.2.3]

  • Improvements

    • Changed parameter type in LPUART_RTOS_Init struct from rtos_lpuart_config to lpuart_rtos_config_t.

  • Bug Fixes

    • Disabled LPUART receive interrupt instead of all NVICs when reading data from ring buffer. Otherwise when the ring buffer is used, receive nonblocking method will disable all NVICs to protect the ring buffer. This may has a negative effect on other IPs that are using the interrupt.

[2.2.2]

  • Improvements

    • Added software reset feature support.

    • Added software reset API in LPUART_Init.

[2.2.1]

  • Improvements

    • Added separate RX/TX IRQ number support.

[2.2.0]

  • Improvements

    • Added support of 7 data bits and MSB.

[2.1.1]

  • Improvements

    • Removed unnecessary check of event flags and assert in LPUART_RTOS_Receive.

    • Added code to always wait for RX event flag in LPUART_RTOS_Receive.

[2.1.0]

  • Improvements

    • Update transactional APIs.


MCM

[2.2.0]

  • Improvements

    • Support platforms with less features.

[2.1.0]

  • Others

    • Remove byteID from mcm_lmem_fault_attribute_t for document update.

[2.0.0]

  • Initial version.


MMDVSQ

[2.0.3]

  • Bug Fixes

    • MISRA C-2012 issue fixed: rule 10.3, 10.4, and 14.4.

[2.0.2]

  • Bug fix:

    • Fixed MMDVSQ_GetExecutionStatus function get execution status wrong.

[2.0.1]

  • Other changes:

    • Changed name of MMDVSQ_GetDivideRemainder and MMDVSQ_GetDivideQuotient functions.

[2.0.0]

  • Initial version.


MSCAN

[2.1.0]

  • Improvements

    • Added wrong data length code(DLC) detection, report kStatus_MSCAN_DataLengthError when DLC is wrong.

[2.0.7]

  • Bug Fixes

    • Fix build warning.

[2.0.6]

  • Bug Fixes

    • Fix MISRA C-2012 rule 10.3.

[2.0.5]

  • Bug Fixes

    • Fixed the code error issue and simplified the algorithm in improved timing APIs.

      • MSCAN_CalculateImprovedTimingValues

[2.0.4]

  • Bug Fixes

    • Fixed the non-divisible case in improved timing API.

      • MSCAN_CalculateImprovedTimingValues

[2.0.3]

  • Bug Fixes

    • MISRA C-2012 issue check.

      • Fixed MISRA C-2012 issue in mcan driver, containing: rule-10.1, rule-10.3, rule-10.4, rule-10.7, rule-11.8, rule-14.4, rule-15.5, rule-16.1, rule-16.4, rule-17.7, rule-8.4, rule-8.5.

[2.0.2]

  • Bug Fixes

    • Fixed issue Clang - disable declaration alignment.

    • Fixed issue Central repository code formatting.

  • Improvements

    • Implemented feature to find classical CAN improved timing configuration.

[2.0.1]

  • Bug Fixes

    • Fixed timestamp issue where it cannot be enabled.

    • Fixed standard mode frame buffer configuration.

    • Added RX Message Buffer Mask helper macro, MSCAN_RX_MB_STD_MASK, MSCAN_RX_MB_EXT_MASK.

    • Fixed dataByte[0-7] order in struct type mscan_frame_t.

    • Updated function MSCAN_WriteTxMb. The MSCAN registers are 8 bits, using 8 bits write for registers.

[2.0.0]

  • Initial version.


PDB

[2.0.4]

  • Bug Fixes

    • Fixed violations of MISRA C-2012 rule 10.1 and 10.4.

[2.0.3]

  • Bug Fixes

    • Fixed violations of MISRA C-2012 rule 17.7.

[2.0.2]

  • Improvement:

    • Used macros in feature file instead of that in IO map.

[2.0.1]

  • Changed PDB register base array to const.

[2.0.0]

  • Initial version.


PMC

[2.0.3]

  • Bug Fixes

    • Fixed the violation of MISRA C-2012 rule 11.3.

[2.0.2]

  • Bug Fixes

    • Fixed the violations of MISRA 2012 rules:

      • Rule 10.3.

[2.0.1]

  • Bug Fixes

    • Fixed MISRA issues.

      • Rule 10.8, Rule 10.3.

[2.0.0]

  • Initial version.


PORT

[2.5.1]

  • Bug Fixes

    • Fix CERT INT31-C issues.

[2.5.0]

  • Bug Fixes

    • Correct the kPORT_MuxAsGpio for some platforms.

[2.4.1]

  • Bug Fixes

    • Fixed the violations of MISRA C-2012 rules: 10.1, 10.8 and 14.4.

[2.4.0]

  • New Features

    • Updated port_pin_config_t to support input buffer and input invert.

[2.3.0]

  • New Features

    • Added new APIs for Electrical Fast Transient(EFT) detect.

    • Added new API to configure port voltage range.

[2.2.0]

  • New Features

    • Added new api PORT_EnablePinDoubleDriveStrength.

[2.1.1]

  • Bug Fixes

    • Fixed the violations of MISRA C-2012 rules: 10.1, 10.4,11.3,11.8, 14.4.

[2.1.0]

  • New Features

    • Updated the driver code to adapt the case of the interrupt configurations in GPIO module. Will move the pin configuration APIs to GPIO module.

[2.0.2]

  • Other Changes

    • Added feature guard macros in the driver.

[2.0.1]

  • Other Changes

    • Added “const” in function parameter.

    • Updated some enumeration variables’ names.


PWT

[2.0.1]

  • Bug Fixes

    • Fixed violations of MISRA C-2012 rules: 10.8, 10.3, 10.6.

[2.0.0]

  • Initial version.


RCM

[2.0.4]

  • Bug Fixes

    • Fixed violation of MISRA C-2012 rule 10.3

[2.0.3]

  • Bug Fixes

    • Fixed violation of MISRA C-2012 rules.

[2.0.2]

  • Bug Fixes

    • Fixed MISRA issue.

      • Rule 10.8, rule 10.1, rule 13.2, rule 3.1.

[2.0.1]

  • Bug Fixes

    • Fixed kRCM_SourceSw bit shift issue.

[2.0.0]

  • Initial version.


RTC

[2.3.0]

  • Improvements

    • Added API RTC_EnableLPOClock to set 1kHz LPO clock.

    • Added API RTC_EnableCrystalClock to replace API RTC_SetClockSource.

[2.2.2]

  • Improvements

    • Refine _rtc_interrupt_enable order.

[2.2.1]

  • Bug Fixes

    • Fixed the issue of Pa082 warning.

    • Fixed the issue of bit field mask checking.

    • Fixed the issue of hard code in RTC_Init.

[2.2.0]

  • Bug Fixes

    • Fixed MISRA C-2012 issue.

      • Fixed rule contain: rule-17.7, rule-14.4, rule-10.4, rule-10.7, rule-10.1, rule-10.3.

    • Fixed central repository code formatting issue.

  • Improvements

    • Added an API for enabling wakeup pin.

[2.1.0]

  • Improvements

    • Added feature macro check for many features.

[2.0.0]

  • Initial version.


SIM

[2.2.0]

  • Improvements

    • Added API to trigger TRGMUX.

[2.1.3]

  • Improvements

    • Updated function SIM_GetUniqueId to support different register names.

[2.1.2]

  • Bug Fixes

    • Fixed SIM_GetUniqueId bug that could not get UIDH.

[2.1.1]

  • Bug Fixes

    • Fixed violations of the MISRA C-2012 rules 10.1, 10.4

[2.1.0]

  • Improvements

    • Added new APIs: SIM_GetRfAddr() and SIM_EnableSystickClock().

[2.0.0]

  • Initial version.


SMC

[2.0.7]

  • Bug Fixes

    • Fixed MISRA-2012 issue 10.3.

[2.0.6]

  • Bug Fixes

    • Fixed issue for MISRA-2012 check.

      • Fixed rule 10.3, rule 11.3.

[2.0.5]

  • Bug Fixes

    • Fixed issue for MISRA-2012 check.

      • Fixed rule 15.7, rule 14.4, rule 10.3, rule 10.1, rule 10.4.

[2.0.4]

  • Bug Fixes

    • When entering stop modes, used RAM function for the flash synchronization issue. Application should make sure that, the RW data of fsl_smc.c is located in memory region which is not powered off in stop modes.

[2.0.3]

  • Improvements

    • Added APIs SMC_PreEnterStopModes, SMC_PreEnterWaitModes, SMC_PostExitWaitModes, and SMC_PostExitStopModes.

[2.0.2]

  • Bug Fixes

    • Added DSB before WFI while ISB after WFI.

  • Other Changes

    • Updated SMC_SetPowerModeVlpw implementation.

[2.0.1]

  • Other Changes

    • Updated for KL8x.

[2.0.0]

  • Initial version.


TRGMUX

[2.0.1]

  • Bug Fixes

    • Fixed violations of the MISRA C-2012 rules 10.1, 10.3, 10.8.

[2.0.0]

  • Initial version.


TSI_V5

[2.6.0]

  • Improvements

    • Add API TSI_ShieldChannelConfig to config all TSI shield channels.

[2.5.0]

  • Improvements

    • Add API TSI_EnableShieldChannels to enable/disable TSI shield channels.

[2.4.0]

  • Bug Fixes

    • Fixed some elements in the array tsi_sensitivity_xdn_option_t does not match the S_XDN bits.

[2.3.0]

  • Other Changes

    • Changed the TSI SINC cutoff divider number.

[2.2.0]

  • Improvements

    • Extended enableShield items from tsi_selfCap_config_t structure to cover three shields in the ke17z series.

    • Added interface for getting instance from TSI base address and apply it for clock and IRQ enable/disable.

[2.1.2]

  • Bug Fixes

    • Fixed the violations of MISRA C-2012 rules: 10.1, 10.8.

[2.1.1]

  • Improvements

    • Improved the module’s noise immunity in mutual cap mode by setting M_TRIM2[0] to 1 in TSI_MUL1 register.

  • Bug Fixes

    • Fixed the violations of MISRA C-2012 rules:

      • Rule 10.1, 10.3, 10.4, 10.8, 12.2, 14.4, 17.7.

[2.1.0]

  • Bug Fixes

    • Fixed incorrect TSI SSC clock calculation.

[2.0.1]

  • Improvements

    • Added functions for M_TX_USED bitfield for ke16z only (Unused TX mutual pins can work as GPIO).

[2.0.0]

  • Initial version.


WDOG32

[2.1.0]

  • Improvements

    • Release peripheral from reset if necessary in init function.

[2.0.4]

  • Improvements

    • To ensure that the reconfiguration is inside 128 bus clocks unlock window, put all re-configuration APIs in quick access code section.

[2.0.3]

  • Bug Fixes

    • Fixed the noncompliance issue of the reference document.

      • Waited until for new configuration to take effect by checking the RCS bit field.

      • Waited until for registers to be unlocked by checking the ULK bit field.

  • Improvements

    • Added 128 bus clocks delay ensures a smooth transition before restarting the counter with the new configuration when there is no RCS status bit.

[2.0.2]

  • Bug Fixes

    • MISRA C-2012 issue fixed.

      • Fixed rules, containing: rule-10.3, rule-14.4, rule-15.5.

    • Fixed the issue of the inseparable process interrupted by other interrupt source.

      • WDOG32_Refresh

[2.0.1]

  • Bug Fixes

    • WDOG must be configured within its configuration time period.

      • Added WDOG32_Init API to quick access section.

      • Defined register variable in WDOG32_Init API.

[2.0.0]

  • Initial version.