Logo
25.06.00-pvw2
MCUXpresso SDK Project v: latest
Document Release Versions
25.06.00-pvw2
25.06.00-pvw1
25.03.00
25.03.00-pvw2
24.12.00
latest

Introduction

  • MCUXpresso SDK
  • Setup

Getting Started

  • Github Repository
  • Zip Package

User Guide

  • Drivers
  • Examples
  • Middlewares
  • RTOS
  • Boards

Development

  • Architecture
  • Build And Configuration System
  • Developing with MCUXpresso SDK

Releases

  • Release Notes
mcuxsdk
  • Docs / 25.06.00-pvw2 »
  • Link DSP Profiles
  • Open on Repo Report an issue with this page

Link DSP Profiles

The Xtensa Software Tools use the linker support packages (LSPs) to link a HiFi4 DSP application for the RT700. An LSP includes both a system memory map and a collection of libraries to include into the final binary. The LSPs are provided in the MCUXpresso SDK and are available at: <SDK_ROOT>/devices/MIMXRT685S/xtensa/.

DSP sample applications are configured to link against one of these custom LSPs. By default, Debug targets are linked against the gdbio LSP intended for use with an attached debugger and captures I/O requests (printf) through gdb. The Release target links against the min-rt LSP, which includes minimal runtime support.

To change the LSP used by a project target in the Xplorer IDE, use the Linker tab in the project Build Properties dialog box.

|

|

The MCUXpresso SDK ships with other standard LSPs for RT700. For more information on LSPs and creating a custom memory map using Xtensa software tools, see the Cadence Linker Support Packages (LSPs) Reference Manual.


Copyright 2025, NXP. Last generated on May 16, 2025 14:38+0200; branch release/25.06.00-pvw2, revision 90a0e8c866b7507e94541ce7c0aaf8f23a4f7861.