Example Development
Overview
In addition to the sources, one example contains CMakeLists.txt, Kconfig, prj.conf and example.yml.
hello_world
    ├── hello_world.c
    ├── CMakeLists.txt
    ├── Kconfig
    ├── prj.conf
    ├── example.yml
CMakeLists.txt
CMakeLists.txt defines the sources, includes and static configurations.
Based on the cmake built-in macro project, we customize the project to provide the following additional arguments:
Argument Name  | 
Argument Type  | 
Explanation  | 
|---|---|---|
PROJECT_BOARD_PORT_PATH  | 
Single  | 
Path for board porting files and data.  | 
PROJECT_DEVICE_PORT_PATH  | 
Single  | 
Path for device porting files and data.  | 
PROJECT_TYPE  | 
Single  | 
Specify the project type, can be   | 
CUSTOM_PRJ_CONF_PATH  | 
Multiple  | 
Specify customized prj.conf search paths.  | 
Here is the hello_world CMakeLists.txt:
cmake_minimum_required(VERSION 3.30.0)
include(${SdkRootDirPath}/cmake/extension/mcux.cmake)
# Specify the project
project(hello_world LANGUAGES C CXX ASM PROJECT_BOARD_PORT_PATH ${board_root}/${board}/demo_apps/hello_world)
# Include device, board, drivers, components, middlewares, RTOS
include(${SdkRootDirPath}/CMakeLists.txt)
mcux_add_source(
    SOURCES hello_world.c
)
RTOSRTOS
mcux_add_include(
    INCLUDES .
)
# convert binary to .bin. 
mcux_convert_binary(BINARY ${APPLICATION_BINARY_DIR}/${MCUX_SDK_PROJECT_NAME}.bin)
Kconfig
Kconfig defines the dynamic configurations.
It is not required to always provide example specific Kconfig. If your example has specific Kconfig, then please follow the pattern to add it:
rsource "../../../Kconfig.mcuxpresso"
mainmenu "Hello world Example Run Time Configuration"
config HELLO_WORLD_EXAMPLE_MACRO
    bool "Hello world example macro"
    default y
    help
        "Hello world example macro"
rsource "../../../Kconfig.mcuxpresso"must be added to load all device, board and other components Kconfigs.Set
mainmenuto give the GUI titleSet the example specific configurations
The Kconfig process will take example specific Kconfig as entry point with priority. If not provided, then it will take the mcuxsdk/Kconfig.mcuxpresso instead.
prj.conf
prj.conf here specifies the example specific configuration values for Kconfig symbols. It will be merged together with other prj.conf values from device, board and shield to produce the final configurations.
See prj.conf for more details.
example.yml
example.yml contains data specifying example category, description, supported devices, boards and shields, etc. It is mainly for tool and CI usage.
Overview
# yaml-language-server: $schema=../../../../scripts/data_schema/example_description_schema.json
hello_world:
  section-type: application
  contents:
    meta_path: examples/demo_apps/hello_world
    project-root-path: boards/${board}/demo_apps/hello_world/${multicore_foldername}
    document:
      name: hello_world${core_id_suffix_name}
      category: demo_apps
      brief: The HelloWorld demo prints the "Hello World" string to the terminal using
        the SDK UART drivers and repeat what user input. The purpose of this demo
        is to show how to use the UART, and to provide a simple project for debugging
        and further development.
      example_readme:
      - examples/demo_apps/hello_world/readme.md
      - ${board_root}/${board}/demo_apps/hello_world/example_board_readme.md
      - ${board_root}/${board}/examples_shared_readme.md
  boards:
    evk9mimx8ulp@cm33: []
    evkbimxrt1050:
    - +armgcc@flexspi_nor_sdram_debug
    - +armgcc@flexspi_nor_sdram_release
    - +armgcc@sdram_txt_debug
    - +armgcc@sdram_txt_release
    - +iar@flexspi_nor_sdram_debug
    - +iar@flexspi_nor_sdram_release
    - +iar@ram_0x1400_debug
    - +iar@ram_0x1400_release
    - +iar@sdram_txt_debug
    - +iar@sdram_txt_release
    - +mdk@flexspi_nor_sdram_debug
    - +mdk@flexspi_nor_sdram_release
    - +mdk@ram_0x1400_debug
    - +mdk@ram_0x1400_release
    - +mdk@sdram_txt_debug
    - +mdk@sdram_txt_release
Example Toolchains and Targets
The supported toolchains and build configuration targets for an example can be got in the following way:
Get the designated board example.yml to get the board default supported toolchains and build configuration targets from board.toolchains.
This is for board examples. For device examples, it should be the device example.yml. We don’t have such cases public yet.
Get the designated board from
boardsdata attributeIf the data attribute is empty, then the board level toolchains and build configuration targets are the example ones.
If the data attribute exists,
+to add extra toolchains and build configuration targets pairs with the board ones.-to reduce extra ones from board ones.
The mcuxsdk/scripts/data_schema/example_decription_schema.json is provided to specify detailedly the data attributes for the example.yml.
Example Types
Board Examples and Device Examples
MCUXpresso SDK supports both board examples and device examples. The board examples are based on board and the mounted device while device examples only use target device without board. For hierarchical configuration for porting, board examples use PROJECT_BOARD_PORT_PATH, device examples use PROJECT_DEVICE_PORT_PATH.
Since most examples are board examples, we will focus on board examples for illustration in later chapters.
Repository Examples and Freestanding Examples
In MCUXpresso SDK, based on example location we distinguish 2 example types: repository and freestanding examples.
Example Type  | 
Example Location(where CMakeLists.txt is placed)  | 
|---|---|
Repository  | 
MCUXpresso SDK repository  | 
Freestanding  | 
Other locations  | 
Repository Examples
Most repository examples CMakelists.txts are located inside mcuxsdk/examples/<example-category>/<example> folder, like the hello_world CMakelists.txt is located in mcuxsdk/examples/demo_apps/hello_world.
sdk_next/
├─── .west/
│    └─── config
└─── mcuxsdk/
     ├── arch/
     ├── cmake/
     ├── examples
     │   	├── demo_apps
     │              ├── reconfig.cmake
     │              ├── prj.conf
     │  	        ├── hello_world
     │                     ├── CMakeLists.txt
     │                     ├── Kconfig
     │                     ├── prj.conf
     │                     ├── hello_world.c
     │                     ├── example.yml
Hierarchical Configuration for Board Porting
For MCUXpresso SDK officially supported boards, the board porting configuration has been provided for all board supported examples in a hierarchical way. In any repository example CMakeLists.txt project macro, the PROJECT_BOARD_PORT_PATH is provided to specify the root board porting path. All the prj.conf files inside each sub folder of PROJECT_BOARD_PORT_PATH will be processed during the example build, they are hierarchically configuring the example in different levels.
Take evkbmimxrt1170 hello_world porting for example, in the hello_world CMakeLists.txt, we have set PROJECT_BOARD_PORT_PATH as examples/_boards/${board}/demo_apps/hello_world as the following:
project(hello_world LANGUAGES C CXX ASM PROJECT_BOARD_PORT_PATH examples/_boards/${board}/demo_apps/hello_world)
So following prj.conf files are taken into examples to do different level configurations.
prj.conf  | 
Application scope of configuration  | 
|---|---|
examples/prj.conf  | 
Apply for all examples  | 
examples/_boards/prj.conf  | 
Apply for all NXP official boards examples  | 
examples/_boards/evkbmimxrt1170/prj.conf  | 
Apply for all evkbmimxrt1170 examples  | 
examples/_boards/evkbmimxrt1170/demo_apps/prj.conf  | 
Apply for all evkbmimxrt1170 demo apps examples  | 
examples/_boards/evkbmimxrt1170/demo_apps/hello_world/prj.conf  | 
Apply for evkbmimxrt1170 hello_world examples  | 
The deeper path of prj.conf, the higher priority it has.
For example without
PROJECT_BOARD_PORT_PATHinsideproject, there is no such hierarchical configuration provided.
Freestanding Examples
Freestanding example points examples located outside MCUXpresso SDK repository. Here is a typical freestanding example layout:
<home>/
├─── sdk_next/
│     ├─── .west/
│     │    └─── config
│     ├── mcuxsdk/
│     └── ...
│
└─── app/
     ├── CMakeLists.txt
     ├── prj.conf
     └── src/
         └── main.c
Freestanding examples share the same build and run way as repository examples. You can still use west build to work.
Configuration
All freestanding examples still share the default configuration of the target device, board and the full scope example configuration just as the repository example: The default prj.conf list is like:
1. devices/prj.conf
2. devices/<soc_series>/prj.conf
3. devices/<soc_series>/<device>/prj.conf
4. devices/<soc_series>/<device>/<core_id>/prj.conf
5. examples/prj.conf # full scope example configuration
6. examples/_boards/prj.conf
7. examples/_boards/<board>/prj.conf
8. examples/_boards/<board>/<core_id>/prj.conf
9. <example location>/prj.conf # The example itself configuration
If PROJECT_BOARD_PORT_PATH is provided inside project macro, a freestanding example can additionally shares the same board hierarchical configuration, then its configuration is same as the repository example except itself part.
The freestanding examples may don’t need the default pin mux and hardware_init/app prj.conf setting, you can disable them in <example location>/prj.conf:
CONFIG_MCUX_PRJSEG_module.board.pinmux_project_folder=n
CONFIG_MCUX_PRJSEG_module.board.pinmux_board_folder=n
CONFIG_MCUX_HAS_PRJSEG_project.use_hw_app=n
CONFIG_MCUX_HAS_PRJSEG_module.board.pinmux_sel=n
Ways to Get MCUXpresso SDK Contents
For freestanding example, there are 2 ways to get the MCUXpresso SDK contents.
Explicitly include root CMakeLists.txt
The CMakeLists.txt shall explicitly include mcux.cmake to get the NXP cmake extension and include the root CMakeLists.txt to get MCUXpresso SDK contents.
include(${SdkRootDirPath}/cmake/extension/mcux.cmake)
# No PROJECT_BOARD_PORT_PATH in project
project(hello_world LANGUAGES C CXX ASM PROJECT_BOARD_PORT_PATH ${board_root}/${board}/<example_category>)
include(${SdkRootDirPath}/CMakeLists.txt)
Use McuxSDK CMake package
Since the MCUXpresso SDK can be exported to be a standard CMake package, so you can directly use find_package(McuxSDK) way to get MCUXpresso SDK contents:
cmake_minimum_required(VERSION 3.30.0)
find_package(McuxSDK 24.12.00 EXACT REQUIRED)
project(hello_world LANGUAGES C CXX ASM)
Please refer McuxSDK CMake Package for details.
Standalone Examples
The build system provides a feature to collect and copy all the components and example self configurations and sources into an individual folder so that the example can build and run just with the stuff in the folder without depending on the mcuxsdk repository.
With this feature, it could be very convenient to zip and share examples between developers.
To build the standalone examples, an individual build system is provided in the location folder.
For toolchains with GUI tool support like IAR/MDK/Codewarrior/Xtensa, the example files like .ewp file for IAR, .uvprojx for MDK, will be generated to use. You can directly use corresponding IDE to work.
For toolchain without GUI tool support like Armgcc, all the examples files and configurations will be flattened into a complete CMakeLists.txt. Build target specific shell and windows cmd batch will be provided to do the build.
There is no Kconfig file in the standalone folder, so there is no Kconfig GUI feature in the standalone example.
The standalone example can be generated with west command line parameters -t standalone_project like:
west build -b evkbmimxrt1170 ./examples/demo_apps/hello_world -Dcore_id=cm7 -p always --toolchain iar -t standalone_project
You can find IAR project is generated in build folder with all the sources. The default destination folder is “build” and can be specified by -d parameter.

The standalone example feature supports repository examples and freestanding examples using the explicitly include root CMakeLists.txt. Freestanding examples using McuxSDK CMake package do not have standalone example feature.
If your example already has generated build artifacts, you can directly type west build -t standalone_project to generate the standalone example.
Convert a Repository Example to a Freestanding Example
If you find one repository example functions are similar to your example and want to copy it from SDK repository into your own workspace as a freestanding example to start the development, you can use west export_app command to do it. Take hello_world as an example:
west export_app examples/demo_apps/hello_world -o <new workspace>
Then you can get output like this:
=== Successfully create the freestanding project, see <new workspace>/examples/demo_apps/hello_world/CMakeLists.txt.
=== you can use following command to build it.
west build -b <board_id> --toolchain armgcc -p always <new workspace>/examples/demo_apps/hello_world -DPrjRootDirPath=<new workspace> -d <new workspace>/build
--buildparameter can tell the extension build the freestanding example after convertion.
-Dcore_id=<core_id>is needed for multicore board
Technically, the freestanding example generated by the above command can support any board.
If you want to specify the target board, you can use -b argument like
west export_app -b evkbmimxrt1170 examples/demo_apps/hello_world -Dcore_id=cm7 -o <new workspace>
Then you can use the following command to build
west build -b evkbmimxrt1170 --toolchain armgcc -p always <new workspace>/examples/demo_apps/hello_world -DPrjRootDirPath=<new workspace> -d <new workspace>/build -Dcore_id=cm7
The -b shall only point evkbmimxrt1170.
Example with different build configurations
An example may have different build configuration(usually for test), see prj.conf. It is easy for developer to add different configurations in example.ymlto make it be visiable to list_project and build extension.
Here is an example:
# examples/demo_apps/hello_world/example.yml+
hello_world:
  hello world content
# The example with custom configuration must end with '@config_name'
hello_world@custom1:
  section-type: custom_application # MUST BE custom_application
  contents:
    document:
      extra_build_args:
      - -DCONF_FILE=examples/demo_apps/hello_world/new.conf
  boards:
    # define your scope for this custom_application
NOTE
Currently, custom_application only support contents -> document -> extra_build_args, do not add other fields.
Component Configuration in Project Construction and Build
There are following ways to do component configuration in the project construction and build
Use Kconfig to do configuration for the component set
Use the prepared customized configuration header file for the component set in the example root
Use the component default provided configuration header file
For a component, it must be defined in Kconfig, otherwise the component won’t be involved into the build tree anyway, but it is not required that component Kconfig item must have concrete configurations. You can still put configurations like macro definitions in the header file.
To make the above ways coexist in a component set, a component set(especially middleware components) shall do the following steps:
Prepare a
configcomponent to hold the default configuration file for the component set.configcomponent means the component files shall be marked withCONFIG: TRUE, and if the config file is a header file, the include path shall useTARGET_FILESto identify the file that corresponds to the path. Theconfigheader file has lowest priority in the build system, if any same name header file is provided in the example root, then it won’t be included. Thisconfigcomponent shall be selected by the core component of the component set, then it can always be selected. So if the customized configuration is not provided for that component, the project can still build with default configuration provided byconfigcomponent.Prepare a project segment in Kconfig file to hold all Kconfig configuration symbols for the component set. All the configuration symbols shall be set to be generated into a designated header file with the same name as component default configuration file.
If you want to use Kconfig to do configuration, then the project segment shall be set to y. The generated configuration header name shall be set in Kconfig and be the same with component default configuration header file so that it will override the component default one. The project segment can depend on the core component of the component set so that it  can involve core component of the set.
If you don’t want to use Kconfig but want to directly provide a configuration header, then project segment should be set to n, the directly provided configuration header shall be put in the root of project.
Create an Example
Firstly, you should make sure that the target device and board data are ready, secondly, you need to follow the above CMakeLists.txt, Kconfig, prj.conf and example.yml chapters to prepare the build and configuration files, then it should be ok.
If the default board and device data and configuration cannot satisfy your needs, then you need to do customization for the certain device or board or both.
There are following ways to do the customization.
Reconfig CMake
In the example CMakeLists.txt, there is such line
include(${SdkRootDirPath}/${board_root}/${board}/demo_apps/hello_world/reconfig.cmake OPTIONAL)
This is the board port cmake. Any board specific configurations can be added in it.
prj.conf
For component selection and configuration, you can use different scope prj.conf to achieve it. Refer the priority of prj.conf in prj.conf chapter to set the data.
Build The Example
Run west build -h to see help information for west build command.
Compared to zephyr’s west build, MCUXpresso SDK build command provides following additional options for examples:
–toolchain: specify the toolchain for this build, default armgcc.
–config: value for CMAKE_BUILD_TYPE, default debug.
Here are some typical usage for generating a SDK example is:
# Build example
west build -b frdmk22f examples/demo_apps/hello_world
# multcore device must be specified with core_id
west build -b evkbmimxrt1170 examples/demo_apps/hello_world -Dcore_id=cm7
# Just print cmake commands, do not execute it
west build -b evkbmimxrt1170 examples/demo_apps/hello_world -Dcore_id=cm7 --dry-run
# Build iar
west build -b evkbmimxrt1170 examples/demo_apps/hello_world -Dcore_id=cm7 --toolchain iar
# Build flexspi_nor_debug target
west build -b evkbmimxrt1170 examples/demo_apps/hello_world -Dcore_id=cm7 --config flexspi_nor_debug
# Switch device
west build -b frdmk22f examples/demo_apps/hello_world --device MK22F12810
west build -b evkbmimxrt1170 examples/demo_apps/hello_world --device=MIMXRT1175 -Dcore_id=cm7 --config flexspi_nor_debug
For shield, please use the --shield to specify the shield to build, like
west build -b mimxrt700evk --shield a8974 examples examples/issdk_examples/sensors/fxls8974cf/fxls8974cf_poll -Dcore_id=cm33_core0
If you want to get available commands for different build config combinations supported by the example and the toolchain, you can run the command below. Please note that @${core_id} suffix for board is only needed for multicore devices.
  west list_project -p examples/mbedtls_examples/mbedtls_selftest -b evkbmimxrt1170@cm7 -t mdk
Here is the output:
INFO: [   1][west build -p always examples/mbedtls_examples/mbedtls_selftest --toolchain mdk --config debug -b evkbmimxrt1170 -Dcore_id=cm7]
INFO: [   2][west build -p always examples/mbedtls_examples/mbedtls_selftest --toolchain mdk --config flexspi_nor_debug -b evkbmimxrt1170 -Dcore_id=cm7]
INFO: [   3][west build -p always examples/mbedtls_examples/mbedtls_selftest --toolchain mdk --config flexspi_nor_release -b evkbmimxrt1170 -Dcore_id=cm7]
INFO: [   4][west build -p always examples/mbedtls_examples/mbedtls_selftest --toolchain mdk --config release -b evkbmimxrt1170 -Dcore_id=cm7]
INFO: [   5][west build -p always examples/mbedtls_examples/mbedtls_selftest --toolchain mdk --config sdram_debug -b evkbmimxrt1170 -Dcore_id=cm7]
INFO: [   6][west build -p always examples/mbedtls_examples/mbedtls_selftest --toolchain mdk --config sdram_release -b evkbmimxrt1170 -Dcore_id=cm7]
For multi-projects example build, you can build all projects by adding --sysbuild for main project . For example:
west build -b evkbmimxrt1170 --sysbuild ./examples/multicore_examples/hello_world/primary -Dcore_id=cm7 --config flexspi_nor_debug -p always
For more details, please refer to System build.
Flash and Debug The Example
Flash
For an example that have been compiled successfully, use the command to flash the image:
west flash
To specify the build directory, use --build-dir (or -d).
Debug
Here are the typical supported debugger servers:
Please install LinkServer or JLink and add it to PATH environment variable firstly, then specify debug server with -r.
If you want to configure debug server, please refer to Flash and Debug Data.
Flash the hello_world example:
west flash -r linkserver
Start a gdb interface by following command:
west debug -r linkserver
All of the above west commands can only be run in mcuxsdk west workspace. If you want to use them outside the workspace, please run
mcuxsdk/mcux-env.cmdin Windows Command Prompt orsource mcuxsdk/mcux-env.shin Linux terminal to activate the commands.
Flash and Debug CMake Configuration Data
MCUXpresso SDK supports to set up customized configuration for board flash runners. Such configuration is stored in ${SdkRootDirPath}/examples/_boards/<board>/board_runner.cmake. It is loaded by ${SdkRootDirPath}/cmake/extension/run.cmake which is used to get runner type and arguments.
Here is an example:
# set runner speicfic arguments
board_runner_args(jlink "--device=${CONFIG_MCUX_TOOLCHAIN_JLINK_CPU_IDENTIFIER}")
board_runner_args(linkserver "--device=${CONFIG_MCUX_HW_DEVICE_ID}:MIMXRT1170-EVKB")
board_runner_args(linkserver "--core=${core_id}")
# load board supported runner cmake file
include(${SdkRootDirPath}/cmake/extension/runner/jlink.board.cmake)
include(${SdkRootDirPath}/cmake/extension/runner/linkserver.board.cmake)
In this example, board_runner_args is used to pass runner-specific arguments, runner cmake files are load from ${SdkRootDirPath}/cmake/extension/runner/ which indicates the supported runners.
The first included runner cmake will be set as the default runner for both flash and debug.
If you want to choose a different runner, you can set following variables in the board variable.cmake:
mcux_set_variable(BOARD_FLASH_RUNNER "linkserver")
mcux_set_variable(BOARD_DEBUG_RUNNER "jlink")
To make the runner get correct flash address, the Kconfig option FLASH_BASE_ADDRESS shall be set correct value for each device core in devices/${soc_portfolio}/${soc_series}/${device}/(${core_id})/prj.conf:
CONFIG_FLASH_BASE_ADDRESS=0x30000400
If your example has different flash base address, please override the above value in your example specific prj.conf.
Project Segment
MCUXpresso SDK is composed of hundreds of devices and boards, thousands of components and ten thousands of examples. Examples on the devices and boards have many shared data like core related settings, common build target settings, device headers and configurations, board files, clock and pin mux. Project segment data section is an abstraction of common shared project data. It is introduced to avoid data duplication.
CMake
Like the component, in cmake files, project segment data shall be recorded inside a if-endif guard. The if condition shall be with prefix CONFIG_MCUX_PRJSEG_, right after it is the project segment name.
Here is one project segment cmake example:
if (CONFIG_MCUX_PRJSEG_module.board.clock)  # project segment name is module.board.clock
    # project segment data
    mcux_add_source(
        BASE_PATH ${SdkRootDirPath}
        SOURCES boards/${board}/clock_config.h
                boards/${board}/clock_config.c
    )
    mcux_add_include(
        BASE_PATH ${SdkRootDirPath}
        INCLUDES boards/${board}
    )
endif()
Kconfig
In Kconfig, symbol for a project segment shall start with MCUX_PRJSEG_ to be identical with cmake project segment name. Project segment configuration and dependency shall be recorded following the below pattern:
config MCUX_PRJSEG_module.board.clock
    bool "Use default clock files"
    imply MCUX_COMPONENT_driver.clock
    if MCUX_PRJSEG_module.board.clock
    endif
Unlike the component dependency, the dependency for project segment is simple, just several parallel imply to state that the project segment depends on some components and maybe other project segment to work. Since it is frequently occuring cases that some examples on certain boards need to modify some predefined project segment dependencies, please use imply instead of select for project segment dependencies because select once is set to true then cannot be deselected anymore.
Predefined Project Segments
There are already many project segments defined in mcuxsdk, here is the frequently used project segments table.
Location  | 
Functionality  | 
|---|---|
arch  | 
The predefined settings and configurations of different SOC architectures  | 
examples/_common  | 
Commonly shared example board modules like board file, pinmux, clock config, etc.  |