Hardware requirements
Micro USB cable
evkmimxrt1180 board
Personal Computer
One of the following modules:
Embedded Artists 1XK M.2 Module (EAR00385) - direct M2 connection.
Embedded Artists 1ZM M.2 Module (EAR00364) - direct M2 connection.
Embedded Artists 2EL M.2 Module (Rev-A1) - direct M2 connection.
Embedded Artists 2LL M.2 Module (EAR00500) - direct M2 connection.
Board settings
Before building the example application select Wi-Fi module macro in the app_bluetooth_config.h. (see #define WIFI_
Jumper settings for RT1180:
connect J1 1-2 connect J2 with external power(controlled by SW1) connect J76 2-3 connect J57 2-3
Hardware rework guide:
The hardware should be reworked according to the hardware rework guide for evkmimxrt1180 and Murata 1XK M.2 Adapter in document Hardware Rework Guide for EdgeFast BT PAL. The hardware should be reworked according to the hardware rework guide for evkmimxrt1180 and Murata 1ZM M.2 Adapter in document Hardware Rework Guide for EdgeFast BT PAL. The rework guide for evkmimxrt1180 and Murata 2EL M.2 Adapter is same as evkmimxrt1180 and Murata 1ZM M.2 Adapter.
Murata Solution Board settings
Murata uSD-M.2 adapter resource page: https://www.murata.com/en-us/products/connectivitymodule/wi-fi-bluetooth/overview/lineup/usd-m2-adapter Murata uSD-M.2 adapter datasheet: https://www.murata.com/-/media/webrenewal/products/connectivitymodule/asset/pub/rfm/data/usd-m2_revb1.ashx Embedded Artists M.2 module resource page: https://www.embeddedartists.com/m2 Embedded Artists 1XK module datasheet: https://www.embeddedartists.com/doc/ds/1XK_M2_Datasheet.pdf Embedded Artists 1ZM module datasheet: https://www.embeddedartists.com/doc/ds/1ZM_M2_Datasheet.pdf Embedded Artists 2EL module datasheet: https://www.embeddedartists.com/doc/ds/2EL_M2_Datasheet.pdf Embedded Artists 2LL module datasheet: https://www.embeddedartists.com/wp-content/uploads/2024/12/2LL_M2_Datasheet.pdf
Note:
To ensure that the LITTLEFS flash region has been cleaned, all flash sectors need to be erased before downloading example code. For Peripheral DMA to be used, the application core must first gain TRDC access from edgelock FW, so this demo must be runnning with edgelock FW alive. Whole memory must be erased before this demo is flashed. After downloaded binary into Quad SPI Flash and boot from Quad SPI Flash directly, please reset the board by pressing SW3 or power off and on the board to run the application.