Hardware requirements
Micro USB cable
EVK-MIMXRT595 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J40) on the board
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the clockout demo in the terminal window:
Clock Output Driver Example.
Please choose one output clock.
	A -- OSC_CLK Clock.
	B -- Low Power Oscillator Clock.
	C -- FRO_DIV2 Clock.
	D -- Main Clock.
	E -- Dsp Main Clock.
	F -- Main System PLL.
	G -- SYSPLL0 AUX0_PLL_Clock.
	H -- DSP PLL Clock.
	I -- SYSPLL0 AUX1_PLL_Clock.
	J -- AUDIO PLL Clock.
	K -- 32 KHz RTC Clock.
To measure the output clock signal, please use the oscilloscope to probe JP27_2.