Hardware requirements
Type-C USB cable
FRDM-MCXE31B board
Personal Computer
Board settings
MASTER(LPI2C_1)                connect to        SLAVE(LPI2C_0)
Pin Name    Board Location                      Pin Name    Board Location
SCL         J2 pin 20                           SCL         J7 pin 6
SDA         J2 pin 18                           SDA         J7 pin 8
Other jumpers keep default configuration.
Prepare the Demo
Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following message shows in the terminal if the example runs successfully.
LPI2C example -- MasterFunctionalInterrupt_SlaveFunctionalInterrupt.
Master will send data :
0x 0  0x 1  0x 2  0x 3  0x 4  0x 5  0x 6  0x 7
0x 8  0x 9  0x a  0x b  0x c  0x d  0x e  0x f
0x10  0x11  0x12  0x13  0x14  0x15  0x16  0x17
0x18  0x19  0x1a  0x1b  0x1c  0x1d  0x1e  0x1f
Slave received data :
0x 0  0x 1  0x 2  0x 3  0x 4  0x 5  0x 6  0x 7
0x 8  0x 9  0x a  0x b  0x c  0x d  0x e  0x f
0x10  0x11  0x12  0x13  0x14  0x15  0x16  0x17
0x18  0x19  0x1a  0x1b  0x1c  0x1d  0x1e  0x1f
This time , slave will send data:
0xff  0xfe  0xfd  0xfc  0xfb  0xfa  0xf9  0xf8
0xf7  0xf6  0xf5  0xf4  0xf3  0xf2  0xf1  0xf0
0xef  0xee  0xed  0xec  0xeb  0xea  0xe9  0xe8
0xe7  0xe6  0xe5  0xe4  0xe3  0xe2  0xe1  0xe0
Master received data :
0xff  0xfe  0xfd  0xfc  0xfb  0xfa  0xf9  0xf8
0xf7  0xf6  0xf5  0xf4  0xf3  0xf2  0xf1  0xf0
0xef  0xee  0xed  0xec  0xeb  0xea  0xe9  0xe8
0xe7  0xe6  0xe5  0xe4  0xe3  0xe2  0xe1  0xe0
End of I2C example .