Hardware requirements
Type-C USB cable
FRDM-MCXW23 Board
Personal Computer
Board settings
Use the default jumper settings.
Prepare the Demo
Connect a USB cable between the host PC and the FRDM board J10.
Open a serial terminal with the following settings
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Build and download the application
Start a debug session or press the reset button
Running the demo
The clock can be measured with an oscilloscope on J1-6.
The log below shows the output of the clockout demo in the terminal window:
Clock Output Driver Example.
Please choose one output clock.
	A -- Main Clock.
	B -- CLKIN Clock.
	C -- FRO 32 MHz Clock.
	D -- FRO 1 MHz Clock.
	E -- FRO 24 MHz clock.
	F -- Oscillator 32 kHz Clock.