Hardware requirements

  • Mini USB cable

  • LPCXpresso55s69 board

  • Personal Computer

Board settings

No special is needed.

Prepare the Demo

Note: MCUXpresso IDE project default debug console is semihost

  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Reset the SoC and run the project.

Running the demo

When the demo runs successfully, the log would be seen on the OpenSDA terminal like:

USART DMA example
Send back received data
Echo every 8 characters

When you input 8 characters, system will echo it by USART and them would be seen on the OpenSDA terminal.