Hardware requirements
MIMXRT700 board
Mini/micro USB cable
Personal Computer
Board settings
Make sure the board is setup to boot from flash.
MCUBoot layout
In all cases, the MCUBOOT bootloader reserves 256kB at the beginning of the external flash followed by 2MB slots for application.
Region  | 
From  | 
To  | 
Size  | 
|---|---|---|---|
MCUboot code  | 
0x28000000  | 
0x2803FFFF  | 
256kB  | 
Primary slot  | 
0x28040000  | 
0x2823FFFF  | 
2048kB  | 
Secondary slot  | 
0x28240000  | 
0x2843FFFF  | 
2048kB  | 
MCUBoot header size is set to 1024 bytes
Signing algorithm is ECDSA-P256
Write alignment is 4 bytes
MCUBoot is configured to use its
DIRECT_XIPimage handling strategy together with FlexSPI flash remapping
Image signing example
imgtool sign   --key sign-ecdsa-p256-priv.pem
               --align 4
               --version 1.1
               --slot-size 0x200000
               --header-size 0x400
               --pad-header
               ota_mcuboot_basic.bin
               ota_mcuboot_basic.SIGNED.bin
Note that for the first image flashed manually together with the bootloader
additional imgtool options --pad and --confirm must be used. Otherwise
the bootloader would reject the image for missing data in the trailer area.