EdgeLock 2GO Blob Test (NS)
This is a test suite which imports and validates EL2GO blobs and their usage with PSA.
Workspace structure:
tfm_s_crypto_client: Project creating the static library required by the secure processing environment (S)
el2go_blob_test_s: Project running in the secure processing environment (S)
el2go_blob_test_ns: Project running in the non-secure processing environment (NS)
Additional information about EdgeLock 2GO Provisioning for MCUs can be found in AN14624 under the following link https://www.nxp.com/webapp/Download?colCode=AN14624&location=null.
Definitions
[GITHUB]: refers to the case where the MCU SDK is cloned as GitHub Repository and the EdgeLock 2GO application is build using meta build sytem. More details can be found in https://mcuxpresso.nxp.com/mcuxsdk/latest/html/gsd/repo.html.
[ZIP]: refers to the case whete MCU SDK is generated as ZIP package and the EdgeLock 2GO application is imported and build in one of supported IDEs. More details can be found in https://mcuxpresso.nxp.com/mcuxsdk/latest/html/gsd/package.html.
Prerequisites
Active EdgeLock 2GO account
Any serial communicator
Python >= 3.9 with packages from requirements.txt
[MCXN] SPSDK or standalone Provisioning Firmware
NOTE: The Python scripts refered to in this example can be found in the scripts folder in the example directory.
Hardware requirements
FRDM-RW612, RD-RW61X-BGA, MCX-N5XX-EVK, MCX-N9XX-EVK or FRDM-MCXN947 or FRDM-MCXN236 board
USB-C (FRDM-RW612, FRDM-MCXN947, FRDM-MCXN236) or Micro-USB (RD-RW61X-BGA, MCX-N5XX-EVK or MCX-N9XX-EVK) cable
Personal Computer
Board settings
[RW61X] The board must be provisioned with an OEM Auth Key Hash.
[MCXN] The board must be provisioned with an OEM Auth Key Hash and an OEM FW Decryption Key in OEM OPEN lifecycle.
Preparing the application
Create device specific blobs:
Inline mode:
Obtain a RTP JSON file from EdgeLock 2GO containing the desired blobs for your board
[MCXN] Connect your board and rewrap all the blobs in the RTP JSON file:
el2go_blob_rewrap.py [RAW_RTP_JSON_PATH] [PROVISIONING_FIRMWARE_PATH] [COM_PORT] [RTP_JSON_PATH] [DEVICE_NAME]
Run the file trough the preprocessor:
el2go_blob_test_pre.py [RTP_JSON_PATH]
[MCXN] Memory mode:
Create a device group in EdgeLock 2GO containing the desired blobs for your board
Provision the blobs to your board via the
el2go-hostapp from SPSDK (set thesecure_objects_addressproperty of the config file to0x001C0000or ‘’ for FRDM-MCXN236 use0x000C4000):el2go-host provision-device -p [COM_PORT] --config [CONFIG_PATH] --workspace [WORKSPACE_PATH]
Run the RTP JSON file downloaded by
el2go-hosttrough the preprocessor, specifying the memory location method and address:el2go_blob_test_pre.py [WORKSPACE_PATH]/provisionings.json --storage_mode memory --blob_address 0x001C0000
For FRDM-MCXN236:
el2go_blob_test_pre.py [WORKSPACE_PATH]/provisionings.json --storage_mode memory --blob_address 0x000C4000
NOTE: This method only works for a maximum of 16 blobs, not exceeding 16KB in total.
ATTENTION: Make sure the lifecycle and OEM Auth Key Hash of your blobs match the one provisioned to the board. Attempting to rewrap/provision blobs with an OEM CLOSED lifecycle to an OEM OPEN board will change the lifecycle!
[OPTIONAL] Enable all possible variations:
By default, the test suite only runs variations that are expected to pass for a given board. If you want to run all possible tests instead, you can specify that:
[GITHUB] By disabling the Kconfig symbol
RUN_VERIFIED_ONLY[ZIP] By defining
RUN_VERIFIED_ONLYas0inmcux_config.h
Note: If you input an entirely unsupported blob, the testcase will still run and fail, even if
RUN_VERIFIED_ONLYis enabled.Enable secure boot:
To correctly run the application on RW61X, the secure boot mode on the device needs to be enabled. For MCXN, this is optional.
The bootheader needs to be removed from the S image, it has to be merged with the NS image and the resulting image must be signed with the OEM key. Additionaly, if the application is supposed to run in the OEM CLOSED life cycle, the image needs to be encrypted with the OEM FW encryption key and loaded as an SB3.1 container.
Details on how to execute these steps can be found in the following documents:
[RW61X] Application note AN13813 “Secure boot on RW61x” (“Documentation->Secure Files” section).
[MCXN] Application note AN14148 “Enabling Secure boot and Trust Provisioning on MCX N series” (“Documentation->Secure Files” section).
[OPTIONAL] Enable support for large blobs:
In order to maximize the TF-M ITS performance, the maximum supported blob size is set to 2908 bytes. In case you want to support larger blobs (8K is the maximum size supported by PSA), you need to adjust two TF-M parameters.
middleware/tfm/tf-m/platform/ext/target/nxp/[BOARD]/config_tfm_target.h
#define ITS_MAX_ASSET_SIZE 3 * 0xC00middleware/tfm/tf-m/platform/ext/target/nxp/[BOARD]/partition/flash_layout.h
#define TFM_HAL_ITS_SECTORS_PER_BLOCK (3)After that, you can enable the testing of large blobs:
[GITHUB] By enabling the Kconfig symbol
LARGE_BLOBS_ENABLED[ZIP] By defining
LARGE_BLOBS_ENABLEDas1inmcux_config.h
Build the application:
[GITHUB] Compile the el2go_blob_test_ns project with your desired toolchain using
--sysbuild.[ZIP] First compile the el2go_blob_test_s project and then the el2go_blob_test_ns project.
Connect the USB-C (FRDM-RW612, FRDM-MCXN947, FRDM-MCXN236) or Micro-USB (RD-RW61X-BGA, MCX-N5XX-EVK or MCX-N9XX-EVK) cable to the PC host and the MCU-Link USB port (J10 [FRDM-RW612], J7 [RD-RW61X-BGA], J5 [MCX-N5XX-EVK or MCX-N9XX-EVK] or J17 [FRDM-MCXN947]) on the board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the application to the target board:
[GITHUB]
west flashwill download both the S and the NS image.[ZIP] Downloading the S image will also download the NS image.
Press the reset button on the board or launch the debugger in your IDE to run the application.
[OPTIONAL] Convert results to JUnit:
If you capure the console output of the application, you can feed it into the postprocessor to recieve the results in the JUnit format:
el2go_blob_test_post.py [CONSOLE_OUTPUT_PATH] [JUNIT_OUT_PATH]
Running the application
The log below shows the output of the application in the terminal window.
Booting the S project (TF-M initialization):
Booting TF-M v2.1.1
[WRN] This device was provisioned with dummy keys. This device is NOT SECURE
[Sec Thread] Secure image initializing!
TF-M Float ABI: Hard
Lazy stacking enabled
[INF][PS] Encryption alg: 0x5500100
Jumping to the NS project, running the blob test suite:
#### Start EL2GO blob tests ####
Running test suite GENERIC (EL2GO_BLOB_TEST_GENERIC_XXXX)
> Executing test EL2GO_BLOB_TEST_GENERIC_0001
Description: 'External CERTIFICATE 425B EXPORT NONE'
Test EL2GO_BLOB_TEST_GENERIC_0001 - PASSED (16 ms)
> Executing test EL2GO_BLOB_TEST_GENERIC_0002
Description: 'External KEYPAIR BRAINPOOLP384R1 SIGVERMSG ECDSAANYHASH'
> Executing variation SHA_224
Variation SHA_224 - PASSED (126 ms)
> Executing variation SHA_512_224
Variation SHA_512_224 - PASSED (124 ms)
> Executing variation SHA_256
Variation SHA_256 - PASSED (126 ms)
> Executing variation SHA_512_256
Variation SHA_512_256 - PASSED (126 ms)
> Executing variation SHA_384
Variation SHA_384 - PASSED (125 ms)
> Executing variation SHA_512
Variation SHA_512 - PASSED (125 ms)
Test EL2GO_BLOB_TEST_GENERIC_0002 - PASSED (814 ms)
> Executing test EL2GO_BLOB_TEST_GENERIC_0003
Description: 'External KEYPAIR ECCMONTDH25519 DERIVE ECDH'
Test EL2GO_BLOB_TEST_GENERIC_0003 - PASSED (52 ms)
> Executing test EL2GO_BLOB_TEST_GENERIC_0004
Description: 'Internal KEYPAIR NISTP256 SIGHASH ECDSASHA256'
Test EL2GO_BLOB_TEST_GENERIC_0004 - PASSED (21 ms)
> Executing test EL2GO_BLOB_TEST_GENERIC_0005
Description: 'Internal KEYPAIR NISTP256 SIGHASH ECDSASHA256'
Test EL2GO_BLOB_TEST_GENERIC_0005 - PASSED (19 ms)
> Executing test EL2GO_BLOB_TEST_GENERIC_0006
Description: 'External CERTIFICATE 420B EXPORT NONE'
psa_import_key returned -149
Failed at psa_blob_export_test:1526
Test EL2GO_BLOB_TEST_GENERIC_0006 - FAILED (4 ms)
1 of 6 FAILED
5 of 6 PASSED
Test suite GENERIC (EL2GO_BLOB_TEST_GENERIC_XXXX) - FAILED (926 ms)
#### Summary ####
Test suite GENERIC (EL2GO_BLOB_TEST_GENERIC_XXXX) - FAILED (926 ms)
#### EL2GO blob tests finished ####