1. General description

The purpose of this demo is to demonstrate the capabilities of the NXP Wireless SoC when used as a Zigbee NCP together with a Zigbee Coordinator application running on the iMX8 (or x86) platform under Linux.

The demo showcases how to connect a Zigbee End Device to the network formed by the Zigbee Coordinator and toggle the RGB LED available on the device.

A step-by-step guide to the hardware and software configurations are provided, as well as the steps needed to be executed in order to get the boards up and running.

List of supported NXP Wireless SoC to act as coprocessor:

  • K32W148

  • MCXW71

  • K32W061

2. Required Hardware

  • 1 x iMX8M-EVK board running Linux - Host

  • 1 x K32W148-EVK board or 1 x K32W061 DK6 board or 1 x FRDM-MCXW71 board – Zigbee NCP coprocessor

  • 1 x K32W061 DK6 board - Zigbee End Device

2.1. iMX8 board configuration

Ensure that SW801 on the IMX8 EVK board is configured for SD card boot. For more information see the following starting guide for iMX8M EVK board: https://www.nxp.com/document/guide/getting-started-with-the-i-mx-8m-plus-evk:GS-iMX-8M-Plus-EVK.

2.2. Zigbee NCP coprocessor board configuration

The Zigbee NCP coprocessor can be either of the SoCs listed in the supported platforms. After the board is properly configured it should be connected to the iMX8M board using a standard micro USB cable that will be also used for power delivery to the board.

2.2.1 K32W148 EVK/FRDM-MCXW71 board configuration

For the detailed K32W148 EVK board configuration, see the “Getting Started with MCUXpresso SDK for K32W148-EVK.pdf” guide, part of the K32W148 SDK.

For the detailed FRDM-MCXW71 board configuration, see the “Getting Started with MCUXpresso SDK for FRDM-MCXW71.pdf” guide, part of the FRDMMCXW71 SDK.

Ensure that the debug firmware on the board is J-Link. If this is not the case, follow the steps in chapter 7 of the aforementioned document to update the firmware accordingly.

The board should be updated with the binary image `k32w148evk_zigbee_coprocessor_bm.axf`/`frdmmcxw71_zigbee_coprocessor_bm.axf`, image which contains the Zigbee NCP. This image can be obtained from the Zigbee application wireless_examples/zigbee/zigbee_coprocessor, application that is part of the K32W148/FRDMMCXW71 SDK.

2.2.2 K32W061 DK6 board configuration

For the detailed board configuration, see the “Getting Started with MCUXpresso SDK for K32W061.pdf” guide, part of the K32W061 SDK.

Ensure that the debug firmware on the board is DK6 Flash Programmer. For additional information, please you the aforementioned document together with the DK6-UG-3127-Production-Flash-Programmer.pdf document.

The board should be updated with the binary image `k32w061dk6_zigbee_coprocessor_bm.axf`, image which contains the Zigbee NCP. This image can be obtained from the Zigbee application wireless_examples/zigbee/zigbee_coprocessor, application that is part of the K32W061 SDK.

2.3. K32W061 DK6 board configuration (ZED RX ON)

For the detailed board configuration see the “Getting Started with MCUXpresso SDK for K32W061.pdf” guide, part of the K32W061 SDK

3. Building

The building process has small differences depending on the host (iMX8 or x86) on which the Zigbee Coordinator application is running on. The user has also the option to cross-compile the Coordinator application under x86 Linux distribution

Environment Setup

The NCP Host offers toolchain files that can be used to compile and cross compile the applications. They are available at ZIGBEE_BASE/platform/NCP_HOST/cmake/toolchains and should be provided to cmake -DCMAKE_TOOLCHAIN_FILE command line argument:

  • x86_64-linux-gnu.cmake - toolchain file for x86 compile

  • arm-linux - toolchain file for imx8 cross-compile

The armgcc toolchain was obtained from official Arm GNU Toolchain website and by default the toolchain file relies on this particular configuration. User can change through environment variables and cmake arguments the default behavior.

  • ARMGCC_DIR - path to installed toolchain

  • TOOLCHAIN_NAME - toolchain name

The Mbedtls package is required for the encryption/decryption capabilities needed to obtain a secured Serial Link. There are three options to obtain the mbedlts library, options configurable through cmake command line arguments:

  • CONFIG_MBEDTLS_SOURCE=SDK - Mbedtls package is obtained from MCUXPRESSO SDK

  • CONFIG_MBEDTLS_SOURCE=GIT - Mbedtls package is retrieved from git official repository

  • CONFIG_MBEDTLS_SOURCE=SYSTEM - Mbedtls package is used as a preinstalled package

Examples for cross-compile:

  • cmake .. -DCMAKE_TOOLCHAIN_FILE=$PWD/../../../../platform/NCP_HOST/cmake/toolchains/arm-linux.cmake -DCONFIG_MBEDTLS_SOURCE=SYSTEM - Cross-compile for imx8 with mbedtls as a preinstalled package. The toolchain file provided detects that machine type is imx8

  • cmake .. -DCMAKE_TOOLCHAIN_FILE=$PWD/../../../../platform/NCP_HOST/cmake/toolchains/arm-linux.cmake -DTOOLCHAIN_NAME=aarch64-linux-gnu - Cross-compile for imx8 with toolchain available for Ubuntu 22.04

3.1. iMX8 platform

Create a directory `out` under the `build_linux` directory and issue the cmake command with the `MACHINE_TYPE=imx8` option. The mbedtls package is preinstalled in the provided Board Support Package (BSP).

>$ cd out ; cmake .. -DMACHINE_TYPE=imx8 
-- The C compiler identification is GNU 13.2.1
-- The CXX compiler identification is GNU GNU 13.2.1
-- Detecting C compiler ABI info
-- Detecting C compiler ABI info - done
-- Check for working C compiler: /usr/bin/aarch64-none-linux-gnu-gcc - skipped
-- Detecting C compile features
-- Detecting C compile features - done
-- Detecting CXX compiler ABI info
-- Detecting CXX compiler ABI info - done
-- Check for working CXX compiler: /usr/bin/aarch64-none-linux-gnu-c++ - skipped
-- Detecting CXX compile features
-- Detecting CXX compile features - done
-- Using preinstalled MbedTLS package /usr/local/mbedtls/cmake
-- Configuring done
-- Generating done
-- Build files have been written to: /home/zb-linux-coord/zigbee/examples/zigbee_coordinator/build_linux/out 

Issue the command make to execute the newly generated Makefile.

>[b06830_local@fsr-ub1864-125 out]$ make 

[  0%] Building C object CMakeFiles/pdum_static.dir/home/zb-linux-coord/zigbee/platform/NCP_HOST/framework/PDUM/Source/pdum.c.o
[  1%] Building C object CCMakeFiles/pdum_static.dir/home/zb-linux-coord/zigbee/platform/NCP_HOST/framework/PDUM/Source/pdum_apl.c.o
[  2%] Building C object CMakeFiles/pdum_static.dir/home/zb-linux-coord/zigbee/platform/NCP_HOST/framework/PDUM/Source/pdum_dbg.c.o
[  3%] Building C object CMakeFiles/pdum_static.dir/home/zb-linux-coord/zigbee/platform/NCP_HOST/framework/PDUM/Source/pdum_nwk.c.o
[  4%] Linking C static library pdum/lib/libpdum.a
[  4%] Built target ncphost-PDUM
[  5%] Building C object CMakeFiles/zb_coord_linux.dir/home/zb-linux-coord/zigbee/examples/zigbee_coordinator/zigbee/examples/zigbee_coordinator/src/linux/pdum_gen_glue.c.o
[  6%] Building C object CMakeFiles/zb_coord_linux.dir/home/zb-linux-coord/zigbee/examples/zigbee_coordinator/zigbee/examples/zigbee_coordinator/src/app_coordinator_ncp.c.o
. . .
[ 99%] Building C object CMakeFiles/zb_coord_linux.dir/home/zb-linux-coord/zigbee/examples/zigbee_coordinator/zigbee/ZCL/Clusters/OTA/Source/OTA.c.o
[100%] Linking C executable zb_coord_linux
[100%] Built target zb_coord_linux

3.2. x86 platform

The Zigbee Coordinator demo application was compiled and verified on a x86 Linux distribution (Ubuntu 22.04.2 LTS). The CMakeFile of the application determines as a prebuild step if the application was provided as part of a MCUXPRESSO SDK package or as standalone Zigbee module. Depending on the SDK package existence, the Mbedtls can be used either from within the SDK package, as a preinstalled package or it can be obtained from official git repository (version 2.28.0).

MCUXPRESSO SDK package

Create a directory `out` under the `build_linux` directory and issue the cmake command. The output will showcase the MCUXPRESSO SDK location and the mbedtls usage from within the SDK package.

>$ cd out ; cmake ..
-- The C compiler identification is GNU 11.4.0
-- The CXX compiler identification is GNU 11.4.0
-- Detecting C compiler ABI info
-- Detecting C compiler ABI info - done
-- Check for working C compiler: /usr/bin/cc - skipped
-- Detecting C compile features
-- Detecting C compile features - done
-- Detecting CXX compiler ABI info
-- Detecting CXX compiler ABI info - done
-- Check for working CXX compiler: /usr/bin/c++ - skipped
-- Detecting CXX compile features
-- Detecting CXX compile features - done
-- Found MCUXPRESSO SDK
-- Using SDK root path /home/mcu-sdk
-- Build mbedtls from SDK source code
-- Configuring done
-- Generating done
-- Build files have been written to: /home/mcu-sdk/middleware/wireless/zigbee/examples/zigbee_coordinator/build_linux/out 

Issue the command make to execute the newly generated Makefile.

>[b06830_local@fsr-ub1864-125 out]$ make 

[  1%] Building C object CMakeFiles/pdum_static.dir/home/mcu-sdk/middleware/wireless/zigbee/platform/NCP_HOST/framework/PDUM/Source/pdum.c.o
[  1%] Building C object CMakeFiles/pdum_static.dir/home/mcu-sdk/middleware/wireless/zigbee/platform/NCP_HOST/framework/PDUM/Source/pdum_apl.c.o
[  2%] Building C object CMakeFiles/pdum_static.dir/home/mcu-sdk/middleware/wireless/zigbee/platform/NCP_HOST/framework/PDUM/Source/pdum_dbg.c.o
[  2%] Building C object CMakeFiles/pdum_static.dir/home/mcu-sdk/middleware/wireless/zigbee/platform/NCP_HOST/framework/PDUM/Source/pdum_nwk.c.o
[  3%] Linking C static library pdum/lib/libpdum.a
[  3%] Built target ncphost-PDUM
[  3%] Building C object mbedtls/library/CMakeFiles/ncp-host-mbedcrypto.dir/aes.c.o
. . .
[ 99%] Building C object CMakeFiles/zb_coord_linux.dir/home/mcu-sdk/middleware/wireless/zigbee//examples/zigbee_coordinator/zigbee/ZCL/Clusters/OTA/Source/OTA.c.o
[100%] Linking C executable zb_coord_linux
[100%] Built target zb_coord_linux

The following error might appear, which indicates that the SDK Mbedtls version is too old:

-- SDK MBEDTLS version is below 2.28, use CONFIG_MBEDTLS_SOURCE as GIT or SYSTEM instead
CMake Error at /home/mcu-sdk/middleware/wireless/zigbee/platform/NCP_HOST/cmake/NxpZbNcpHostConfig.cmake:46 (message):
Call Stack (most recent call first):
  CMakeLists.txt:32 (include)

If so, switch the Mbedtls origin to GIT instead, by building with the following commands:

>$ cd out ; cmake -DCONFIG_MBEDTLS_SOURCE=GIT ..
-- The C compiler identification is GNU 11.4.0
-- The CXX compiler identification is GNU 11.4.0
-- Detecting C compiler ABI info
-- Detecting C compiler ABI info - done
-- Check for working C compiler: /usr/bin/cc - skipped
-- Detecting C compile features
-- Detecting C compile features - done
-- Detecting CXX compiler ABI info
-- Detecting CXX compiler ABI info - done
-- Check for working CXX compiler: /usr/bin/c++ - skipped
-- Detecting CXX compile features
-- Detecting CXX compile features - done
-- Found MCUXPRESSO SDK internal
-- Using SDK root path /home/mcu-sdk
-- Populate mbedtls repository
Cloning into 'repo'...
HEAD is now at 8b3f26a5ac Merge pull request #868 from ARMmbed/mbedtls-2.28.0rc0-pr
...

-- Found Python3: /usr/bin/python3.10 (found version "3.10.12") found components: Interpreter
-- Performing Test C_COMPILER_SUPPORTS_WFORMAT_SIGNEDNESS
-- Performing Test C_COMPILER_SUPPORTS_WFORMAT_SIGNEDNESS - Success
-- Looking for pthread.h
-- Looking for pthread.h - found
-- Performing Test CMAKE_HAVE_LIBC_PTHREAD
-- Performing Test CMAKE_HAVE_LIBC_PTHREAD - Success
-- Found Threads: TRUE


-- Configuring done
-- Generating done
-- Build files have been written to: /home/zb-linux-coord/zigbee/examples/zigbee_coordinator/build_linux/out 

Then issue the command make as usual to execute the newly generated Makefile.

Standalone Zigbee module

The Zigbee coordinator application can be obtained and compiled as a standalone application, without the presence of a MCUXPRESSO SDK. The mbedtls package is required as a preinstalled package or can be configured through user environment variables `export MBEDTLS_ORIGIN=GIT` to be obtained from official repository.

Create a directory out under the build_linux directory and issue the cmake command.

>$ cd out ; cmake ..
-- The C compiler identification is GNU 11.4.0
-- The CXX compiler identification is GNU 11.4.0
-- Detecting C compiler ABI info
-- Detecting C compiler ABI info - done
-- Check for working C compiler: /usr/bin/cc - skipped
-- Detecting C compile features
-- Detecting C compile features - done
-- Detecting CXX compiler ABI info
-- Detecting CXX compiler ABI info - done
-- Check for working CXX compiler: /usr/bin/c++ - skipped
-- Detecting CXX compile features
-- Detecting CXX compile features - done
-- Populate mbedtls repository
Cloning into 'repo'...
HEAD is now at 8b3f26a5ac Merge pull request #868 from ARMmbed/mbedtls-2.28.0rc0-pr
...

-- Found Python3: /usr/bin/python3.10 (found version "3.10.12") found components: Interpreter
-- Performing Test C_COMPILER_SUPPORTS_WFORMAT_SIGNEDNESS
-- Performing Test C_COMPILER_SUPPORTS_WFORMAT_SIGNEDNESS - Success
-- Looking for pthread.h
-- Looking for pthread.h - found
-- Performing Test CMAKE_HAVE_LIBC_PTHREAD
-- Performing Test CMAKE_HAVE_LIBC_PTHREAD - Success
-- Found Threads: TRUE


-- Configuring done
-- Generating done
-- Build files have been written to: /home/zb-linux-coord/zigbee/examples/zigbee_coordinator/build_linux/out 

Issue the command make to execute the newly generated Makefile.

>[b06830_local@fsr-ub1864-125 out]$ make 

[  0%] Building C object CMakeFiles/pdum_static.dir/home/zb-linux-coord/zigbee/platform/NCP_HOST/framework/PDUM/Source/pdum.c.o
[  1%] Building C object CCMakeFiles/pdum_static.dir/home/zb-linux-coord/zigbee/platform/NCP_HOST/framework/PDUM/Source/pdum_apl.c.o
[  2%] Building C object CMakeFiles/pdum_static.dir/home/zb-linux-coord/zigbee/platform/NCP_HOST/framework/PDUM/Source/pdum_dbg.c.o
[  3%] Building C object CMakeFiles/pdum_static.dir/home/zb-linux-coord/zigbee/platform/NCP_HOST/framework/PDUM/Source/pdum_nwk.c.o
[  4%] Linking C static library pdum/lib/libpdum.a
[  4%] Built target ncphost-PDUM
[  5%] Building C object CMakeFiles/zb_coord_linux.dir/home/zb-linux-coord/zigbee/examples/zigbee_coordinator/zigbee/examples/zigbee_coordinator/src/linux/pdum_gen_glue.c.o
[  6%] Building C object CMakeFiles/zb_coord_linux.dir/home/zb-linux-coord/zigbee/examples/zigbee_coordinator/zigbee/examples/zigbee_coordinator/src/app_coordinator_ncp.c.o
. . .
[ 99%] Building C object CMakeFiles/zb_coord_linux.dir/home/zb-linux-coord/zigbee/examples/zigbee_coordinator/zigbee/ZCL/Clusters/OTA/Source/OTA.c.o
[100%] Linking C executable zb_coord_linux
[100%] Built target zb_coord_linux

4. Running the application

4.1. Starting the coordinator

Make sure that the iMX8 board is connected to the Zigbee NCP coprocessor board as in the picture below. The two boards are connected through a USB cable (micro-USB for K32W148 EVK board and mini-USB for K32W061 DK6 board), between the MCU-Link connected on the K32W148/K32W061 board (marked as such on the silk screen), and the OTG connector on the iMX8 board.

The Linux Zigbee Coordinator allows the user to specify the serial port on which the NCP coprocessor board is connected. Usually on the iMX8 board, this is /dev/ttyACM0 for K32W148 and /dev/ttyUSB0 for K32W061. For the K32W061 based NCP coprocessor, the user should pay attention and modify the default latency timer (255msec) to a smaller value (it should be below 16msec).

Command to display default latency timer for ttyUSB interface: cat /sys/bus/usb-serial/devices/ttyUSB0/latency_timer

Command to modify default latency timer for ttyUSB interface: echo 1 | sudo tee /sys/bus/usb-serial/devices/ttyUSB0/latency_timer.

Example to start the Zigbee NCP Coordinator:

>root@ubuntu:~ ./zb_coord_linux /dev/ttyACM0 
[0] Created NCP Host Task with pid 653686
[0] MAIN
[0] ZQ: Initialised a queue: Handle=565ec8c4 Length=30 ItemSize=96
[0] ZQ: Initialised a queue: Handle=565ece50 Length=30 ItemSize=4
[0] ZQ: Initialised a queue: Handle=565ece68 Length=35 ItemSize=4
[0] ZQ: Initialised a queue: Handle=565ece38 Length=3 ItemSize=48
[0] ZQ: Initialised a queue: Handle=565f3700 Length=20 ItemSize=4
[0] ZQ: Initialised a queue: Handle=565f3728 Length=38 ItemSize=4
[0] serial Link initialised
[0] eOTA_NewImageLoaded status = 1
[2] New max process gap 1
[2] Pkt Type 0010 Set New Max Response Time 2
[212] New max process gap 210
[226] Pkt Type 0012 Set New Max Response Time 13
[1178] Recovered Application State 0 On Network 0
>

4.2. Forming the network

[3259] Form
[3259] APP-EVT: Event 8, NodeState=0
[3267] BDB: Forming Centralized Nwk
[3285] Pkt Type 0024 Set New Max Response Time 18
[3285] APP-EVT: Request Nwk Formation 00
[3805] Nwk formation took 538 MS
[3805] BDB: APP_vGenCallback [0 4]
ZPS_vSetTCLockDownOverride
[3805] APP-BDB: NwkFormation Success
[3805] APP-ZDO: Network started Channel = 12

4.3. Steer the network

[5879] Steer
[5879] APP-EVT: Event 6, NodeState=10
[5888] APP-BDB: NwkSteering Success
[5888] APP-EVT: Request Nwk Steering 00
[6765] BDB: APP_vGenCallback [0 9]
[6765] APP-ZDO: New Node 0be0 Has Joined
[7024] BDB: APP_vGenCallback [0 1]
[7024] APP-ZDO: Data Indication Status 00 from 0be0 Src Ep 0 Dst Ep 0 Profile 0000 Cluster 0013
[7101] BDB: APP_vGenCallback [0 14]
[7101] APP-ZDO: Discovery Confirm

The APP-ZDO Data Indication message signals that an Zigbee End Device has successfully joined the network and is ready to be controlled.

4.4. Find and Bind

Since the Zigbee End Device in this demo is behaving as a light bulb, we need to bind its On/Off cluster (server) to the Zigbee Coordinator On/Off cluster (client) in order to receive reports and be able to toggle it. This is done based on the BDB Find & Bind procedure, where the Zigbee Coordinator is the initiator and the Zigbee End Device is the target. For the first step we’ll use the `find` command, while the `bind` is going to be automatically done by the Zigbee Coordinator, since the On/Off cluster is the cluster of interest.

To kick off the F&B procedure, the user needs to enter the `find` command (case insensitive) into the Zigbee Coordinator console and the corresponding output:

>[187966] Find
>[187966] APP-EVT: Event 7, NodeState=10
>[187984] APP-EVT: Find and Bind initiate 00
>[188125] - for identify cluster
>[188125]
>CallBackBDB[188125] BDB ZCL Event 8
>[188216] Pkt Type 0052 Set New Max Response Time 23
>[188392] BDB: APP_vGenCallback [0 1]
>[188395] APP-BDB: F&B Simple Desc response From 0be0 Profle 0104 Device 0100 Ep 1 Version 1
>[188399] APP-BDB: Check For Binding Cluster 0006
>[188399] Pkt Type 8074 Took 111
>[188399] Pkt Type 8074 Set New Max Response Time 111
>[188414] APP-BDB: Bind Created for cluster 0006
>[188420] Remote Bind Dst addr 0be0, Ieee Dst Addr b1d48a734e2b758c Ieee Src 00158d00031f14c8
>[188433] Sending a remote bind request Status =0
>[188436] APP-BDB: Bind Created for target EndPt 1
>[188448] APP-ZDO: Data Indication Status 00 from 0be0 Src Ep 0 Dst Ep 0 Profile 0000 Cluster 8004
>[188612]
>

4.5. Toggle commands

The Zigbee End Device is sending periodic reports regarding the state of the light (on/off), as well as reports when there’s a change request state from the initiator. In order to change the state of the light, the user needs to enter the command `toggle` (case insensitive) in the Zigbee Coordinator console, as per the example below:

>[239792] Toggle
>[239792] APP-EVT: Event 5, NodeState=10
>[239792] APP-EVT: Send Toggle Cmd 
>[239792] ZCL Attribute Report: Cluster 0006 Attribute 0000 Value 1

4.6. ZigBee Over-The-Air (OTA) upgrade

Over-The-Air (OTA) Upgrade is the method by which a new firmware image is transferred to a device that is already installed and running as part of a ZigBee network. Support for the OTA Upgrade cluster as a Server has been included for the Coordinator device.

To add an image to the coordinator, the OTA images must be placed in the `out` directory and must obey the following convention: begin OTA image name with `OTA_Image` and use a `.bin` file format. For example: OTA_Image_k32w061dk6_zigbee_ed_rx_on_bmClient_UpgradeImagewithOTAHeaderV2_Enc.bin.

Example output for a successful OTA transfer:

[19539] Pkt Type 0002 Set New Max Response Time 23
[22830] Pkt Type 0002 Set New Max Response Time 29
[145090] Pkt Type 0002 Set New Max Response Time 33
[421207] Pkt Type 0002 Set New Max Response Time 49
[607037] Nwk status Ind addr 0be0 Status 11
[607037] BDB: APP_vGenCallback [0 13]
[607037] APP-ZDO: Network status Indication 11 addr 0be0
Upgrade End Req received from 0be0 status 0...
[1014587] BDB: APP_vGenCallback [0 9]
[1014587] APP-ZDO: New Node 0be0 Has Joined
[1014753] BDB: APP_vGenCallback [0 1]
[1014753] APP-ZDO: Data Indication Status 00 from 0be0 Src Ep 0 Dst Ep 0 Profile 0000 Cluster 0013
[1014841] BDB: APP_vGenCallback [0 14]
[1014841] APP-ZDO: Discovery Confirm