MCUXpresso SDK: coreMQTT Agent Library
This repository is a fork of coreMQTT Agent library (https://github.com/FreeRTOS/coremqtt-agent)(1.2.0). Modifications have been made to adapt to NXP MCUXpresso SDK. CMakeLists.txt and Kconfig added to enable coreMQTT Agent repo sources build in MCUXpresso SDK. It is part of the MCUXpresso SDK overall delivery which is composed of several sub-repositories/projects. Navigate to the top/parent repository mcuxsdk-manifests(https://github.com/nxp-mcuxpresso/mcuxsdk-manifests) for the complete delivery of MCUXpresso SDK.
coreMQTT Agent Library
The coreMQTT Agent library is a high level API that adds thread safety to the coreMQTT library. The library provides thread safe equivalents to the coreMQTT’s APIs, greatly simplifying its use in multi-threaded environments. The coreMQTT Agent library manages the MQTT connection by serializing the access to the coreMQTT library and reducing implementation overhead (e.g., removing the need for the application to repeatedly call to MQTT_ProcessLoop
). This allows your multi-threaded applications to share the same MQTT connection, and enables you to design an embedded application without having to worry about coreMQTT thread safety.
This library has gone through code quality checks including verification that no function has a GNU Complexity score over 8, and checks against deviations from mandatory rules in the MISRA coding standard. Deviations from the MISRA C:2012 guidelines are documented under MISRA Deviations. This library has also undergone both static code analysis from Coverity static analysis, and validation of memory safety through the CBMC automated reasoning tool.
See memory requirements for this library here.
Cloning this repository
This repo uses Git Submodules to bring in dependent components.
To clone using HTTPS:
git clone https://github.com/FreeRTOS/coreMQTT-Agent.git --recurse-submodules
Using SSH:
git clone git@github.com:FreeRTOS/coreMQTT-Agent.git --recurse-submodules
If you have downloaded the repo without using the --recurse-submodules
argument, you need to run:
git submodule update --init --recursive
coreMQTT Agent Library Configurations
The MQTT Agent library uses the same core_mqtt_config.h
configuration file as coreMQTT, with the addition of configuration constants listed at the top of core_mqtt_agent.h and core_mqtt_agent_command_functions.h. Documentation for these configurations can be found here.
To provide values for these configuration values, they must be either:
Defined in
core_mqtt_config.h
used by coreMQTT ORPassed as compile time preprocessor macros
Porting the coreMQTT Agent Library
In order to use the MQTT Agent library on a platform, you need to supply thread safe functions for the agent’s messaging interface.
Messaging Interface
Each of the following functions must be thread safe.
Function Pointer |
Description |
---|---|
|
A function that sends commands (as |
|
A function used by |
|
A function that returns a pointer to an allocated |
|
A function called to indicate that a command structure that had been allocated with the |
Reference implementations for the interface functions can be found in the reference examples below.
Additional Considerations
Static Memory
If only static allocation is used, then the MQTTAgentCommandGet_t
and MQTTAgentCommandRelease_t
could instead be implemented with a pool of MQTTAgentCommand_t
structures, with a queue or semaphore used to control access and provide thread safety. The below reference examples use static memory with a command pool.
Subscription Management
The MQTT Agent does not track subscriptions for MQTT topics. The receipt of any incoming PUBLISH packet will result in the invocation of a single MQTTAgentIncomingPublishCallback_t
callback, which is passed to MQTTAgent_Init()
for initialization. If it is desired for different handlers to be invoked for different incoming topics, then the publish callback will have to manage subscriptions and fan out messages. A platform independent subscription manager example is implemented in the reference examples below.
Building the Library
You can build the MQTT Agent source files that are in the source directory, and add source/include to your compiler’s include path. Additionally, the MQTT Agent library requires the coreMQTT library, whose files follow the same source/
and source/include
pattern as the agent library; its build instructions can be found here.
If using CMake, the mqttAgentFilePaths.cmake file contains the above information of the source files and the header include path from this repository. The same information is found for coreMQTT from mqttFilePaths.cmake
in the coreMQTT submodule.
For a CMake example of building the MQTT Agent library with the mqttAgentFilePaths.cmake
file, refer to the coverity_analysis
library target in test/CMakeLists.txt file.
Building Unit Tests
Checkout CMock Submodule
To build unit tests, the submodule dependency of CMock is required. Use the following command to clone the submodule:
git submodule update --checkout --init --recursive test/unit-test/CMock
Unit Test Platform Prerequisites
For running unit tests
C90 compiler like gcc
CMake 3.13.0 or later
Ruby 2.0.0 or later is additionally required for the CMock test framework (that we use).
For running the coverage target, gcov and lcov are additionally required.
Steps to build Unit Tests
Go to the root directory of this repository. (Make sure that the CMock submodule is cloned as described above)
Run the cmake command:
cmake -S test -B build
Run this command to build the library and unit tests:
make -C build all
The generated test executables will be present in
build/bin/tests
folder.Run
cd build && ctest
to execute all tests and view the test run summary.
CBMC
To learn more about CBMC and proofs specifically, review the training material here.
The test/cbmc/proofs
directory contains CBMC proofs.
In order to run these proofs you will need to install CBMC and other tools by following the instructions here.
Reference examples
Please refer to the demos of the MQTT Agent library in the following locations for reference examples on FreeRTOS platforms:
Location |
---|
Documentation
The MQTT Agent API documentation can be found here.
Generating documentation
The Doxygen references were created using Doxygen version 1.9.2. To generate the Doxygen pages yourself, please run the following command from the root of this repository:
doxygen docs/doxygen/config.doxyfile
Getting help
You can use your Github login to get support from both the FreeRTOS community and directly from the primary FreeRTOS developers on our active support forum. You can find a list of frequently asked questions here.
Contributing
See CONTRIBUTING.md for information on contributing.
License
This library is licensed under the MIT License. See the LICENSE file.