MCUXpresso SDK Release Notes
Overview
The MCUXpresso SDK is a comprehensive software enablement package designed to simplify and accelerate application development with Arm Cortex-M-based devices from NXP, including its general purpose, crossover and Bluetooth-enabled MCUs. MCUXpresso SW and Tools for DSC further extends the SDK support to current 32-bit Digital Signal Controllers. The MCUXpresso SDK includes production-grade software with integrated RTOS (optional), integrated enabling software technologies (stacks and middleware), reference software, and more.
In addition to working seamlessly with the MCUXpresso IDE, the MCUXpresso SDK also supports and provides example projects for various toolchains. The Development tools chapter in the associated Release Notes provides details about toolchain support for your board. Support for the MCUXpresso Config Tools allows easy cloning of existing SDK examples and demos, allowing users to leverage the existing software examples provided by the SDK for their own projects.
Underscoring our commitment to high quality, the MCUXpresso SDK is MISRA compliant and checked with Coverity static analysis tools. For details on MCUXpresso SDK, see MCUXpresso-SDK: Software Development Kit for MCUXpresso.
MCUXpresso SDK
As part of the MCUXpresso software and tools, MCUXpresso SDK is the evolution of Kinetis SDK, includes support for LPC, DSC,PN76, and i.MX System-on-Chip (SoC). The same drivers, APIs, and middleware are still available with support for Kinetis, LPC, DSC, and i.MX silicon. The MCUXpresso SDK adds support for the MCUXpresso IDE, an Eclipse-based toolchain that works with all MCUXpresso SDKs. Easily import your SDK into the new toolchain to access to all of the available components, examples, and demos for your target silicon. In addition to the MCUXpresso IDE, support for the MCUXpresso Config Tools allows easy cloning of existing SDK examples and demos, allowing users to leverage the existing software examples provided by the SDK for their own projects.
In order to maintain compatibility with legacy Freescale code, the filenames and source code in MCUXpresso SDK containing the legacy Freescale prefix FSL has been left as is. The FSL prefix has been redefined as the NXP Foundation Software Library.
Development tools
The MCUXpresso SDK was tested with following development tools. Same versions or above are recommended.
IAR Embedded Workbench for Arm, version is 9.60.4
MCUXpresso for VS Code v25.06
GCC Arm Embedded Toolchain 14.2.x
Supported development systems
This release supports board and devices listed in following table. The board and devices in bold were tested in this release.
Development boards |
MCU devices |
---|---|
EVK-MCIMX7ULP |
MCIMX7U5CVP06, MCIMX7U5DVK07, MCIMX7U5DVP07, |
MCUXpresso SDK release package
The MCUXpresso SDK release package content is aligned with the silicon subfamily it supports. This includes the boards, CMSIS, devices, middleware, and RTOS support.
Device support
The device folder contains the whole software enablement available for the specific System-on-Chip (SoC) subfamily. This folder includes clock-specific implementation, device register header files, device register feature header files, and the system configuration source files. Included with the standard SoC support are folders containing peripheral drivers, toolchain support, and a standard debug console. The device-specific header files provide a direct access to the microcontroller peripheral registers. The device header file provides an overall SoC memory mapped register definition. The folder also includes the feature header file for each peripheral on the microcontroller. The toolchain folder contains the startup code and linker files for each supported toolchain. The startup code efficiently transfers the code execution to the main() function.
Board support
The boards folder provides the board-specific demo applications, driver examples, and middleware examples.
Demo application and other examples
The demo applications demonstrate the usage of the peripheral drivers to achieve a system level solution. Each demo application contains a readme file that describes the operation of the demo and required setup steps. The driver examples demonstrate the capabilities of the peripheral drivers. Each example implements a common use case to help demonstrate the driver functionality.
RTOS
FreeRTOS
Real-time operating system for microcontrollers from Amazon
Middleware
CMSIS DSP Library
The MCUXpresso SDK is shipped with the standard CMSIS development pack, including the prebuilt libraries.
IoT Sensing Software Development Kit (ISSDK)
The IoT Sensing Software Development Kit (ISSDK) is the embedded software framework enabling the NXP digital and analog sensors for IoT applications. ISSDK combines a set of robust sensor drivers and algorithms along with example applications that allow users to get started with using NXP IoT motion & pressure sensors. ISSDK is being offered as a middleware component in MCUXpresso SDK.
USB Host, Device, OTG Stack
See the MCUXpresso SDK USB Stack User’s Guide (document MCUXSDKUSBSUG) for more information.
TinyCBOR
Concise Binary Object Representation (CBOR) Library
PKCS#11
The PKCS#11 standard specifies an application programming interface (API), called “Cryptoki,” for devices that hold cryptographic information and perform cryptographic functions. Cryptoki follows a simple object based approach, addressing the goals of technology independence (any kind of device) and resource sharing (multiple applications accessing multiple devices), presenting to applications a common, logical view of the device called a “cryptographic token”.
Multicore
Multicore Software Development Kit
MMCAU
The NXP Memory-Mapped Cryptographic Acceleration Unit
mbedTLS
mbedtls SSL/TLS library v2.x
llhttp
HTTP parser llhttp
FreeMASTER
FreeMASTER communication driver for 32-bit platforms.
Release contents
Provides an overview of the MCUXpresso SDK release package contents and locations.
Deliverable |
Location |
---|---|
Boards |
INSTALL_DIR/boards |
Demo Applications |
INSTALL_DIR/boards/<board_name>/demo_apps |
Driver Examples |
INSTALL_DIR/boards/<board_name>/driver_examples |
eIQ examples |
INSTALL_DIR/boards/<board_name>/eiq_examples |
Board Project Template for MCUXpresso IDE NPW |
INSTALL_DIR/boards/<board_name>/project_template |
Driver, SoC header files, extension header files and feature header files, utilities |
INSTALL_DIR/devices/<device_name> |
CMSIS drivers |
INSTALL_DIR/devices/<device_name>/cmsis_drivers |
Peripheral drivers |
INSTALL_DIR/devices/<device_name>/drivers |
Toolchain linker files and startup code |
INSTALL_DIR/devices/<device_name>/<toolchain_name> |
Utilities such as debug console |
INSTALL_DIR/devices/<device_name>/utilities |
Device Project Template for MCUXpresso IDE NPW |
INSTALL_DIR/devices/<device_name>/project_template |
CMSIS Arm Cortex-M header files, DSP library source |
INSTALL_DIR/CMSIS |
Components and board device drivers |
INSTALL_DIR/components |
RTOS |
INSTALL_DIR/rtos |
Release Notes, Getting Started Document and other documents |
INSTALL_DIR/docs |
Tools such as shared cmake files |
INSTALL_DIR/tools |
Middleware |
INSTALL_DIR/middleware |
Known issues
This section lists the known issues, limitations, and/or workarounds.
Cannot add SDK components into FreeRTOS projects
It is not possible to add any SDK components into FreeRTOS project using the MCUXpresso IDE New Project wizard.
LPSPI b2b examples transfer fail on iar/armgcc flash target
Due to the latency of instruction retrieval (XiP), LPSPI-related flash target examples may fail. The failure happens because the data is not retrieved in time from FIFO on the receiving end.
To prevent the failure and boost the instruction fetch performance, place the fsl_lpspi.c file in the SRAM.
Apply the patch as below,
$ git diff MCIMX7U5xxxxx_cm4_flash.ld
diff --git a/MCIMX7U5/gcc/MCIMX7U5xxxxx_cm4_flash.ld b/MCIMX7U5/gcc/MCIMX7U5xxxxx_cm4_flash.ld
index b29b41a2b1..91dc0782e5 100644
--- a/MCIMX7U5/gcc/MCIMX7U5xxxxx_cm4_flash.ld
+++ b/MCIMX7U5/gcc/MCIMX7U5xxxxx_cm4_flash.ld
@@ -68,10 +68,22 @@ SECTIONS
.text :
{
. = ALIGN(4);
- *(.text) /* .text sections (code) */
- *(.text*) /* .text* sections (code) */
- *(.rodata) /* .rodata sections (constants, strings, etc.) */
- *(.rodata*) /* .rodata* sections (constants, strings, etc.) */
+ *(EXCLUDE_FILE(
+ /* Exclude flash and frequently executed functions from XIP */
+ */fsl_lpspi.c.obj
+ ) .text) /* .text sections (code) */
+ *(EXCLUDE_FILE(
+ /* Exclude flash and frequently executed functions from XIP */
+ */fsl_lpspi.c.obj
+ ) .text*) /* .text* sections (code) */
+ *(EXCLUDE_FILE(
+ /* Exclude flash and frequently executed functions from XIP */
+ */fsl_lpspi.c.obj
+ ) .rodata) /* .rodata sections (constants, strings, etc.) */
+ *(EXCLUDE_FILE(
+ /* Exclude flash and frequently executed functions from XIP */
+ */fsl_lpspi.c.obj
+ ) .rodata*) /* .rodata* sections (constants, strings, etc.) */
*(.glue_7) /* glue arm to thumb code */
*(.glue_7t) /* glue thumb to arm code */
*(.eh_frame)
@@ -173,6 +185,7 @@ SECTIONS
__quickaccess_start__ = .;
. = ALIGN(32);
*(CodeQuickAccess)
+ /* Explicit placement of flash and frequently executed functions in SRAM */
+ */fsl_lpspi.c.obj(.text .text* .rodata .rodata*)
*(DataQuickAccess)
. = ALIGN(128);
__quickaccess_end__ = .;
LPSPI b2b examples transfer fail on iar/armgcc flash target.
Due to the latency of instruction retrieval (XiP), LPSPI-related flash target examples may fail. The failure happens because the data is not retrieved in time from FIFO on the receiving end.
.. code-block:: none
$ git diff MCIMX7U5xxxxx_cm4_flash.ld diff –git a/MCIMX7U5/gcc/MCIMX7U5xxxxx_cm4_flash.ld b/MCIMX7U5/gcc/MCIMX7U5xxxxx_cm4_flash.ld index b29b41a2b1..91dc0782e5 100644 — a/MCIMX7U5/gcc/MCIMX7U5xxxxx_cm4_flash.ld +++ b/MCIMX7U5/gcc/MCIMX7U5xxxxx_cm4_flash.ld @@ -68,10 +68,22 @@ SECTIONS .text : { . = ALIGN(4); - (.text) / .text sections (code) / - (.text) / .text* sections (code) / - (.rodata) / .rodata sections (constants, strings, etc.) / - (.rodata) / .rodata sections (constants, strings, etc.) */ + (EXCLUDE_FILE( + / Exclude flash and frequently executed functions from XIP */ + /fsl_lpspi.c.obj + ) .text) / .text sections (code) / + (EXCLUDE_FILE( + / Exclude flash and frequently executed functions from XIP / + /fsl_lpspi.c.obj + ) .text) / .text sections (code) */ + (EXCLUDE_FILE( + / Exclude flash and frequently executed functions from XIP */ + /fsl_lpspi.c.obj + ) .rodata) / .rodata sections (constants, strings, etc.) / + (EXCLUDE_FILE( + / Exclude flash and frequently executed functions from XIP / + /fsl_lpspi.c.obj + ) .rodata) / .rodata sections (constants, strings, etc.) */ (.glue_7) / glue arm to thumb code */ (.glue_7t) / glue thumb to arm code */ *(.eh_frame) @@ -173,6 +185,7 @@ SECTIONS quickaccess_start = .; . = ALIGN(32); (CodeQuickAccess) + / Explicit placement of flash and frequently executed functions in SRAM / + /fsl_lpspi.c.obj(.text .text .rodata .rodata) *(DataQuickAccess) . = ALIGN(128); quickaccess_end = .;
Workaround: To prevent the failure and boost the instruction fetch performance, place the fsl_lpspi.c file in the SRAM. Apply the patch as below,
The freertos_lpuart example does not complete successfully
The example hangs after console output ‘FreeRTOS LPUART driver example’.
Examples: freertos_lpuart
Affected toolchains: All
The example does not perform as expected (Ticks do not printed on the console or the application does not wake up from the sleep mode).
Examples: freertos_tickless
Affected toolchains: All