Hardware requirements
Mini/micro USB cable
Loopback network cable RJ45 standard
EVKB-IMXRT1050 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Insert loopback network cable to Ethernet RJ45 port.
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Make loopback network cable: 568B standard Unknowed standard J1 orange+white green+white J2 orange green J3 green+white orange+white J4 blue brown+white J5 blue+white brown J6 green orange J7 brown+white blue J8 brown blue+white
Connect J1 => J3, J2 => J6, J4 => J7, J5 => J8. 10/100M transfer only requires J1, J2, J3, J6, and 1G transfer requires all 8 pins. Check your net cable color order and refer to 568B standard or the other standard. If your cable’s color order is not showed in the list, please connect J1~J8 based on your situation.
Running the demo
When the demo runs, the log would be seen on the terminal like:
ENET PTP 1588 example start.
Get the 1-th time xx second xx nanosecond …….. Get the 10-th time xx second xx nanosecond
The 1 frame transmitted success! the timestamp is xx second, xx nanosecond The 2 frame transmitted success! the timestamp is xx second, xx nanosecond The 3 frame transmitted success! the timestamp is xx second, xx nanosecond The 4 frame transmitted success! the timestamp is xx second, xx nanosecond …… The 20 frame transmitted success! the timestamp is xx second, xx nanosecond
Note: the xx second and xx nanosecond should not be zero and should be number with solid increment.
when a 1000 length ptp event message frame is received, the log would be added to the terminal like: A frame received. the length 1000 the timestamp is xx second, xx nanosecond Dest Address xx:xx:xx:xx:xx:xx Src Address xx:xx:xx:xx:xx:xx