Hardware requirements
Mini/micro USB cable
EVKB-IMXRT1050 board
Headphone(OMTP standard)
Personal Computer
Board settings
J12, headphone connected
remove R98,R99,R100,R101 and connect FLEXIO pins to the pad close to U13 as follows:
Pin Name Board Location Pin Name Board Location
RX_DATA SW5-1 RX_DATA U13-16
TX_DATA SW5-2 TX_DATA U13-14
SYNC SW5-3 SYNC U13-13
BCLK SW5-4 BCLK U13-12
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
Note: This demo uses both headphone mic and board main mic(P1) as input source. The headphone mic provides left channel data, and main mic (P1) provides right channel data. If users found there is noise while do record operation, most probably it is the headphone standard issue (OMTP and CTIA standard difference). You should use the OMTP standard headphone. You can disable the left channel by using an headphone without microphone feature.
When the demo runs successfully, the log would be seen on the OpenSDA terminal like as below.
~~~~~~~~~~~~~~~~~~~~~
FLEXIO_I2S interrupt example started!
FLEXIO_I2S interrupt example finished!
~~~~~~~~~~~~~~~~~~~~~