Hardware requirements
Mini/micro USB cable
MIMXRT1060-EVKB board
Personal Computer
Board settings
ADC0_IN15 and ADC0_IN0 are ADC inputs. Please sample voltage by J33-1 and J33-2 pins.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the hello world demo in the terminal window:
ADC_ETC_Hardware_Trigger_Conv Example Start!
ADC_DoAutoCalibration() Done.
ADC Full Range: XXXX
Please press any key to get user channel's ADC value.
ADC conversion value is 107 and 3882
ADC conversion value is 103 and 3884
ADC conversion value is 104 and 3880
ADC conversion value is 88 and 3890
ADC conversion value is 88 and 3890
ADC conversion value is 88 and 3890
ADC conversion value is 104 and 3882
ADC conversion value is 104 and 3882
...