Hardware requirements

  • Mini/micro USB cable

  • MIMXRT1170-EVKB board

  • Personal Computer

  • RK055MHD091 panel or RK055AHD091 panel or RK055IQH091 panel

Board settings

Connect the panel to J48 Connect 5V power to J43, set J38 to 1-2

Prepare the Demo

  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Build the project, the project uses RK055MHD091 by default, to use other panels, set the coresponding panel DEMO_PANEL_xxx(without ‘_SUPPORT’) to y in prj.conf under board example folder before project generation. The supported panels can be found in examples_boards<board>\project_segments\display_support\Kconfig.prjseg. Or change the macro DEMO_PANEL in mcux_config.h of the project, which number represents which panel can be found in display_support.h

  4. Download the program to the target board.

  5. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, press any key in the terminal, the panel shows different porter duff mode result.