Hardware requirements
Mini/micro USB cable
MIMXRT1170-EVKB board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the OpenSDA terminal like:
XECC Multiple Errors Example Start!
First level BusFault interrupt finished.
Uncorrecdted read data: 0xddccbba9
Multiple error address: 0x80000000
Multiple error read data: 0xddccbba9
Multiple error ECC code: 0x22cc44aa
Multiple error bit field: 0x1
XECC multiple errors example successfully!
Note: this example need to burn XECC_ENABLE(840[3]) in fuse to enable XECC module, which is disabled by default.