Hardware requirements

  • Mini/micro USB cable

  • Network cable RJ45 standard

  • MIMXRT1170-EVKB board

  • Personal Computer

Board settings

This example uses 1G port(J4) as default. If want to test 100M port(J3), please set the macro BOARD_NETWORK_USE_100M_ENET_PORT to 1.

Running the demo

Platform specific behavior: When an application programmatically performs software-induced reset while in a debugging session, the execution stalls in the ROM code. This is a feature. Your attention is needed at that moment: please perform reset manually by pressing the on-board hw reset button once you spot “SystemReset” message in the serial console. Manual reset is not needed while MCU is running freely without a debugger.