Hardware requirements

  • Mini/micro USB cable

  • MIMXRT1060-EVKC board

  • Personal Computer

Board settings

Remove the resistor R305 and weld 0Ω resistor to R346,R350,R356,R362.

To make the example work, connections needed to be as follows:

       MASTER           connect to      SLAVE
Pin Name   Board Location     Pin Name    Board Location
SOUT       J17-4                SIN       SW2-3
SIN        J17-5                SOUT      SW2-2
SCK        J17-6                SCK       SW2-1
PCS0       J17-3                PCS0      SW2-4

Prepare the Demo

  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

You can see the similar message shows following in the terminal if the example runs successfully.

LPSPI Master interrupt - FLEXIO SPI Slave interrupt example start.

This example use one lpspi instance as master and one flexio spi slave on one board.

Master and slave are both use interrupt way.

Please make sure you make the correct line connection. Basically, the connection is:

LPSPI_master -- FLEXIO_SPI_slave

   CLK      --    CLK

   PCS      --    PCS

   SOUT     --    SIN

   SIN      --    SOUT

This is FLEXIO SPI slave call back.

LPSPI master <-> FLEXIO SPI slave transfer all data matched!

End of Example.