Hardware requirements
Micro USB cable
MIMX8MN6-EVK board
J-Link Debug Probe
12V power supply
Personal Computer
Board settings
I2C one board:
Transfer data from SLAVE_BOARD to MASTER_BOARD of I2C interface, I2C3 pins of SLAVE_BOARD are connected with I2C3 pins of MASTER_BOARD
SLAVE_BOARD CONNECTS TO MASTER_BOARD
Pin Name Board Location Pin Name Board Location
I2C3_SCL J1003-5 I2C3_SCL J1003-5
I2C3_SDA J1003-3 I2C3_SDA J1003-3
GND J1003-9 GND J1003-9
Prepare the Demo
Connect 12V power supply and J-Link Debug Probe to the board, switch SW101 to power on the board
Connect a USB cable between the host PC and the J901 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the following message is displayed in the terminal:
CMSIS I2C board2board interrupt example – Slave transfer.
Slave received data : 0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7 0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f 0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17 0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of I2C example .