Hardware requirements
Micro USB cable
two MIMX8ULP-EVK/EVK9 board
JLink Plus
5V power supply
Personal Computer
Board settings
Prepare the Demo
Connect 5V power supply and JLink Plus to the board, switch SW10 to power on the board
Connect a micro USB cable between the host PC and the J17 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
After power on board, stop the uboot and ensure the board will not autoboot to linux.
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the hello world demo in the terminal window:
FLEXSPI example started!
IP Command Read/Write data succeed at all address range !
AHB Command Read/Write data succeed at all address range !