Hardware requirements

  • Micro USB cable

  • MIMX8ULP-EVK/EVK9 board

  • J-Link Debug Probe

  • 5V power supply

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo

  1. Connect 5V power supply and J-Link Debug Probe to the board, switch SW10 to power on the board.

  2. Connect a micro USB cable between the host PC and the J17 USB port on the cpu board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Launch the debugger in your IDE to begin running the example.

Running the demo

NOTE: Depending on the toolchain configuration, the benchmark result might be different.

CMSIS DSP benchmark software matrix test start.
arm_mat_add_q15Test: xxx
arm_mat_add_q31Test: xxx
arm_mat_add_f32Test: xxx
arm_mat_sub_q15Test: xxx
arm_mat_sub_q31Test: xxx
arm_mat_sub_f32Test: xxx
arm_mat_mult_q15Test: xxx
arm_mat_mult_q31Test: xxx
arm_mat_mult_f32Test: xxx
arm_mat_inverse_f32Test: xxx
arm_mat_trans_q15Test: xxx
arm_mat_trans_q31Test: xxx
arm_mat_trans_f32Test: xxx
arm_mat_scale_q15Test: xxx
arm_mat_scale_q31Test: xxx
arm_mat_scale_f32Test: xxx

CMSIS DSP benchmark software matrix test succeeded.