Hardware requirements
Micro USB cable
MIMX8ULP-EVK/EVK9 board
J-Link Debug Probe
5V power supply
Personal Computer
Board settings
The Multicore RPMsg-Lite string echo project does not call for any special hardware configurations. Although not required, the recommendation is to leave the development board jumper settings and configurations in default state when running this demo.
Prepare the Demo
Generate i.MX8ULP image file with imx-mkimage and write to emmc/flexspi0 nor flash with U-Boot/UUU/JLink. For details, please refer to Getting Started with SDK v.2.0 for i.MX 8ULP Derivatives (Doc No: SDK20IMX8ULPGSUG)
Connect a micro USB cable between the host PC and the J17 USB port on the target board.
Open two serial terminals for A Core and M Core with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control (e.g. /dev/ttyUSB0~3, /dev/ttyUSB2 for A Core, /dev/ttyUSB3 for M Core)
Flash the image to emmc/flexspi0 nor flash using u-boot/UUU/JLink.(Don’t use IAR/GDB to download m33 binary to SSRAM to test it)
Repower on board to boot system
Login to linux
After login, make sure imx_rpmsg_tty kernel module is inserted (lsmod) or insert it (modprobe imx_rpmsg_tty).
Running the demo
After the boot process succeeds, the ARM Cortex-M33 terminal displays the following information:
RPMSG String Echo FreeRTOS RTOS API Demo...
Nameservice sent, ready for incoming messages...
After the Linux RPMsg tty module was installed, the ARM Cortex-M33 terminal displays the following information:
Get Messgae From Master Side : "hello world!" [len : 12]
The user can then input an arbitrary string to the virtual RPMsg tty using the following echo command on Cortex-A terminal:
echo test > /dev/ttyRPMSG<num>
<num> here is the allocated ttyRPMsg channel number. Please find out the number in the file system by "ls" command.
Log below shows the output of the RPMsg-Lite str echo demo in the terminal window:
On the M33 terminal, the received string content and its length is output, as shown in the log.
Get Message From Master Side : "test" [len : 4]
Get New Line From Master Side