Hardware requirements
Mini/micro USB cable
EVK-MIMXRT1010 board
Personal Computer
Board settings
Remove the resistor R90 and weld 0Ω resistor to R800. To make the example work, connections needed to be as follows:
MASTER connect to SLAVE
Pin Name Board Location Pin Name Board Location
SOUT J57-8 SIN J26-6
SIN J57-10 SOUT J26-4
SCK J57-12 SCK J26-8
PCS0 J57-6 PCS0 J56-10
Prepare the Demo
Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
You can see the similar message shows following in the terminal if the example runs successfully.
LPSPI Master interrupt - FLEXIO SPI Slave edma dynamic transfer example start.
This example use one lpspi instance as master and one flexio spi slave on one board.
Master uses interrupt and slave uses edma way.
Master transfers indefinite amount of data to slave, and the CS signal remains low during transfer.
After master finishes the transfer and re-asserts the CS signal, interrupt is triggered to let user know.
Slave must configure the transfer size larger than master's.
Please make sure you make the correct line connection. Basically, the connection is:
LPSPI_master -- FLEXIO_SPI_slave
CLK -- CLK
PCS -- PCS
SOUT -- SIN
SIN -- SOUT
Slave received 128 bytes of data
Slave received 128 bytes of data
LPSPI master <-> FLEXIO SPI slave transfer all data matched!
End of Example.
Note: To debug in qspiflash, following steps are needed:
Select the flash target and compile.
Set the SW8: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J41.
Start debugging in IDE.
Keil: Click “Download (F8)” to program the image to qspiflash first then clicking “Start/Stop Debug Session (Ctrl+F5)” to start debugging.