Hardware requirements
Mini/micro USB cable
EVK-MIMXRT1015 board
Personal Computer
USB to Com Converter
Board settings
Connect pin:
RX of USB2COM to J17-2
TX of USB2COM to J17-1
GND of USB2COM to J19-7
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
7 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal(from USB To Serial Adapter):
Lpuart polling example with seven data bits
Board will send back received characters
Note: To debug in qspiflash, following steps are needed:
Select the flash target and compile.
Set the SW8: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J41.
Start debugging in IDE.
Keil: Click “Download (F8)” to program the image to qspiflash first then clicking “Start/Stop Debug Session (Ctrl+F5)” to start debugging.