Hardware requirements
Mini/micro USB cable
Network cable RJ45 standard
EVK-MIMXRT1020 board
Personal Computer
Board settings
No special settings are required.
Note: To debug in qspiflash, following steps are needed:
Select the flash target and compile.
Set the SW8: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J23.
Start debugging in IDE.
Keil: Click “Download (F8)” to program the image to qspiflash first then clicking “Start/Stop Debug Session (Ctrl+F5)” to start debugging.