Hardware requirements

  • Mini/micro USB cable

  • MIMXRT1024-EVK board

  • Personal Computer

Board settings

ADC1_IN10 and ADC1_IN11 are ADC inputs. Please sample voltage by J18-2 and J18-4 pins.

Prepare the Demo

  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output of the hello world demo in the terminal window:

ADC_ETC_Hardware_Trigger_Conv Example Start!
ADC_DoAutoCalibration() Done.
ADC Full Range: XXXX
Please press any key to get user channel's ADC value.
ADC conversion value is 107 and 3882
ADC conversion value is 103 and 3884
ADC conversion value is 104 and 3880
ADC conversion value is 88 and 3890
ADC conversion value is 88 and 3890
ADC conversion value is 88 and 3890
ADC conversion value is 104 and 3882
ADC conversion value is 104 and 3882
...

Note: To debug in qspiflash, following steps are needed:

  1. Select the flash target and compile.

  2. Set the SW8: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J23.

  3. Start debugging in IDE.

    • Keil: Click “Download (F8)” to program the image to qspiflash first then clicking “Start/Stop Debug Session (Ctrl+F5)” to start debugging.