Hardware requirements
Mini/micro USB cable
MIMXRT1040-EVK board
Personal Computer
Board settings
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the hello world demo in the terminal window:
***NOR Flash Component Demo Start!***
***NOR Flash Page 0 Read/Write Success!***
***NOR Flash Page 1 Read/Write Success!***
***NOR Flash Page 2 Read/Write Success!***
***NOR Flash Page 3 Read/Write Success!***
.....
***NOR Flash Page 12 Read/Write Success!***
***NOR Flash Page 13 Read/Write Success!***
***NOR Flash Page 14 Read/Write Success!***
***NOR Flash Page 15 Read/Write Success!***
***NOR Flash All Pages Read/Write Success!***
Known issue
The MCUX release target and armgcc flexspi_nor_release run fail.