Hardware requirements
Two Micro USB cable
MIMXRT1040-EVK board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board for downloading the program and supply power for the board, connect another USB cable between host PC and USB port on the target board.
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Open a serial terminal(like putty) to communicate with the board via virtual com.
Running the demo
The log below shows the output of this demo in the terminal window:
hello world.
Terminal will echo back the received characters.