Hardware requirements
Mini/micro USB cable
EVK-MIMXRT1064 board
Personal Computer
Board settings
Remove the resistor R334 and weld 0Ω resistor to R278,R279,R280,R281.
To make the example work, connections needed to be as follows:
MASTER connect to SLAVE
Pin Name Board Location Pin Name Board Location
SOUT J24-4 SIN SW5-3
SIN J24-5 SOUT SW5-2
SCK J24-6 SCK SW5-1
PCS0 J24-3 PCS0 SW5-4
Prepare the Demo
Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
You can see the similar message shows following in the terminal if the example runs successfully.
LPSPI Master interrupt - FLEXIO SPI Slave edma dynamic transfer example start.
This example use one lpspi instance as master and one flexio spi slave on one board.
Master uses interrupt and slave uses edma way.
Master transfers indefinite amount of data to slave, and the CS signal remains low during transfer.
After master finishes the transfer and re-asserts the CS signal, interrupt is triggered to let user know.
Slave must configure the transfer size larger than master's.
Please make sure you make the correct line connection. Basically, the connection is:
LPSPI_master -- FLEXIO_SPI_slave
CLK -- CLK
PCS -- PCS
SOUT -- SIN
SIN -- SOUT
Slave received 128 bytes of data
Slave received 128 bytes of data
LPSPI master <-> FLEXIO SPI slave transfer all data matched!
End of Example.