Hardware requirements
Mini/micro USB cable
EVK-MIMXRT1064 board
Personal Computer
Board settings
This example project does not call for any special hardware configurations. Although not required, the recommendation is to leave the development board’s jumper settings and configurations in default state when running this example.
Prepare the Demo
Connect a USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
When the demo runs successfully, the log would be seen on the terminal like:
FLEXRAM ram allocate example.
Allocate on-chip ram:
OCRAM bank numbers 4
DTCM bank numbers 4
ITCM bank numbers 8
Allocate on-chip ram success
OCRAM access to 0x20220000 boundary.
DTCM access to nearly 0x20020000 boundary.
ITCM access to nearly 0x40000 boundary.
FLEXRAM ram allocate example finish.