Hardware requirements
Mini/micro USB cable
EVK-MIMXRT1064 board
Personal Computer
Board settings
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, you can see the similar information from the terminal as below.
FLEXSPI edma example started! Vendor ID: 0xef Erasing Serial NOR over FlexSPI… Erase data - successfully. Program data - successfully.
Note:
1, this example do erase/program/read operations in internal quad flash(W25Q32JV) and its image also loads to internal flash(W25Q32JV) for flash target.
2, internal flash pin connection like below:
DQS <---> GPIO_SPI_B1_00
CS <---> GPIO_SPI_B1_06
CLK <---> GPIO_SPI_B0_08
IO0 <---> GPIO_SPI_B0_02
IO1 <---> GPIO_SPI_B1_03
IO2 <---> GPIO_SPI_B1_02
IO3 <---> GPIO_SPI_B0_10
RESET <---> GPIO_SPI_B0_13
GND2 <---> VSS
VCC <---> NVCC_GPIO
GND <---> VSS