Hardware requirements
Mini/micro USB cable
MIMXRT1160-EVK board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Note: To download binary of cm7 core into qspiflash and boot from qspiflash directly, following steps are needed:
Compile flash target of the project, and get the binaray file “hello_world.bin”.
Set the SW1: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J11.
Drop the binaray into disk “RT1160-EVK” on PC.
Wait for the disk disappear and appear again which will take couple of seconds.
Reset the board by pressing SW3 or power off and on the board. (If default boot core is cm4, binary of cm4 could be downloaded and boot according to steps above.)