Hardware requirements
Mini/micro USB cable
MIMXRT1160-EVK board
Personal Computer
Board settings
Remove 0Ω resistor to R200,R406,R408,R404.
To make the example work, connections needed to be as follows:
SLAVE connect to MASTER
Pin Name Board Location Pin Name Board Location
SOUT J10-10 SIN J26-6
SIN J10-8 SOUT J26-4
SCK J10-12 SCK J26-2
PCS0 J10-6 PCS0 J26-8
Prepare the Demo
Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
You can see the similar message shows following in the terminal if the example runs successfully.
FLEXIO Master - LPSPI Slave polling example start.
This example use one flexio spi as master and one lpspi instance as slave on one board.
Master uses polling and slave uses interrupt way.
Please make sure you make the correct line connection. Basically, the connection is:
FLEXIO_SPI_master -- LPSPI_slave
CLK -- CLK
PCS -- PCS
SOUT -- SIN
SIN -- SOUT
This is LPSPI slave call back.
FLEXIO SPI master <-> LPSPI slave transfer all data matched!
End of example.