Hardware requirements

  • Mini/micro USB cable

  • MIMXRT1160-EVK board

  • Personal Computer

  • Oscilloscope

Board settings

  • Remove R414.

  • Connect input signal to J9-8.

  • Use oscilloscope to measure output the signal pin at J9-12.

Prepare the Demo

  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the example.

Running the demo

When the demo runs successfully, the following message is displayed in the terminal:


****Input capture example.****

****Provide a signal input to the QTMR pin****

Input Captured value=1f

****Output PWM example.****

*********Make sure to connect an oscilloscope.*********

****A 50 duty cycle PWM wave is observed on an oscilloscope.****

~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~