Hardware requirements
Mini/micro USB cable
EVK-MIMXRT1160 board
Personal Computer
SD card
Board settings
Please make sure R136 is weld for GPIO card detect.
Prepare the Demo
Connect a micro USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Insert SD card to card slot
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the terminal like:
SDCARD fatfs freertos example.
Card inserted.
Make file system......The time may be long if the card capacity is big.
Create directory......
TASK1: write file successed.
TASK1: file access is blocking.
TASK1: file access is blocking.
TASK2: write file successed.
TASK2: file access is blocking.
TASK2: file access is blocking.
TASK1: finsied.
TASK2: finsied.