Hardware requirements
Mini/micro USB cable
MIMXRT1180-EVK board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
Copyright  2022  NXP
LOG SHELL>> installbackend debugconsole
LOG SHELL>> log error
       22350: ERROR log_main.c:104:This is "error" log message
LOG SHELL>> log fatal
       27900: FATAL log_main.c:100:This is "fatal" log message
LOG SHELL>> log warning
       35430: WARN  log_main.c:108:This is "warning" log message
LOG SHELL>> log info
       38585: INFO  log_main.c:112:This is "info" log message
LOG SHELL>> log debug
       41330: DEBUG log_main.c:116:This is "debug" log message
LOG SHELL>> log trace
       45090: TRACE log_main.c:120:This is "trace" log message
LOG SHELL>> log test
       49835: ERROR log_main.c:124:The input arguement "test" is not valid
LOG SHELL>> uninstallbackend debugconsole
LOG SHELL>>