Hardware requirements
Mini/micro USB cable
MIMXRT1180-EVK board
Personal Computer
Board settings
The mcuboot binary must be processed by SPSDK tools to allow ROM code to boot it from flash. If this is not done automatically during build/postbuild it needs to be done manually. When using NXP tools such as MCUXpresso IDE or MCUXpresso Secure Provisioning Tool this should be done automatically by the tool.
MCUBoot layout
Region |
From |
To |
Size |
|---|---|---|---|
MCUboot code |
0x28000000 |
0x2803FFFF |
256kB |
Primary slot |
0x28040000 |
0x2823FFFF |
2048kB |
Secondary slot |
0x28240000 |
0x2843FFFF |
2048kB |
MCUBoot header size is set to 1024 bytes
Signing algorithm is RSA-2048
Write alignment is 4 bytes
MCUBoot is configured to use
SWAP_MOVEimage handling strategy
Image signing example
imgtool sign --key sign-rsa2048-priv.pem
--align 4
--version 1.1
--slot-size 0x200000
--header-size 0x400
--pad-header
ota_mcuboot_basic.bin
ota_mcuboot_basic.SIGNED.bin