Hardware requirements

  • Mini/micro USB cable

  • MIMXRT1180-EVK board

  • Personal Computer

  • SD card

Board settings

1.Please make sure R257/R140 is weld for GPIO card detect. 2.Please make sure J76 1-2 and J57 2-3 are installed for sdcard socket. Note: As the EVK board limitaion, there is eletronic mux added for switch between M.2 and sdcard which will affect the sdcard SDR104 timing. So the maximum sd card timing frequency been decreased to 100MHZ to improve the stability. User can remove the limitation by change the macro BOARD_SDMMC_SD_HOST_SUPPORT_SDR104_FREQ in sdmmc_config.h from (200000000U / 2U) to (200000000U).

Prepare the Demo

  1. Connect a micro USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Insert SD card to card slot

  4. Download the program to the target board.

  5. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, the log would be seen on the terminal like:


SDCARD fatfs freertos example.

Card inserted.

Make file system......The time may be long if the card capacity is big.

Create directory......
TASK1: write file successed.
TASK2: write file successed.
TASK1: finsied.
TASK2: finsied.