Hardware requirements
Mini/micro USB cable
MIMXRT1180-EVK board
Personal Computer
Note
The example is set up for TCM and FlexSPI targets. The provided .mex project file for the TEE Config tool is valid only for the TCM configuration. For FlexSPI, manual changes were applied to the generated source file; note the differences between tzm_config.c and the TEE tool source code output.
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the hello world demo in the terminal window:
Hello from secure world!
Entering normal world.
Welcome in normal world!
This is a text printed from normal world!
Comparing two string as a callback to normal world
String 1: Test1
String 2: Test2
Both strings are not equal!