Hardware requirements
Micro USB cable
EVK-MIMXRT595 board
Personal Computer
Board settings
The example provides 2 options of SPI interfaces in communication.
SPI5 (default, normal SPI: #define USE_HS_SPI 0)
SPI14 (optional, high speed SPI: #define USE_HS_SPI 1) User can change the USE_HS_SPI value in spi_dma_b2b_transfer_master.c to choose different SPI interface.
Connect SPI master on board to SPI slave on other board. Only 1 set of signals need to be connected, either SPI5 or SPI14 depending on the USE_HS_SPI setting. NOTE: To use SPI14 on EVK board, please connect JP32 1-2.
Master_board(SPI14) Slave_board(SPI14)
Pin Name Board Location Pin Name Board Location
MISO J36 pin 5 MISO J36 pin 5
MOSI J36 pin 3 MOSI J36 pin 3
SCK J36 pin 7 SCK J36 pin 7
PCS0 J36 pin 1 PCS0 J36 pin 1
GND J36 pin 9 GND J36 pin 9
Connect SPI master on board to SPI slave on other board
Master_board(SPI5) Slave_board(SPI5)
Pin Name Board Location Pin Name Board Location
MISO JP26 pin 3 MISO JP26 pin 3
MOSI JP26 pin 2 MOSI JP26 pin 2
SCK JP26 pin 4 SCK JP26 pin 4
PCS0 JP26 pin 1 PCS0 JP26 pin 1
GND JP26 pin 5 GND JP26 pin 5
Prepare the Demo
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J40) on the board
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the terminal like:
This is SPI DMA tranfer master example.
This example will communicate with another slave SPI on the other board.
Please start the slave board first!
The received data are:
0x00 0x01 0x02 0x03 0x04 0x05 0x06 0x07 0x08 0x09 0x0A 0x0B 0x0C 0x0D 0x0E 0x0F
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17 0x18 0x19 0x1A 0x1B 0x1C 0x1D 0x1E 0x1F
0x20 0x21 0x22 0x23 0x24 0x25 0x26 0x27 0x28 0x29 0x2A 0x2B 0x2C 0x2D 0x2E 0x2F
0x30 0x31 0x32 0x33 0x34 0x35 0x36 0x37 0x38 0x39 0x3A 0x3B 0x3C 0x3D 0x3E 0x3F
SPI transfer all data matched!