Hardware requirements
Micro USB cable
EVK-MIMXRT595 board
Personal Computer
Board settings
Prepare the Demo
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J40) on the board
Open a serial terminal with the following settings:
9600 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the terminal as follows (Note: please don’t input more than 16 bytes once as it might lead to UART FIFO overflow and result in failure):
USART DMA low power example
Send back received data
Echo every 8 characters (1st char 'q' leads to end).
------------------
Input any key to start.
Now enter deep sleep and wait for 8 characters.
12345678
------------------
Input any key to start.
Now enter deep sleep and wait for 8 characters.
asdfghjk
------------------
Input any key to start.
Now enter deep sleep and wait for 8 characters.
qwertyui
Done!